This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2538-CC2592EMK:2592:ZNP代码修改,用于配置UART接口。

Guru**** 2886930 points

Other Parts Discussed in Thread: CC2538-CC2592EMK, Z-STACK, CC2538, CC2592

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/653809/cc2538-cc2592emk-znp-code-modification-for-configuring-uart-interface

部件号:CC2538-CC2592EMK</s>2592
主题中讨论的其他部件: Z-stackCC2538CC2592

您好,

我想使用cc2538-cc2592emk作为2592作为带 UART接口的ZNP。

1)需要对z-stack 3.0 中的ZNP项目进行修改

2) CC2538引脚,用于UART接口。

3) Raspberry Pi上对应的UART引脚。

4) Z-stack Linux网关需要修改