请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:CC2650 大家好,
我想为6LoWPAN建立一个网关,根据网站上的可用选项,我选择了CC2650 (基于CC2650DK)。
现在,我对CC2650 IC的功能有一个疑问:
1.它是网关芯片,是多通道多收发器吗? 它可以解调多少个并发路径?
我提出这个问题是因为智能产品将发送/接收控制命令和重要信息,因此我们希望减少延迟。
此致
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果您想了解有关CC2650无线电部分的更多信息,建议您参阅 CC2650技术参考手册中的第23章。