This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2520:CC2520虚假FCC

Guru**** 2895520 points

Other Parts Discussed in Thread: CC2520

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1096967/cc2520-cc2520-spurious-fcc

部件号:CC2520

需要一些有关虚假问题的帮助。

我尝试通过FCC和台湾无线电认证,但我必须将功率级别降低到1 (-7dBm)。

我发现在2.34GHz和2.35GHz之间的杂散值约为50dbuV,即使在级别1 (-7dBm)。

我也检查了CC2520EVB (评估板),但寄生水平是相似的。 (连接的级别为2 (-4dBm))

结果是否合理?

CC2520数据表显示-41dbm (= 66dbuV),在2485.3MHz及以上(FCC受限频段)时为4级(0dBm)。  

“2485.3MHz及以上”还包括2.34GHz和2.35GHz,不确定...