This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2538:关于 Z-Stack 3.0.1 OTA CRC32

Guru**** 2966500 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1113693/cc2538-about-z-stack-3-0-1-ota-crc32

器件型号:CC2538

大家好、

客户希望了解 hal_ota.c 中以下代码的含义:

typedef long (* volatile HAPI_CRC32_T)(unsigned char *, unsigned long);
#define HAPI_CRC32_FUNC_PTR 0x00000048
#define P_HAPI_CRC32 ((HAPI_CRC32_T *)HAPI_CRC32_FUNC_PTR)
#define CalcCrc32(a,b) (*P_HAPI_CRC32)(a,b)

代码如何实现映像的 CRC 校验? 0x00000048指向什么?

请帮您检查一下。

此致、

Kevin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Kevin:

    HAPI 表示"硬 API"、0x00000048指向存储在 ROM 中的 CRC32函数。

    #ifndef __ROM_H__
    #define __ROM_H__
    
    //*****************************************************************************
    //
    // If building with a C++ compiler, make all of the definitions in this header
    // have a C binding.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    extern "C"
    {
    #endif
    
    #include "hw_types.h"
    
    //
    // Start address of the ROM hard API access table (located after the ROM FW rev field)
    //
    #define ROM_API_TABLE_ADDR 0x00000048
    
    //
    // ROM utility function interface types
    //
    typedef uint32_t       (* volatile FPTR_CRC32_T)       (uint8_t* /*pData*/, uint32_t /*byteCount*/);
    typedef uint32_t       (* volatile FPTR_GETFLSIZE_T)   (void);
    typedef uint32_t       (* volatile FPTR_GETCHIPID_T)   (void);
    typedef int32_t        (* volatile FPTR_PAGEERASE_T)   (uint32_t /*FlashAddr*/, uint32_t /*Size*/);
    typedef int32_t        (* volatile FPTR_PROGFLASH_T)   (uint32_t* /*pRamData*/, uint32_t /*FlashAdr*/, uint32_t /*ByteCount*/);
    typedef void           (* volatile FPTR_RESETDEV_T)    (void);
    typedef void*          (* volatile FPTR_MEMSET_T)      (void* /*s*/, int32_t /*c*/, uint32_t /*n*/);
    typedef void*          (* volatile FPTR_MEMCPY_T)      (void* /*s1*/, const void* /*s2*/, uint32_t /*n*/);
    typedef int32_t        (* volatile FPTR_MEMCMP_T)      (const void* /*s1*/, const void* /*s2*/, uint32_t /*n*/);
    typedef void*          (* volatile FPTR_MEMMOVE_T)     (void* /*s1*/, const void* /*s2*/, uint32_t /*n*/);
    
    //
    // ROM Hard-API access table type
    //
    typedef struct
        {
            FPTR_CRC32_T        Crc32;
            FPTR_GETFLSIZE_T    GetFlashSize;
            FPTR_GETCHIPID_T    GetChipId;
            FPTR_PAGEERASE_T    PageErase;
            FPTR_PROGFLASH_T    ProgramFlash;
            FPTR_RESETDEV_T     ResetDevice;
            FPTR_MEMSET_T       memset;
            FPTR_MEMCPY_T       memcpy;
            FPTR_MEMCMP_T       memcmp;
            FPTR_MEMMOVE_T      memmove;
        } ROM_API_T;
    
    //
    // Pointer to the ROM API table
    //
    #define P_ROM_API              ((ROM_API_T*) ROM_API_TABLE_ADDR)
    
    #define ROM_Crc32(a,b)          P_ROM_API->Crc32(a,b)
    #define ROM_GetFlashSize()      P_ROM_API->GetFlashSize()
    #define ROM_GetChipId()         P_ROM_API->GetChipId()
    #define ROM_PageErase(a,b)      P_ROM_API->PageErase(a,b)
    #define ROM_ProgramFlash(a,b,c) P_ROM_API->ProgramFlash(a,b,c)
    #define ROM_ResetDevice()       P_ROM_API->ResetDevice()
    #define ROM_Memset(a,b,c)       P_ROM_API->memset(a,b,c)
    #define ROM_Memcpy(a,b,c)       P_ROM_API->memcpy(a,b,c)
    #define ROM_Memcmp(a,b,c)       P_ROM_API->memcmp(a,b,c)
    #define ROM_Memmove(a,b,c)      P_ROM_API->memmove(a,b,c)
    
    //*****************************************************************************
    //
    // Mark the end of the C bindings section for C++ compilers.
    //
    //*****************************************************************************
    #ifdef __cplusplus
    }
    #endif
    
    #endif // __ROM_H__

    此致、
    Ryan