This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-CC1352P:在 ZR 警告器件示例中读取 ADC。

Guru**** 3001220 points

Other Parts Discussed in Thread: LAUNCHXL-CC1352P

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1022497/launchxl-cc1352p-adc-read-in-zr-warning-device-example

器件型号:LAUNCHXL-CC1352P
Thread 中讨论的其他器件: SYSBIOS

您好!

SDK 5.10

器件:LAUNCHXL-CC1352P

我想读取 ZR 警告设备中的连续 ADC。 我已完全禁用 UI。 此外、我添加了 ADC 代码、但在一段时间后、它将停止工作。 请找到以下代码。 我尝试了很多,但没有找到解决方案。 335次 ADC 迭代后、整个代码停止工作。 请指导我。

/**************************************************************************************************
Filename: zcl_samplewarningdevice.c
Revised: $Date: 2015-08-19 17:11:00 -0700 (Wed, 19 Aug 2015) $
Revision: $Revision: 44460 $

Description: Zigbee Cluster Library - warning device application.


Copyright 2006-2013 Texas Instruments Incorporated. All rights reserved.

IMPORTANT: Your use of this Software is limited to those specific rights
granted under the terms of a software license agreement between the user
who downloaded the software, his/her employer (which must be your employer)
and Texas Instruments Incorporated (the "License"). You may not use this
Software unless you agree to abide by the terms of the License. The License
limits your use, and you acknowledge, that the Software may not be modified,
copied or distributed unless embedded on a Texas Instruments microcontroller
or used solely and exclusively in conjunction with a Texas Instruments radio
frequency transceiver, which is integrated into your product. Other than for
the foregoing purpose, you may not use, reproduce, copy, prepare derivative
works of, modify, distribute, perform, display or sell this Software and/or
its documentation for any purpose.

YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL
TEXAS INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER
LEGAL EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES
INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE
OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT
OF SUBSTITUTE GOODS, TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES
(INCLUDING BUT NOT LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.

Should you have any questions regarding your right to use this Software,
contact Texas Instruments Incorporated at www.TI.com.
**************************************************************************************************/

/*********************************************************************
This application implements a Zigbee IAS Warning Device, based on Z-Stack 3.0.

This application is based on the common sample-application user interface. Please see the main
comment in zcl_sampleapp_ui.c. The rest of this comment describes only the content specific for
this sample application.

Application-specific UI peripherals being used:

- LEDs:
LED1 Blinking if there is an alarm in the local device. Solid On if there is a warning message
from another device. Blink once when a Squawk is received from CIE. Off otherwise.

Application-specific menu system:
Screens:
Enrollment Mode Configuration Screen:
TRIP_TO_PAIR:
Zone should perform manual Zone Enroll Request by user action (e.g. through UI)
Enabled by default, use the <SEND ENROLL REQ > App screen to perform this action.
AUTO_ENROLL_REQUEST:
Zone should automatically send a Zone Enroll Request after the
CIE IEEE Addr attribute is written by the CIE
Discover Zone Device Screen: Press 'Enter' to discover the Zone device that is already discoverable, to perform the
enrollment of the Zone device.
Zone Enrollment Screen: Summarizes the enrollment status of the Zone device displaying if the enrollment
process has finished or not. This screen also displays the type of Zone (fire alarm in this case)
Toggle Alarm screen: Press 'Enter' to toggle between Alarm or No Alarm, this will trigger a Change Notification
Request to CIE if fully enrolled.
Status Lines:
CIE Address/Zone ID: Shows the current values of CIE IEEE Address + Zone ID
1.- If no CIE Address has been provided, then it is set to F's.
2.- If CIE address is provided, enrollement can be sent using the Zone Enrollment Screen, or by
enabling Auto Enrollment via the Enrollment Configuration screen
3.- If fully enrolled, CIE address is displayed allong with the Zone Id.
Zone Status: Shows if the device is currently Zone Enrolled, the type of Zone, and if the Zone
is currently Alarmed or not
Strobe Alarmed: This line displays warning messages received from CIE (Alarm in Progress) if no alarm is
currenty running on the local device.

*********************************************************************/

/*********************************************************************
* INCLUDES
*/
#include "rom_jt_154.h"
#include "zcomdef.h"
#include "zcl.h"
#include "zcl_general.h"
#include "zcl_ha.h"
#include "zcl_ss.h"

#include "zcl_samplewarningdevice.h"


#include <ti/drivers/apps/Button.h>
#include <ti/drivers/apps/LED.h>
#include <ti/display/Display.h>
#include <ti/drivers/ADC.h>
#include <ti/drivers/NVS.h>

#include "ti_drivers_config.h"

#ifndef CUI_DISABLE
#include "zcl_sampleapps_ui.h"
#include "zcl_sample_app_def.h"
#endif
#include "bdb_interface.h"

#include "nvintf.h"
#include "zstackmsg.h"
#include "zcl_port.h"

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Task.h>

#include "zstackapi.h"
#include "util_timer.h"
#include "addr_mgr.h"
#include <string.h>


#if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE)
#include "gp_common.h"
#endif
/*********************************************************************
* MACROS
*/

/*********************************************************************
* TYPEDEFS
*/

/*********************************************************************
* GLOBAL VARIABLES
*/
//static LED_Handle gRedLedHandle;
static LED_Handle gas10LedHandle;
static LED_Handle gas7LedHandle;
static LED_Handle gas5LedHandle;
static LED_Handle gas25LedHandle;
static LED_Handle heatLedHandle;
static LED_Handle gasLedHandle;
static LED_Handle buzzerLedHandle;
static Display_Handle display;


/*********************************************************************
* GLOBAL FUNCTIONS
*/

/*********************************************************************
* LOCAL VARIABLES
*/
// Semaphore used to post events to the application thread
static Semaphore_Handle appSemHandle;
static Semaphore_Struct appSem;

/* App service ID used for messaging with stack service task */
static uint8_t appServiceTaskId;
/* App service task events, set by the stack service task when sending a message */
static uint32_t appServiceTaskEvents;
static endPointDesc_t zclSampleWarningDeviceEpDesc = {0};

#if ZG_BUILD_ENDDEVICE_TYPE
static Clock_Handle EndDeviceRejoinClkHandle;
static Clock_Struct EndDeviceRejoinClkStruct;
#endif

static Clock_Handle AutoEnrollReqClkHandle;
static Clock_Struct AutoEnrollReqClkStruct;
static Clock_Handle AutobindingReqClkHandle;
static Clock_Handle AutobindingstopClkHandle;
static Clock_Handle AutogasReqClkHandle;
static Clock_Struct AutogasReqClkStruct;
static Clock_Struct SquawkClkStruct;
static Clock_Struct AutobindingReqClkStruct;
static Clock_Struct AutobindingstopClkStruct;
static Clock_Handle WarningDurationClkHandle;
static Clock_Struct WarningDurationClkStruct;
#ifndef CUI_DISABLE
static Clock_Handle SquawkClkHandle;
#endif

// Passed in function pointers to the NV driver
static NVINTF_nvFuncts_t *pfnZdlNV = NULL;

#ifndef CUI_DISABLE
static uint16_t zclSampleWarningDevice_BdbCommissioningModes;
#endif

afAddrType_t zclSampleWarningDevice_DstAddr;

//Temporal variable to store the CIE endpoint
static uint8_t tempCIEsrcEndpoint = 0;

#ifdef ZCL_WD
uint8_t tempWarningInProgress = 0;
bool gSquawkReq = FALSE;
#endif

//static LED_Handle gRedLedHandle;

#ifndef CUI_DISABLE
CONST char zclSampleWarningDevice_appStr[] = APP_TITLE_STR;
CUI_clientHandle_t gCuiHandle;
static uint32_t gSampleWarningDeviceInfoLine1;
static uint32_t gSampleWarningDeviceInfoLine2;
static uint32_t gSampleWarningDeviceInfoLine3;
#endif

// Modify this to select the default Zone Enrollment Mode.
// Choices are (per spec):
// TRIP_TO_PAIR
// AUTO_ENROLL_REQUEST
static IAS_Zone_EnrollmentModes_t zclSampleWarningDevice_enrollmentMode = TRIP_TO_PAIR;

/*********************************************************************
* LOCAL FUNCTIONS
*/
static void zclSampleWarningDevice_initialization(void);
static void zclSampleWarningDevice_process_loop(void);
static void zclSampleWarningDevice_initParameters(void);
static void zclSampleWarningDevice_processZStackMsgs(zstackmsg_genericReq_t *pMsg);
static void SetupZStackCallbacks(void);
static void zclSampleWarningDevice_processAfIncomingMsgInd(zstack_afIncomingMsgInd_t *pInMsg);
static void zclSampleWarningDevice_initializeClocks(void);
#if ZG_BUILD_ENDDEVICE_TYPE
static void zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback(UArg a0);
#endif
static void zclSampleWarningDevice_processWarningDurationTimeoutCallback(UArg a0);
static void zclSampleWarningDevice_processAutoEnrollReqTimeoutCallback(UArg a0);
static void zclSampleWarningDevice_processAutobindingReqTimeoutCallback(UArg a0);
static void zclSampleWarningDevice_processAutobindingstopTimeoutCallback(UArg a0);
static void zclSampleWarningDevice_processAuto_adc_readCallback(UArg a0);
#ifndef CUI_DISABLE
static void zclSampleWarningDevice_processSquawkClkTimeoutCallback(UArg a0);

static void zclSampleWarningDevice_processKey(uint8_t key, Button_EventMask buttonEvents);
static void zclSampleWarningDevice_RemoveAppNvmData(void);
static void zclSampleWarningDevice_InitializeStatusLine(CUI_clientHandle_t gCuiHandle);
static void zclSampleWarningDevice_UpdateStatusLine(void);
#endif
static void zclSampleWarningDevice_Init( void );

static void zclSampleWarningDevice_BasicResetCB( void );
static void zclSampleWarningDevice_ProcessCommissioningStatus(bdbCommissioningModeMsg_t *bdbCommissioningModeMsg);

// Functions to process ZCL Foundation incoming Command/Response messages
static uint8_t zclSampleWarningDevice_ProcessIncomingMsg( zclIncoming_t *msg );
#ifdef ZCL_READ
static uint8_t zclSampleWarningDevice_ProcessInReadRspCmd( zclIncoming_t *pInMsg );
#endif
#ifdef ZCL_WRITE
static uint8_t zclSampleWarningDevice_ProcessInWriteRspCmd( zclIncoming_t *pInMsg );
#endif
static uint8_t zclSampleWarningDevice_ProcessInDefaultRspCmd( zclIncoming_t *pInMsg );
#ifdef ZCL_DISCOVER
static uint8_t zclSampleWarningDevice_ProcessInDiscCmdsRspCmd( zclIncoming_t *pInMsg );
static uint8_t zclSampleWarningDevice_ProcessInDiscAttrsRspCmd( zclIncoming_t *pInMsg );
static uint8_t zclSampleWarningDevice_ProcessInDiscAttrsExtRspCmd( zclIncoming_t *pInMsg );
#endif

#ifdef ZCL_WD
//WD Cluster
static ZStatus_t zclSampleWarningDevice_StartWarningCB(zclWDStartWarning_t *pCmd);
static ZStatus_t zclSampleWarningDevice_SquawkCB(zclWDSquawk_t *squawk);
#endif

#ifdef ZCL_ZONE
static void zclSampleWarningDevice_SendEnrollReqToCIE(void);
static ZStatus_t zclSampleWarningDevice_EnrollResponseCB(zclZoneEnrollRsp_t *rsp);
static uint8_t zclSampleWarningDevice_AuthenticateCIE(afAddrType_t *srcAddr, zclAttrRec_t *pAttr, uint8_t oper);
#ifndef CUI_DISABLE
static void zclSampleWarningDevice_SendChangeNotification(void);
static void ArrayToString (uint8_t * buf, char * str, uint8_t num_of_digists, bool big_endian);
#endif
#endif // ZCL_ZONE
void Gas_sensor(void);
static void gaschange_SendChangeNotification(void);
static void Temp_SendChangeNotification(void);
static void Test_SendChangeNotification(void);

/*********************************************************************
* CONSTANTS
*/

uint8_t status;
uint8_t auto_binding=0;
uint8_t timer_start_flag=0;


uint32_t buffersCompletedCounter = 0;
uint16_t TempsampleBufferOne[ADCSAMPLESIZE];
uint16_t TempsampleBufferTwo[ADCSAMPLESIZE];
uint32_t TempmicroVoltBuffer[ADCSAMPLESIZE];
uint32_t TempoutputBuffer[ADCSAMPLESIZE];
uint8_t alarm_condition=0;
uint8_t Temp=0;
uint8_t gpio_status=0;
uint32_t average;
uint32_t calculated_average;
uint8_t NVS_read_flag=0;
uint8_t status;
uint32_t Temperature;
uint8_t Test=0;
uint8_t Test_button_flag=1;
uint32_t adc_open_flag=0;
uint8_t ledson=0;
uint32_t count=0;
/*********************************************************************
* REFERENCED EXTERNALS
*/
ADC_Handle adc;
ADC_Params params_adc;

/*********************************************************************
* ZCL General Profile Callback table
*/
static zclGeneral_AppCallbacks_t zclSampleWarningDevice_CmdCallbacks =
{
zclSampleWarningDevice_BasicResetCB, // Basic Cluster Reset command
NULL, // Identfiy cmd
NULL, // Identify Query command
NULL, // Identify Query Response command
NULL, // Identify Trigger Effect command
#ifdef ZCL_ON_OFF
NULL, // On/Off cluster commands
NULL, // On/Off cluster enhanced command Off with Effect
NULL, // On/Off cluster enhanced command On with Recall Global Scene
NULL, // On/Off cluster enhanced command On with Timed Off
#endif
#ifdef ZCL_LEVEL_CTRL
NULL, // Level Control Move to Level command
NULL, // Level Control Move command
NULL, // Level Control Step command
NULL, // Level Control Stop command
NULL, // Level Control Move to Closest Frequency command
#endif
#ifdef ZCL_GROUPS
NULL, // Group Response commands
#endif
#ifdef ZCL_SCENES
NULL, // Scene Store Request command
NULL, // Scene Recall Request command
NULL, // Scene Response command
#endif
#ifdef ZCL_ALARMS
NULL, // Alarm (Response) commands
#endif
#ifdef SE_UK_EXT
NULL, // Get Event Log command
NULL, // Publish Event Log command
#endif
NULL, // RSSI Location command
NULL // RSSI Location Response command
};


/*********************************************************************
* ZCL SS Profile Callback table
*/
static zclSS_AppCallbacks_t zclSampleWarningDevice_SSCmdCallbacks =
{
NULL, // Change Notification command
NULL, // Enroll Request command
zclSampleWarningDevice_EnrollResponseCB, // Enroll Reponse command
NULL, // Initiate Normal Operation Mode command
NULL, // Initiate Test Mode command
NULL, // Arm command
NULL, // Bypass command
NULL, // Emergency command
NULL, // Fire command
NULL, // Panic command
NULL, // Get Zone ID Map command
NULL, // Get Zone Information Command
NULL, // Get Panel Status Command
NULL, // Get Bypassed Zone List Command
NULL, // Get Zone Status Command
NULL, // ArmResponse command
NULL, // Get Zone ID Map Response command
NULL, // Get Zone Information Response command
NULL, // Zone Status Changed command
NULL, // Panel Status Changed command
NULL, // Get Panel Status Response command
NULL, // Set Bypassed Zone List command
NULL, // Bypass Response command
NULL, // Get Zone Status Response command
zclSampleWarningDevice_StartWarningCB, // Start Warning command
zclSampleWarningDevice_SquawkCB // Squawk command
};


/*******************************************************************************
* @fn sampleApp_task
*
* @brief Application task entry point for the Z-Stack
* Sample Application
*
* @param pfnNV - pointer to the NV functions
*
* @return none
*/
void sampleApp_task(NVINTF_nvFuncts_t *pfnNV)
{
// Save and register the function pointers to the NV drivers
pfnZdlNV = pfnNV;
zclport_registerNV(pfnZdlNV, ZCL_PORT_SCENE_TABLE_NV_ID);

// Initialize application
zclSampleWarningDevice_initialization();
Display_init();

display = Display_open(Display_Type_UART, NULL);
if (display == NULL) {
/* Failed to open display driver */
while (1);
}
Display_printf(display, 0, 0, "Starting the acdsinglechannel example\n");


// No return from task process
zclSampleWarningDevice_process_loop();
}


/*******************************************************************************
* @fn zclSampleWarningDevice_initialization
*
* @brief Initialize the application
*
* @param none
*
* @return none
*/
static void zclSampleWarningDevice_initialization(void)
{
/* Initialize user clocks */
zclSampleWarningDevice_initializeClocks();

/* create semaphores for messages / events
*/
Semaphore_Params semParam;
Semaphore_Params_init(&semParam);
semParam.mode = ti_sysbios_knl_Semaphore_Mode_COUNTING;
Semaphore_construct(&appSem, 0, &semParam);
appSemHandle = Semaphore_handle(&appSem);

appServiceTaskId = OsalPort_registerTask(Task_self(), appSemHandle, &appServiceTaskEvents);


//Initialize stack
zclSampleWarningDevice_Init();
}

/*********************************************************************
* @fn zclSampleWarningDevice_Init
*
* @brief Initialization function for the zclGeneral layer.
*
* @param none
*
* @return none
*/
static void zclSampleWarningDevice_Init( void )
{

// Set destination address to indirect
zclSampleWarningDevice_DstAddr.addrMode = (afAddrMode_t)AddrNotPresent;
zclSampleWarningDevice_DstAddr.endPoint = 0;
zclSampleWarningDevice_DstAddr.addr.shortAddr = 0;

//Register Endpoint
zclSampleWarningDeviceEpDesc.endPoint = SAMPLEWARNINGDEVICE_ENDPOINT;
zclSampleWarningDeviceEpDesc.simpleDesc = &zclSampleWarningDevice_SimpleDesc;
zclport_registerEndpoint(appServiceTaskId, &zclSampleWarningDeviceEpDesc);

#if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE)
gp_endpointInit(appServiceTaskId);
#endif

// Register the ZCL General Cluster Library callback functions
zclGeneral_RegisterCmdCallbacks( SAMPLEWARNINGDEVICE_ENDPOINT, &zclSampleWarningDevice_CmdCallbacks );

// Register the ZCL Security and Safety Cluster Library callback functions
zclSS_RegisterCmdCallbacks( SAMPLEWARNINGDEVICE_ENDPOINT, &zclSampleWarningDevice_SSCmdCallbacks );

// Register the application's attribute list and reset to default values
zclSampleWarningDevice_ResetAttributesToDefaultValues();
zcl_registerAttrList( SAMPLEWARNINGDEVICE_ENDPOINT, zclSampleWarningDevice_NumAttributes, zclSampleWarningDevice_Attrs );

// Register the Application to receive the unprocessed Foundation command/response messages
zclport_registerZclHandleExternal(SAMPLEWARNINGDEVICE_ENDPOINT, zclSampleWarningDevice_ProcessIncomingMsg);

zcl_registerReadWriteCB( SAMPLEWARNINGDEVICE_ENDPOINT, NULL, zclSampleWarningDevice_AuthenticateCIE );

//Write the bdb initialization parameters
zclSampleWarningDevice_initParameters();

//Setup ZDO callbacks
SetupZStackCallbacks();


#if defined ( BDB_TL_INITIATOR )
zclSampleWarningDevice_BdbCommissioningModes |= BDB_COMMISSIONING_MODE_INITIATOR_TL;
#endif

#if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE)
app_Green_Power_Init(appServiceTaskId, &appServiceTaskEvents, appSemHandle, SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT,
SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT, SAMPLEAPP_PROCESS_GP_TEMP_MASTER_EVT);
#endif

#ifndef CUI_DISABLE
// set up default application BDB commissioning modes based on build type
if(ZG_BUILD_COORDINATOR_TYPE && ZG_DEVICE_COORDINATOR_TYPE)
{
zclSampleWarningDevice_BdbCommissioningModes = BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_NWK_STEERING | BDB_COMMISSIONING_MODE_FINDING_BINDING;
}
else if (ZG_BUILD_JOINING_TYPE && ZG_DEVICE_JOINING_TYPE)
{
zclSampleWarningDevice_BdbCommissioningModes = BDB_COMMISSIONING_MODE_NWK_STEERING | BDB_COMMISSIONING_MODE_FINDING_BINDING;
}


gCuiHandle = UI_Init( appServiceTaskId, // Application Task ID
&appServiceTaskEvents, // The events processed by the sample application
appSemHandle, // Semaphore to post the events in the application thread
&zclSampleWarningDevice_IdentifyTime,
&zclSampleWarningDevice_BdbCommissioningModes, // A pointer to the application's bdbCommissioningModes
zclSampleWarningDevice_appStr, // A pointer to the app-specific name string
zclSampleWarningDevice_processKey, // A pointer to the app-specific key process function
zclSampleWarningDevice_RemoveAppNvmData // A pointer to the app-specific NV Item reset function
);

//Request the Red LED for App
LED_Params ledParams;
LED_Params_init(&ledParams);
gRedLedHandle = LED_open(CONFIG_LED_RED, &ledParams);

//Initialize the SampleWarningDevice UI status line
zclSampleWarningDevice_InitializeStatusLine(gCuiHandle);
#endif
/* LEDs declaration */
// Gas Led 10%
LED_Params led10Params;
LED_Params_init(&led10Params);
gas10LedHandle = LED_open(LED_10_PER, &led10Params);
//Gas Led 7%
LED_Params led7Params;
LED_Params_init(&led7Params);
gas7LedHandle = LED_open(LED_7_PER, &led7Params);
//Gas Led 5%
LED_Params led5Params;
LED_Params_init(&led5Params);
gas5LedHandle = LED_open(LED_5_PER, &led5Params);
//Gas Led 25%
LED_Params led25Params;
LED_Params_init(&led25Params);
gas25LedHandle = LED_open(LED_25_PER, &led25Params);
//temp led
LED_Params ledheatParams;
LED_Params_init(&ledheatParams);
heatLedHandle = LED_open(HEAT_LED, &ledheatParams);

LED_Params ledgasParams;
LED_Params_init(&ledgasParams);
gasLedHandle = LED_open(GAS_LED, &ledgasParams);

LED_Params ledbuzzerParams;
LED_Params_init(&ledbuzzerParams);
buzzerLedHandle = LED_open(BUZZER, &ledbuzzerParams);

/* Initialize IAS ZONE Nv Items */
if(SUCCESS == zclport_initializeNVItem(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_STATE_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneState),&zclSampleWarningDevice_ZoneState))
{
//retrieve the Zone State, either enrolled or not
zclport_readNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_STATE_NV_SUBID,0, sizeof(zclSampleWarningDevice_ZoneState),&zclSampleWarningDevice_ZoneState);
}
if(SUCCESS == zclport_initializeNVItem(IAS_ZONE_NV_ID, IAS_ZONE_CIE_ADDRESS_NV_SUBID, sizeof(zclSampleWarningDevice_CIE_Address),zclSampleWarningDevice_CIE_Address))
{
//retrieve the CIE Address
zclport_readNV(IAS_ZONE_NV_ID, IAS_ZONE_CIE_ADDRESS_NV_SUBID,0, sizeof(zclSampleWarningDevice_CIE_Address),zclSampleWarningDevice_CIE_Address);
}
if(SUCCESS == zclport_initializeNVItem(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_ID_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneId),&zclSampleWarningDevice_ZoneId))
{
//retrieve the Zone ID
zclport_readNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_ID_NV_SUBID, 0, sizeof(zclSampleWarningDevice_ZoneId),&zclSampleWarningDevice_ZoneId);
}

// Call BDB initialization. Should be called once from application at startup to restore
// previous network configuration, if applicable.
zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
zstack_bdbStartCommissioningReq.commissioning_mode = 0;
Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
// UtilTimer_setTimeout( AutobindingReqClkHandle, SAMPLEAPP_AUTO_BINDING_REQ_DELAY );
// UtilTimer_start( &AutobindingReqClkStruct );
// UtilTimer_setTimeout( AutobindingstopClkHandle, SAMPLEAPP_AUTO_BINDING_STOP_DELAY );
// UtilTimer_start( &AutobindingstopClkStruct );
UtilTimer_setTimeout( AutogasReqClkHandle, SAMPLEAPP_GAS_READ_DELAY );
UtilTimer_start( &AutogasReqClkStruct );
}

#ifndef CUI_DISABLE
/*********************************************************************
* @fn zclSampleWarningDevice_RemoveAppNvmData
*
* @brief Callback when Application performs reset to Factory New Reset.
* Application must restore the application to default values
*
* @param none
*
* @return none
*/
static void zclSampleWarningDevice_RemoveAppNvmData(void)
{
zclSampleWarningDevice_BasicResetCB();
}
#endif


static void zclSampleWarningDevice_initParameters(void)
{
zstack_bdbSetAttributesReq_t zstack_bdbSetAttrReq;

zstack_bdbSetAttrReq.bdbCommissioningGroupID = BDB_DEFAULT_COMMISSIONING_GROUP_ID;
zstack_bdbSetAttrReq.bdbPrimaryChannelSet = BDB_DEFAULT_PRIMARY_CHANNEL_SET;
zstack_bdbSetAttrReq.bdbScanDuration = BDB_DEFAULT_SCAN_DURATION;
zstack_bdbSetAttrReq.bdbSecondaryChannelSet = BDB_DEFAULT_SECONDARY_CHANNEL_SET;
zstack_bdbSetAttrReq.has_bdbCommissioningGroupID = TRUE;
zstack_bdbSetAttrReq.has_bdbPrimaryChannelSet = TRUE;
zstack_bdbSetAttrReq.has_bdbScanDuration = TRUE;
zstack_bdbSetAttrReq.has_bdbSecondaryChannelSet = TRUE;
#if (ZG_BUILD_COORDINATOR_TYPE)
zstack_bdbSetAttrReq.has_bdbJoinUsesInstallCodeKey = TRUE;
zstack_bdbSetAttrReq.has_bdbTrustCenterNodeJoinTimeout = TRUE;
zstack_bdbSetAttrReq.has_bdbTrustCenterRequireKeyExchange = TRUE;
zstack_bdbSetAttrReq.bdbJoinUsesInstallCodeKey = BDB_DEFAULT_JOIN_USES_INSTALL_CODE_KEY;
zstack_bdbSetAttrReq.bdbTrustCenterNodeJoinTimeout = BDB_DEFAULT_TC_NODE_JOIN_TIMEOUT;
zstack_bdbSetAttrReq.bdbTrustCenterRequireKeyExchange = BDB_DEFAULT_TC_REQUIRE_KEY_EXCHANGE;
#endif
#if (ZG_BUILD_JOINING_TYPE)
zstack_bdbSetAttrReq.has_bdbTCLinkKeyExchangeAttemptsMax = TRUE;
zstack_bdbSetAttrReq.has_bdbTCLinkKeyExchangeMethod = TRUE;
zstack_bdbSetAttrReq.bdbTCLinkKeyExchangeAttemptsMax = BDB_DEFAULT_TC_LINK_KEY_EXCHANGE_ATTEMPS_MAX;
zstack_bdbSetAttrReq.bdbTCLinkKeyExchangeMethod = BDB_DEFAULT_TC_LINK_KEY_EXCHANGE_METHOD;
#endif

Zstackapi_bdbSetAttributesReq(appServiceTaskId, &zstack_bdbSetAttrReq);
}

/*******************************************************************************
* @fn zclSampleWarningDevice_initializeClocks
*
* @brief Initialize Clocks
*
* @param none
*
* @return none
*/
static void zclSampleWarningDevice_initializeClocks(void)
{
#if ZG_BUILD_ENDDEVICE_TYPE
// Initialize the timers needed for this application
EndDeviceRejoinClkHandle = UtilTimer_construct(
&EndDeviceRejoinClkStruct,
zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback,
SAMPLEAPP_END_DEVICE_REJOIN_DELAY,
0, false, 0);
#endif

WarningDurationClkHandle = UtilTimer_construct(
&WarningDurationClkStruct,
zclSampleWarningDevice_processWarningDurationTimeoutCallback,
zclSampleWarningDevice_MaxDuration*1000,
0, false, 0);


AutoEnrollReqClkHandle = UtilTimer_construct(
&AutoEnrollReqClkStruct,
zclSampleWarningDevice_processAutoEnrollReqTimeoutCallback,
SAMPLEAPP_AUTO_ENROLL_REQ_DELAY,
0, false, 0);

AutobindingReqClkHandle = UtilTimer_construct(
&AutobindingReqClkStruct,
zclSampleWarningDevice_processAutobindingReqTimeoutCallback,
SAMPLEAPP_AUTO_BINDING_REQ_DELAY,
10000, false, 0);

AutobindingstopClkHandle = UtilTimer_construct(
&AutobindingstopClkStruct,
zclSampleWarningDevice_processAutobindingstopTimeoutCallback,
SAMPLEAPP_AUTO_BINDING_STOP_DELAY,
0, false, 0);

AutogasReqClkHandle = UtilTimer_construct(
&AutogasReqClkStruct,
zclSampleWarningDevice_processAuto_adc_readCallback,
SAMPLEAPP_GAS_READ_DELAY,
500, true, 0);
#ifndef CUI_DISABLE
SquawkClkHandle = UtilTimer_construct(
&SquawkClkStruct,
zclSampleWarningDevice_processSquawkClkTimeoutCallback,
SAMPLEAPP_AUTO_ENROLL_REQ_DELAY,
0, false, 0);
#endif

}

#if ZG_BUILD_ENDDEVICE_TYPE
/*******************************************************************************
* @fn zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback
*
* @brief Timeout handler function
*
* @param a0 - ignored
*
* @return none
*/
static void zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_END_DEVICE_REJOIN_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}
#endif

/*******************************************************************************
* @fn zclSampleWarningDevice_processWarningDurationTimeoutCallback
*
* @brief Timeout handler function
*
* @param a0 - ignored
*
* @return none
*/
static void zclSampleWarningDevice_processWarningDurationTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_WARNING_DURATION_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}

/*******************************************************************************
* @fn zclSampleWarningDevice_processAutobindingReqTimeoutCallback
*
* @brief Timeout handler function for auto binding
*
* @param a0 - ignored
*
* @return none
*/

static void zclSampleWarningDevice_processAutobindingReqTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_AUTO_BINDING_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}

/*******************************************************************************
* @fn zclSampleWarningDevice_processAutobindingstopTimeoutCallback
*
* @brief Timeout handler function for auto binding
*
* @param a0 - ignored
*
* @return none
*/

static void zclSampleWarningDevice_processAutobindingstopTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_AUTO_BINDING_STOP_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}


#ifndef CUI_DISABLE
/*******************************************************************************
* @fn zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback
*
* @brief Timeout handler function
*
* @param a0 - ignored
*
* @return none
*/
static void zclSampleWarningDevice_processSquawkClkTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_SQUAWK_UI_TIMEOUT_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}
#endif

/*******************************************************************************
* @fn zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback
*
* @brief Timeout handler function
*
* @param a0 - ignored
*
* @return none
*/
static void zclSampleWarningDevice_processAutoEnrollReqTimeoutCallback(UArg a0)
{
(void)a0; // Parameter is not used

appServiceTaskEvents |= SAMPLEAPP_AUTO_ENROLL_REQ_EVT;

// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}

/*******************************************************************************
* @fn zclSampleWarningDevice_processEndDeviceRejoinTimeoutCallback
*
* @brief Timeout handler function
*
* @param a0 - ignored
*
* @return none
*/
static void zclSampleWarningDevice_processAuto_adc_readCallback(UArg a0)
{
Gas_sensor();

}

/*******************************************************************************
* @fn SetupZStackCallbacks
*
* @brief Setup the Zstack Callbacks wanted
*
* @param none
*
* @return none
*/
static void SetupZStackCallbacks(void)
{
zstack_devZDOCBReq_t zdoCBReq = {0};

// Register for Callbacks, turn on:
// Device State Change,
// ZDO Match Descriptor Response,
zdoCBReq.has_devStateChange = true;
zdoCBReq.devStateChange = true;

(void)Zstackapi_DevZDOCBReq(appServiceTaskId, &zdoCBReq);
}

/*******************************************************************************
* @fn gas sensor adc read
*
* @brief get gas data using adc
*
* @param none
*
* @return none
*/

void Gas_sensor(void){

uint16_t i;

int_fast16_t res;
NVS_Handle nvsHandle;
NVS_Attrs regionAttrs;
NVS_Params nvsParams;
uint16_t sampleBufferOne[ADCSAMPLESIZE];
uint16_t sampleBufferTwo[ADCSAMPLESIZE];
uint32_t microVoltBuffer[ADCSAMPLESIZE];
uint32_t outputBuffer[ADCSAMPLESIZE];
if (adc_open_flag==0){
ADC_init();


ADC_Params_init(&params_adc);
NVS_init();
NVS_Params_init(&nvsParams);
adc = ADC_open(GAS_ADC, &params_adc);

if (adc == NULL) {
Display_printf(display, 0, 0, "Error initializing CONFIG_ADC_1\n");
while (1){};
}
adc_open_flag++;
}
uint32_t * buffer_ = (uint32_t *) malloc(TEMP_BUF_SIZE);


for (i = 0; i < ADCSAMPLESIZE; i++) {
res = ADC_convert(adc, &sampleBufferOne[i]);
Task_sleep(1);

if (res == ADC_STATUS_SUCCESS) {

outputBuffer[i] = ADC_convertRawToMicroVolts(adc, sampleBufferOne[i]);
}
}


/* Calculate average ADC data value in uV */
average = 0;
uint8_t * buffer = (uint8_t *) malloc(TEMP_BUF_SIZE);
for (i = 0; i < ADCSAMPLESIZE; i++) {
average += outputBuffer[i];
}
average = average/ADCSAMPLESIZE;
average=average/1000;
Display_printf(display, 0, 0, "CONFIG_ADC_0 raw result: %d\n", average);
Display_printf(display, 0, 0, "CONFIG_ADC_0 raw result: %d\n", count);

gpio_status=GPIO_read(CAL_JUMPER);
if (gpio_status==0){
// calibration_process(average);
average=0;
}

else{
calculated_average=2713; //default cal value
if(average>calculated_average){
if (zclSampleWarningDevice_ZoneStatus==1){
gaschange_SendChangeNotification();
}
// Display_printf(display, 0, 0, "10% aleart");
alarm_condition++;
LED_write(gas10LedHandle,FALSE);
LED_write(gas7LedHandle,FALSE);
LED_write(gas5LedHandle,FALSE);
LED_write(gas25LedHandle,FALSE);
LED_write(gasLedHandle,FALSE);
LED_startBlinking(buzzerLedHandle,1000,LED_BLINK_FOREVER);

}
else if(average>=(calculated_average*0.7))
{
if (zclSampleWarningDevice_ZoneStatus==1){
gaschange_SendChangeNotification();
}
// Display_printf(display, 0, 0, "7% aleart");
alarm_condition++;
LED_write(gas7LedHandle,FALSE);
LED_write(gas5LedHandle,FALSE);
LED_write(gas25LedHandle,FALSE);
LED_write(gasLedHandle,FALSE);
LED_startBlinking(buzzerLedHandle,1000,LED_BLINK_FOREVER);

}

else if(average>=(calculated_average*0.5))
{
if (zclSampleWarningDevice_ZoneStatus==1){
gaschange_SendChangeNotification();
}
// Display_printf(display, 0, 0, "5% aleart");


alarm_condition++;
LED_write(gas5LedHandle,FALSE);
LED_write(gas25LedHandle,FALSE);
LED_startBlinking(buzzerLedHandle,1000,LED_BLINK_FOREVER);
}
else if(average>=(calculated_average*0.25))
{
// Display_printf(display, 0, 0, "2.5% aleart");
alarm_condition++;
LED_write(gas25LedHandle,FALSE);
}
else{
if (alarm_condition!=0){
gaschange_SendChangeNotification();
alarm_condition=0;

}

// default_led_pattern();
}

count++;
}
}

/*******************************************************************************
* @fn Temperature sensor adc read
*
* @brief get NTC temp using adc
*
* @param none
*
* @return none
*/
void Temperature_sensor()
{
uint16_t i;
ADC_Handle adc;
ADC_Params params;
int_fast16_t res;

ADC_Params_init(&params);
adc = ADC_open(TEMP_ADC, &params);

if (adc == NULL) {
while (1);
}

for (i = 0; i < ADCSAMPLESIZE; i++) {
res = ADC_convert(adc, &TempsampleBufferOne[i]);

if (res == ADC_STATUS_SUCCESS) {

TempoutputBuffer[i] = ADC_convertRawToMicroVolts(adc, TempsampleBufferOne[i]);
}
}


/* Calculate average ADC data value in uV */
Temperature = 0;
for (i = 0; i < ADCSAMPLESIZE; i++) {
Temperature += TempoutputBuffer[i];
}
Temperature = Temperature/ADCSAMPLESIZE;
Temperature=Temperature/1000; //convert to mV
calculated_average=0;
if (Temperature>calculated_average){
if (zclSampleWarningDevice_ZoneStatus==0){

LED_setOn(gas10LedHandle,100);
LED_setOn(gas7LedHandle,100);
LED_setOn(gas5LedHandle,100);
LED_setOn(gas25LedHandle,100);
Temp_SendChangeNotification();
Temp++;

//zclSampleWarningDevice_UpdateStatusLine();
}

}
else{
if (Temp!=0){
Temp_SendChangeNotification();
Temp=0;
//zclSampleWarningDevice_UpdateStatusLine();
}
LED_setOff(gas10LedHandle);
LED_setOff(gas7LedHandle);
LED_setOff(gas5LedHandle);
LED_setOff(gas25LedHandle);


}

ADC_close(adc);

}

/*******************************************************************************
* @fn Temp_SendChangeNotification
*
* @brief
*
* @param
*
* @return none
*/


static void Temp_SendChangeNotification(void)
{
uint8_t extendedStatus = 0;
uint16_t delay = 0;

zstack_getZCLFrameCounterRsp_t Rsp;
uint8_t disableDefaultRsp = TRUE;

// Using this as the "Alarm Switch"
//Toggle the zone status attrib with button press
zclSampleWarningDevice_ZoneStatus ^= (SS_IAS_ZONE_STATUS_ALARM2_ALARMED-1);

//get the appropiate sequence number
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);

//generates a Zone Status Change Notification Command
zclSS_IAS_Send_ZoneStatusChangeNotificationCmd(SAMPLEWARNINGDEVICE_ENDPOINT,
&zclSampleWarningDevice_DstAddr,
zclSampleWarningDevice_ZoneStatus, extendedStatus, zclSampleWarningDevice_ZoneId,delay,
disableDefaultRsp, Rsp.zclFrameCounter );


}

/*******************************************************************************
* @fn Test_SendChangeNotification
*
* @brief
*
* @param
*
* @return none
*/
static void Test_SendChangeNotification(void)
{
uint8_t extendedStatus = 0;
uint16_t delay = 0;

zstack_getZCLFrameCounterRsp_t Rsp;
uint8_t disableDefaultRsp = TRUE;

// Using this as the "Alarm Switch"
//Toggle the zone status attrib with button press
zclSampleWarningDevice_ZoneStatus ^= (SS_IAS_ZONE_STATUS_TEST-0xFF);

//get the appropiate sequence number
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);

//generates a Zone Status Change Notification Command
zclSS_IAS_Send_ZoneStatusChangeNotificationCmd(SAMPLEWARNINGDEVICE_ENDPOINT,
&zclSampleWarningDevice_DstAddr,
zclSampleWarningDevice_ZoneStatus, extendedStatus, zclSampleWarningDevice_ZoneId,delay,
disableDefaultRsp, Rsp.zclFrameCounter );

}

/*******************************************************************************
* @fn gaschange_SendChangeNotification
*
* @brief
*
* @param
*
* @return none
*/
static void gaschange_SendChangeNotification(void)
{
uint8_t extendedStatus = 0;
uint16_t delay = 0;

zstack_getZCLFrameCounterRsp_t Rsp;
uint8_t disableDefaultRsp = TRUE;

// Using this as the "Alarm Switch"
//Toggle the zone status attrib with button press
zclSampleWarningDevice_ZoneStatus ^= SS_IAS_ZONE_STATUS_ALARM1_ALARMED;

//get the appropiate sequence number
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);

//generates a Zone Status Change Notification Command
zclSS_IAS_Send_ZoneStatusChangeNotificationCmd(SAMPLEWARNINGDEVICE_ENDPOINT,
&zclSampleWarningDevice_DstAddr,
zclSampleWarningDevice_ZoneStatus, extendedStatus, zclSampleWarningDevice_ZoneId,delay,
disableDefaultRsp, Rsp.zclFrameCounter );

}


/*******************************************************************************
* @fn zclSampleWarningDevice_process_loop
*
* @brief Application task processing start.
*
* @param none
*
* @return void
*/
static void zclSampleWarningDevice_process_loop(void)
{
uint32_t i=0;
/* Forever loop */
for(;;)
{
zstackmsg_genericReq_t *pMsg = NULL;
bool msgProcessed = FALSE;
Display_printf(display, 0, 0, "Task events: %x\n", appServiceTaskEvents);
/* Wait for response message */
if(Semaphore_pend(appSemHandle, BIOS_WAIT_FOREVER ))
{
// /* Retrieve the response message */
if( (pMsg = (zstackmsg_genericReq_t*) OsalPort_msgReceive( appServiceTaskId )) != NULL)
{
/* Process the message from the stack */
zclSampleWarningDevice_processZStackMsgs(pMsg);
// Free any separately allocated memory
msgProcessed = Zstackapi_freeIndMsg(pMsg);
}

if((msgProcessed == FALSE) && (pMsg != NULL))
{
OsalPort_msgDeallocate((uint8_t*)pMsg);
}


#ifndef CUI_DISABLE
//Process the events that the UI may have
zclsampleApp_ui_event_loop();
#endif

if((appServiceTaskEvents & SAMPLEAPP_AUTO_BINDING_EVT)) //5 min
// &&(seconds_reporting<=600)
{
zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
Display_printf(display, 0, 0, "*******In loop of auto binding event *******\n");
zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_STEERING | BDB_COMMISSIONING_MODE_FINDING_BINDING;
Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
appServiceTaskEvents &= ~SAMPLEAPP_AUTO_BINDING_EVT;
Display_printf(display, 0, 0, "iteration: %d\n", i);
i++;
}
if((appServiceTaskEvents & SAMPLEAPP_AUTO_BINDING_STOP_EVT)) //5min

{
if(UtilTimer_isActive(&AutobindingReqClkStruct)==true) {
UtilTimer_stop(&AutobindingReqClkStruct);
}
Display_printf(display, 0, 0, "*************************Stop the timer***************\n");
// UtilTimer_stop( &AutobindingReqClkStruct );
UtilTimer_stop( &AutobindingstopClkStruct );
appServiceTaskEvents &= ~SAMPLEAPP_AUTO_BINDING_STOP_EVT;
}
if(appServiceTaskEvents==0) //5min

{
appServiceTaskEvents=0x8000;
}
if(appServiceTaskEvents & SAMPLEAPP_WRITE_TO_CIE_DONE_EVT)
{
zstack_zdoSetBindUnbindAuthAddr_t zstack_zdoSetBindUnbindAuthAddr;

//Set that the only remote device that can modify binds to the ZONE cluster is the CIE
OsalPort_memcpy(zstack_zdoSetBindUnbindAuthAddr.AuthAddress, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
zstack_zdoSetBindUnbindAuthAddr.Endpoint = SAMPLEWARNINGDEVICE_ENDPOINT;
zstack_zdoSetBindUnbindAuthAddr.ClusterId = ZCL_CLUSTER_ID_SS_IAS_ZONE;
Zstackapi_ZdoSetBindUnbindAuthAddrReq(appServiceTaskId, &zstack_zdoSetBindUnbindAuthAddr);

#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif

//save in nv the CIE Address
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_CIE_ADDRESS_NV_SUBID, sizeof(zclSampleWarningDevice_CIE_Address),zclSampleWarningDevice_CIE_Address);

appServiceTaskEvents &= ~SAMPLEAPP_WRITE_TO_CIE_DONE_EVT;
}


#if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE)
if(appServiceTaskEvents & SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT)
{
if(zgGP_ProxyCommissioningMode == TRUE)
{
zcl_gpSendCommissioningNotification();
}
else
{
zcl_gpSendNotification();
}
appServiceTaskEvents &= ~SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT;
}

if(appServiceTaskEvents & SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT)
{
gp_expireDuplicateFiltering();
appServiceTaskEvents &= ~SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT;
}

if(appServiceTaskEvents & SAMPLEAPP_PROCESS_GP_TEMP_MASTER_EVT)
{
gp_returnOperationalChannel();
appServiceTaskEvents &= ~SAMPLEAPP_PROCESS_GP_TEMP_MASTER_EVT;
}
#endif

#if ZG_BUILD_ENDDEVICE_TYPE
if ( appServiceTaskEvents & SAMPLEAPP_END_DEVICE_REJOIN_EVT )
{
zstack_bdbZedAttemptRecoverNwkRsp_t zstack_bdbZedAttemptRecoverNwkRsp;

Zstackapi_bdbZedAttemptRecoverNwkReq(appServiceTaskId,&zstack_bdbZedAttemptRecoverNwkRsp);

appServiceTaskEvents &= ~SAMPLEAPP_END_DEVICE_REJOIN_EVT;
}
#endif

if( appServiceTaskEvents & SAMPLEAPP_AUTO_ENROLL_REQ_EVT )
{
zclSampleWarningDevice_SendEnrollReqToCIE();

appServiceTaskEvents &= ~SAMPLEAPP_AUTO_ENROLL_REQ_EVT;
}
if( appServiceTaskEvents & SAMPLEAPP_WARNING_DURATION_EVT )
{
tempWarningInProgress = FALSE;
//Only if there is no fire in the local device
// if(zclSampleWarningDevice_ZoneStatus == 0)
// {
// LED_stopBlinking(gRedLedHandle);
// LED_setOff(gRedLedHandle);
// }
#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif
appServiceTaskEvents &= ~SAMPLEAPP_WARNING_DURATION_EVT;
}

if( appServiceTaskEvents & SAMPLEAPP_SQUAWK_UI_TIMEOUT_EVT)
{
gSquawkReq = FALSE;
#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif
appServiceTaskEvents &= ~SAMPLEAPP_SQUAWK_UI_TIMEOUT_EVT;
}

}
// else{
// Gas_sensor();
// }
}


}


/*******************************************************************************
* @fn zclSampleLight_processZStackMsgs
*
* @brief Process event from Stack
*
* @param pMsg - pointer to incoming ZStack message to process
*
* @return void
*/
static void zclSampleWarningDevice_processZStackMsgs(zstackmsg_genericReq_t *pMsg)
{
switch(pMsg->hdr.event)
{
case zstackmsg_CmdIDs_BDB_NOTIFICATION:
{
zstackmsg_bdbNotificationInd_t *pInd;
pInd = (zstackmsg_bdbNotificationInd_t*)pMsg;
zclSampleWarningDevice_ProcessCommissioningStatus(&(pInd->Req));
}
break;

case zstackmsg_CmdIDs_BDB_IDENTIFY_TIME_CB:
{
#ifndef CUI_DISABLE
zstackmsg_bdbIdentifyTimeoutInd_t *pInd;
pInd = (zstackmsg_bdbIdentifyTimeoutInd_t*) pMsg;
uiProcessIdentifyTimeChange(&(pInd->EndPoint));
#endif
}
break;

case zstackmsg_CmdIDs_BDB_BIND_NOTIFICATION_CB:
{
#ifndef CUI_DISABLE
zstackmsg_bdbBindNotificationInd_t *pInd;
pInd = (zstackmsg_bdbBindNotificationInd_t*) pMsg;
uiProcessBindNotification(&(pInd->Req));
#endif
}
break;

case zstackmsg_CmdIDs_AF_INCOMING_MSG_IND:
{
// Process incoming data messages
zstackmsg_afIncomingMsgInd_t *pInd;
pInd = (zstackmsg_afIncomingMsgInd_t *)pMsg;
zclSampleWarningDevice_processAfIncomingMsgInd( &(pInd->req) );
}
break;


#if (ZG_BUILD_JOINING_TYPE)
case zstackmsg_CmdIDs_BDB_CBKE_TC_LINK_KEY_EXCHANGE_IND:
{
zstack_bdbCBKETCLinkKeyExchangeAttemptReq_t zstack_bdbCBKETCLinkKeyExchangeAttemptReq;
/* Z3.0 has not defined CBKE yet, so lets attempt default TC Link Key exchange procedure
* by reporting CBKE failure.
*/

zstack_bdbCBKETCLinkKeyExchangeAttemptReq.didSuccess = FALSE;

Zstackapi_bdbCBKETCLinkKeyExchangeAttemptReq(appServiceTaskId,
&zstack_bdbCBKETCLinkKeyExchangeAttemptReq);
}
break;

case zstackmsg_CmdIDs_BDB_FILTER_NWK_DESCRIPTOR_IND:

/* User logic to remove networks that do not want to join
* Networks to be removed can be released with Zstackapi_bdbNwkDescFreeReq
*/

Zstackapi_bdbFilterNwkDescComplete(appServiceTaskId);
break;

#endif
case zstackmsg_CmdIDs_DEV_STATE_CHANGE_IND:
{
#ifndef CUI_DISABLE
// The ZStack Thread is indicating a State change
zstackmsg_devStateChangeInd_t *pInd =
(zstackmsg_devStateChangeInd_t *)pMsg;
UI_DeviceStateUpdated(&(pInd->req));
#endif
}
break;

/*
* These are messages/indications from ZStack that this
* application doesn't process. These message can be
* processed by your application, remove from this list and
* process them here in this switch statement.
*/

#if !defined (DISABLE_GREENPOWER_BASIC_PROXY) && (ZG_BUILD_RTR_TYPE)
case zstackmsg_CmdIDs_GP_DATA_IND:
{
zstackmsg_gpDataInd_t *pInd;
pInd = (zstackmsg_gpDataInd_t*)pMsg;
gp_processDataIndMsg( &(pInd->Req) );
}
break;

case zstackmsg_CmdIDs_GP_SECURITY_REQ:
{
zstackmsg_gpSecReq_t *pInd;
pInd = (zstackmsg_gpSecReq_t*)pMsg;
gp_processSecRecMsg( &(pInd->Req) );
}
break;

case zstackmsg_CmdIDs_GP_CHECK_ANNCE:
{
zstackmsg_gpCheckAnnounce_t *pInd;
pInd = (zstackmsg_gpCheckAnnounce_t*)pMsg;
gp_processCheckAnnceMsg( &(pInd->Req) );
}
break;

case zstackmsg_CmdIDs_GP_COMMISSIONING_MODE_IND:
{
#ifndef CUI_DISABLE
zstackmsg_gpCommissioningModeInd_t *pInd;
pInd = (zstackmsg_gpCommissioningModeInd_t*)pMsg;
UI_SetGPPCommissioningMode( &(pInd->Req) );
#endif
}
break;
#endif

#ifdef BDB_TL_TARGET
case zstackmsg_CmdIDs_BDB_TOUCHLINK_TARGET_ENABLE_IND:
{
zstackmsg_bdbTouchLinkTargetEnableInd_t *pInd =
(zstackmsg_bdbTouchLinkTargetEnableInd_t*)pMsg;

uiProcessTouchlinkTargetEnable(&(pInd->req));
}
break;
#endif
case zstackmsg_CmdIDs_BDB_TC_LINK_KEY_EXCHANGE_NOTIFICATION_IND:
case zstackmsg_CmdIDs_AF_DATA_CONFIRM_IND:
case zstackmsg_CmdIDs_ZDO_DEVICE_ANNOUNCE:
case zstackmsg_CmdIDs_ZDO_NWK_ADDR_RSP:
case zstackmsg_CmdIDs_DEV_PERMIT_JOIN_IND:
case zstackmsg_CmdIDs_ZDO_IEEE_ADDR_RSP:
case zstackmsg_CmdIDs_ZDO_NODE_DESC_RSP:
case zstackmsg_CmdIDs_ZDO_POWER_DESC_RSP:
case zstackmsg_CmdIDs_ZDO_SIMPLE_DESC_RSP:
case zstackmsg_CmdIDs_ZDO_ACTIVE_EP_RSP:
case zstackmsg_CmdIDs_ZDO_COMPLEX_DESC_RSP:
case zstackmsg_CmdIDs_ZDO_USER_DESC_RSP:
case zstackmsg_CmdIDs_ZDO_USER_DESC_SET_RSP:
case zstackmsg_CmdIDs_ZDO_SERVER_DISC_RSP:
case zstackmsg_CmdIDs_ZDO_END_DEVICE_BIND_RSP:
case zstackmsg_CmdIDs_ZDO_BIND_RSP:
case zstackmsg_CmdIDs_ZDO_UNBIND_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_NWK_DISC_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_LQI_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_RTG_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_BIND_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_LEAVE_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_DIRECT_JOIN_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_PERMIT_JOIN_RSP:
case zstackmsg_CmdIDs_ZDO_MGMT_NWK_UPDATE_NOTIFY:
case zstackmsg_CmdIDs_ZDO_SRC_RTG_IND:
case zstackmsg_CmdIDs_ZDO_CONCENTRATOR_IND:
case zstackmsg_CmdIDs_ZDO_LEAVE_CNF:
case zstackmsg_CmdIDs_ZDO_LEAVE_IND:
case zstackmsg_CmdIDs_SYS_RESET_IND:
case zstackmsg_CmdIDs_AF_REFLECT_ERROR_IND:
case zstackmsg_CmdIDs_ZDO_TC_DEVICE_IND:
break;

default:
break;
}

}

/*******************************************************************************
*
* @fn zclSampleWarningDevice_processAfIncomingMsgInd
*
* @brief Process AF Incoming Message Indication message
*
* @param pInMsg - pointer to incoming message
*
* @return none
*
*/
static void zclSampleWarningDevice_processAfIncomingMsgInd(zstack_afIncomingMsgInd_t *pInMsg)
{
afIncomingMSGPacket_t afMsg;

/*
* All incoming messages are passed to the ZCL message processor,
* first convert to a structure that ZCL can process.
*/
afMsg.groupId = pInMsg->groupID;
afMsg.clusterId = pInMsg->clusterId;
afMsg.srcAddr.endPoint = pInMsg->srcAddr.endpoint;
afMsg.srcAddr.panId = pInMsg->srcAddr.panID;
afMsg.srcAddr.addrMode = (afAddrMode_t)pInMsg->srcAddr.addrMode;
if( (afMsg.srcAddr.addrMode == afAddr16Bit)
|| (afMsg.srcAddr.addrMode == afAddrGroup)
|| (afMsg.srcAddr.addrMode == afAddrBroadcast) )
{
afMsg.srcAddr.addr.shortAddr = pInMsg->srcAddr.addr.shortAddr;
}
else if(afMsg.srcAddr.addrMode == afAddr64Bit)
{
OsalPort_memcpy(afMsg.srcAddr.addr.extAddr, &(pInMsg->srcAddr.addr.extAddr), 8);
}
afMsg.macDestAddr = pInMsg->macDestAddr;
afMsg.endPoint = pInMsg->endpoint;
afMsg.wasBroadcast = pInMsg->wasBroadcast;
afMsg.LinkQuality = pInMsg->linkQuality;
afMsg.correlation = pInMsg->correlation;
afMsg.rssi = pInMsg->rssi;
afMsg.SecurityUse = pInMsg->securityUse;
afMsg.timestamp = pInMsg->timestamp;
afMsg.nwkSeqNum = pInMsg->nwkSeqNum;
afMsg.macSrcAddr = pInMsg->macSrcAddr;
afMsg.radius = pInMsg->radius;
afMsg.cmd.DataLength = pInMsg->n_payload;
afMsg.cmd.Data = pInMsg->pPayload;

zcl_ProcessMessageMSG(&afMsg);
}


#ifndef CUI_DISABLE
/*********************************************************************
* @fn zclSampleWarningDevice_processKey
*
* @brief Key event handler function
*
* @param key - key to handle action for
* buttonEvents - event to handle action for
*
* @return none
*/
static void zclSampleWarningDevice_processKey(uint8_t key, Button_EventMask buttonEvents)
{
if (buttonEvents & Button_EV_CLICKED)
{
if(key == CONFIG_BTN_LEFT)
{
zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;

zstack_bdbStartCommissioningReq.commissioning_mode = zclSampleWarningDevice_BdbCommissioningModes;
Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
}
if(key == CONFIG_BTN_RIGHT)
{
if(zclSampleWarningDevice_ZoneState == SS_IAS_ZONE_STATE_ENROLLED)
{
zclSampleWarningDevice_SendChangeNotification();
}
else
{
//Try Trip-To-Pair enrollment
zclSampleWarningDevice_SendEnrollReqToCIE();
}
}
}
}
#endif

/*********************************************************************
* @fn zclSampleWarningDevice_ProcessCommissioningStatus
*
* @brief Callback in which the status of the commissioning process are reported
*
* @param bdbCommissioningModeMsg - Context message of the status of a commissioning process
*
* @return none
*/
static void zclSampleWarningDevice_ProcessCommissioningStatus(bdbCommissioningModeMsg_t *bdbCommissioningModeMsg)
{
switch(bdbCommissioningModeMsg->bdbCommissioningMode)
{
case BDB_COMMISSIONING_FORMATION:
if(bdbCommissioningModeMsg->bdbCommissioningStatus == BDB_COMMISSIONING_SUCCESS)
{
//YOUR JOB:
}
else
{
//Want to try other channels?
//try with bdb_setChannelAttribute
}
break;
case BDB_COMMISSIONING_NWK_STEERING:
if(bdbCommissioningModeMsg->bdbCommissioningStatus == BDB_COMMISSIONING_SUCCESS)
{
//YOUR JOB:
//We are on the nwk, what now?
#if ZG_BUILD_ENDDEVICE_TYPE
// speed up polling until zone enrollment has occured
zstack_sysConfigWriteReq_t writeReq = { 0 };
writeReq.has_pollRate = true;
writeReq.pollRate = 500;
writeReq.pollRateType = POLL_RATE_TYPE_APP_1;
Zstackapi_sysConfigWriteReq(appServiceTaskId, &writeReq);
#endif
}
else
{
//See the possible errors for nwk steering procedure
//No suitable networks found
//Want to try other channels?
//try with bdb_setChannelAttribute
}
break;
case BDB_COMMISSIONING_FINDING_BINDING:
if(bdbCommissioningModeMsg->bdbCommissioningStatus == BDB_COMMISSIONING_SUCCESS)
{
//YOUR JOB:
}
else
{
//YOUR JOB:
//retry?, wait for user interaction?
}
break;
case BDB_COMMISSIONING_INITIALIZATION:
//Initialization notification can only be successful. Failure on initialization
//only happens for ZED and is notified as BDB_COMMISSIONING_PARENT_LOST notification

//YOUR JOB:
//We are on a network, what now?

break;
#if ZG_BUILD_ENDDEVICE_TYPE
case BDB_COMMISSIONING_PARENT_LOST:
if(bdbCommissioningModeMsg->bdbCommissioningStatus == BDB_COMMISSIONING_NETWORK_RESTORED)
{
//We did recover from losing parent
}
else
{
//Parent not found, attempt to rejoin again after a fixed delay
UtilTimer_setTimeout( EndDeviceRejoinClkHandle, SAMPLEAPP_END_DEVICE_REJOIN_DELAY );
UtilTimer_start(&EndDeviceRejoinClkStruct);
}
break;
#endif
}

#ifndef CUI_DISABLE
UI_UpdateBdbStatusLine(bdbCommissioningModeMsg);
#endif
}


/*********************************************************************
* @fn zclSampleWarningDevice_BasicResetCB
*
* @brief Callback from the ZCL General Cluster Library
* to set all the Basic Cluster attributes to default values.
*
* @param none
*
* @return none
*/
static void zclSampleWarningDevice_BasicResetCB( void )
{
zclSampleWarningDevice_ResetAttributesToDefaultValues();

//Update the attributes in Nv
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_CIE_ADDRESS_NV_SUBID, sizeof(zclSampleWarningDevice_CIE_Address),zclSampleWarningDevice_CIE_Address);
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_ID_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneId),&zclSampleWarningDevice_ZoneId);
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_STATE_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneState),&zclSampleWarningDevice_ZoneState);

// update the display
#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine( );
#endif
}


#ifndef CUI_DISABLE
static void zclSampleWarningDevice_InitializeStatusLine(CUI_clientHandle_t gCuiHandle)
{
/* Request Async Line for Light application Info */
CUI_statusLineResourceRequest(gCuiHandle, " APP Info"CUI_DEBUG_MSG_START"1"CUI_DEBUG_MSG_END, false, &gSampleWarningDeviceInfoLine1);
CUI_statusLineResourceRequest(gCuiHandle, " APP Info"CUI_DEBUG_MSG_START"2"CUI_DEBUG_MSG_END, false, &gSampleWarningDeviceInfoLine2);
CUI_statusLineResourceRequest(gCuiHandle, " APP Info"CUI_DEBUG_MSG_START"3"CUI_DEBUG_MSG_END, false, &gSampleWarningDeviceInfoLine3);

zclSampleWarningDevice_UpdateStatusLine();
}


static void zclSampleWarningDevice_UpdateStatusLine(void)
{
char lineFormat1[MAX_STATUS_LINE_VALUE_LEN] = {'\0'};
char lineFormat2[MAX_STATUS_LINE_VALUE_LEN] = {'\0'};
char lineFormat3[MAX_STATUS_LINE_VALUE_LEN] = {'\0'};
char StrCIEAddr[17];
char StrzoneId[3];

strcpy(lineFormat1, "["CUI_COLOR_YELLOW"CIE Address"CUI_COLOR_RESET"] ");

//Copy the CIE address
ArrayToString(zclSampleWarningDevice_CIE_Address, StrCIEAddr,16, FALSE);
StrCIEAddr[16] = 0;
strcat(lineFormat1,StrCIEAddr);


//Indicate the Zone ID
strcat(lineFormat1, " ["CUI_COLOR_YELLOW"Zone Id"CUI_COLOR_RESET"] 0x");
ArrayToString(&zclSampleWarningDevice_ZoneId,StrzoneId,2,FALSE);
StrzoneId[2] = 0;
strcat(lineFormat1,StrzoneId);

//Indicate Zone enrollment status
strcat(lineFormat2, "["CUI_COLOR_YELLOW"Zone Enrolled"CUI_COLOR_RESET"] ");
if(zclSampleWarningDevice_ZoneState == SS_IAS_ZONE_STATE_ENROLLED)
{
strcat(lineFormat2, "Yes");
}
else
{
strcat(lineFormat2, "No");
}

strcat(lineFormat2, " ["CUI_COLOR_YELLOW"Zone Type"CUI_COLOR_RESET"] Fire detector");

//Indicate if Zone is alarmed
strcat(lineFormat2, " ["CUI_COLOR_YELLOW"Zone Alarmed"CUI_COLOR_RESET"] ");
if(zclSampleWarningDevice_ZoneStatus & SS_IAS_ZONE_STATUS_ALARM1_ALARMED)
{
strcat(lineFormat2, "Yes");
}
else
{
strcat(lineFormat2, "No");
}

//Indicate if Strobe is alarmed
strcat(lineFormat3, "["CUI_COLOR_YELLOW"Strobe Alarmed"CUI_COLOR_RESET"] ");
if(tempWarningInProgress)
{
strcat(lineFormat3, "Yes");
}
else
{
strcat(lineFormat3, "No");
}

if(gSquawkReq)
{
strcat(lineFormat3, " "CUI_COLOR_MAGENTA"SQUAWK!!!"CUI_COLOR_RESET);
UtilTimer_stop( &SquawkClkStruct );
UtilTimer_setTimeout( SquawkClkHandle, SAMPLEAPP_SQUAWK_UI_TIMEOUT );
UtilTimer_start( &SquawkClkStruct );
}

CUI_statusLinePrintf(gCuiHandle, gSampleWarningDeviceInfoLine1, lineFormat1);
CUI_statusLinePrintf(gCuiHandle, gSampleWarningDeviceInfoLine2, lineFormat2);
CUI_statusLinePrintf(gCuiHandle, gSampleWarningDeviceInfoLine3, lineFormat3);
}

#endif

/******************************************************************************
*
* Functions for processing ZCL Foundation incoming Command/Response messages
*
*****************************************************************************/

/*********************************************************************
* @fn zclSampleWarningDevice_ProcessIncomingMsg
*
* @brief Process ZCL Foundation incoming message
*
* @param pInMsg - pointer to the received message
*
* @return uint8_t - TRUE if got handled
*/
static uint8_t zclSampleWarningDevice_ProcessIncomingMsg( zclIncoming_t *pInMsg )
{
uint8_t handled = FALSE;

switch ( pInMsg->hdr.commandID )
{
#ifdef ZCL_READ
case ZCL_CMD_READ_RSP:
zclSampleWarningDevice_ProcessInReadRspCmd( pInMsg );
handled = TRUE;
break;
#endif
#ifdef ZCL_WRITE
case ZCL_CMD_WRITE_RSP:
zclSampleWarningDevice_ProcessInWriteRspCmd( pInMsg );
handled = TRUE;
break;
#endif
#ifdef ZCL_REPORT
// See ZCL Test Applicaiton (zcl_testapp.c) for sample code on Attribute Reporting
case ZCL_CMD_CONFIG_REPORT:
//zclSampleWarningDevice_ProcessInConfigReportCmd( pInMsg );
break;

case ZCL_CMD_CONFIG_REPORT_RSP:
//zclSampleWarningDevice_ProcessInConfigReportRspCmd( pInMsg );
break;

case ZCL_CMD_READ_REPORT_CFG:
//zclSampleWarningDevice_ProcessInReadReportCfgCmd( pInMsg );
break;

case ZCL_CMD_READ_REPORT_CFG_RSP:
//zclSampleWarningDevice_ProcessInReadReportCfgRspCmd( pInMsg );
break;

case ZCL_CMD_REPORT:
//zclSampleWarningDevice_ProcessInReportCmd( pInMsg );
break;
#endif
case ZCL_CMD_DEFAULT_RSP:
zclSampleWarningDevice_ProcessInDefaultRspCmd( pInMsg );
handled = TRUE;
break;
#ifdef ZCL_DISCOVER
case ZCL_CMD_DISCOVER_CMDS_RECEIVED_RSP:
zclSampleWarningDevice_ProcessInDiscCmdsRspCmd( pInMsg );
handled = TRUE;
break;

case ZCL_CMD_DISCOVER_CMDS_GEN_RSP:
zclSampleWarningDevice_ProcessInDiscCmdsRspCmd( pInMsg );
handled = TRUE;
break;

case ZCL_CMD_DISCOVER_ATTRS_RSP:
zclSampleWarningDevice_ProcessInDiscAttrsRspCmd( pInMsg );
handled = TRUE;
break;

case ZCL_CMD_DISCOVER_ATTRS_EXT_RSP:
zclSampleWarningDevice_ProcessInDiscAttrsExtRspCmd( pInMsg );
handled = TRUE;
break;
#endif
default:
break;
}

return handled;
}

#ifdef ZCL_READ
/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInReadRspCmd
*
* @brief Process the "Profile" Read Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInReadRspCmd( zclIncoming_t *pInMsg )
{
zclReadRspCmd_t *readRspCmd;
uint8_t i;

readRspCmd = (zclReadRspCmd_t *)pInMsg->attrCmd;
for (i = 0; i < readRspCmd->numAttr; i++)
{
// Notify the originator of the results of the original read attributes
// attempt and, for each successfull request, the value of the requested
// attribute
}

return TRUE;
}
#endif // ZCL_READ

#ifdef ZCL_WRITE
/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInWriteRspCmd
*
* @brief Process the "Profile" Write Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInWriteRspCmd( zclIncoming_t *pInMsg )
{
zclWriteRspCmd_t *writeRspCmd;
uint8_t i;

writeRspCmd = (zclWriteRspCmd_t *)pInMsg->attrCmd;
for (i = 0; i < writeRspCmd->numAttr; i++)
{
// Notify the device of the results of the its original write attributes
// command.
}

return TRUE;
}
#endif // ZCL_WRITE

/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInDefaultRspCmd
*
* @brief Process the "Profile" Default Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInDefaultRspCmd( zclIncoming_t *pInMsg )
{
// zclDefaultRspCmd_t *defaultRspCmd = (zclDefaultRspCmd_t *)pInMsg->attrCmd;
// Device is notified of the Default Response command.
(void)pInMsg;
return TRUE;
}

#ifdef ZCL_DISCOVER
/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInDiscCmdsRspCmd
*
* @brief Process the Discover Commands Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInDiscCmdsRspCmd( zclIncoming_t *pInMsg )
{
zclDiscoverCmdsCmdRsp_t *discoverRspCmd;
uint8_t i;

discoverRspCmd = (zclDiscoverCmdsCmdRsp_t *)pInMsg->attrCmd;
for ( i = 0; i < discoverRspCmd->numCmd; i++ )
{
// Device is notified of the result of its attribute discovery command.
}

return TRUE;
}

/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInDiscAttrsRspCmd
*
* @brief Process the "Profile" Discover Attributes Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInDiscAttrsRspCmd( zclIncoming_t *pInMsg )
{
zclDiscoverAttrsRspCmd_t *discoverRspCmd;
uint8_t i;

discoverRspCmd = (zclDiscoverAttrsRspCmd_t *)pInMsg->attrCmd;
for ( i = 0; i < discoverRspCmd->numAttr; i++ )
{
// Device is notified of the result of its attribute discovery command.
}

return TRUE;
}

/*********************************************************************
* @fn zclSampleWarningDevice_ProcessInDiscAttrsExtRspCmd
*
* @brief Process the "Profile" Discover Attributes Extended Response Command
*
* @param pInMsg - incoming message to process
*
* @return none
*/
static uint8_t zclSampleWarningDevice_ProcessInDiscAttrsExtRspCmd( zclIncoming_t *pInMsg )
{
zclDiscoverAttrsExtRsp_t *discoverRspCmd;
uint8_t i;

discoverRspCmd = (zclDiscoverAttrsExtRsp_t *)pInMsg->attrCmd;
for ( i = 0; i < discoverRspCmd->numAttr; i++ )
{
// Device is notified of the result of its attribute discovery command.
}

return TRUE;
}
#endif // ZCL_DISCOVER

#ifdef ZCL_WD
/*********************************************************************
* @fn zclSampleWarningDevice_StartWarningCB
*
* @brief Process in the received StartWarning Command.
*
* @param pCmd - pointer to the incoming command
*
*/
static ZStatus_t zclSampleWarningDevice_StartWarningCB(zclWDStartWarning_t *pCmd)
{
//Only blinks if the alarm is set
if(((zclWDStartWarning_t *)pCmd->warningmessage.warningbits.warnMode != \
SS_IAS_START_WARNING_WARNING_MODE_STOP)
||((zclWDStartWarning_t *)pCmd->warningmessage.warningbits.warnStrobe != \
SS_IAS_START_WARNING_STROBE_NO_STROBE_WARNING))
{
//Only if there is no fire in the local device
if(zclSampleWarningDevice_ZoneStatus == 0)
{
uint32_t timeout;
if(zclSampleWarningDevice_MaxDuration < pCmd->warningDuration)
{
timeout = zclSampleWarningDevice_MaxDuration * 1000;
}
else
{
timeout = pCmd->warningDuration * 1000;
}

//Start the timer to process the warning duration
UtilTimer_setTimeout( WarningDurationClkHandle, timeout );
UtilTimer_start(&WarningDurationClkStruct);

tempWarningInProgress = TRUE;
// LED_stopBlinking(gRedLedHandle);
// LED_setOn(gRedLedHandle, LED_BRIGHTNESS_MAX);
}
}
else //if the alarm is not present
{
tempWarningInProgress = FALSE;

//Only if there is no fire in the local device
// if(zclSampleWarningDevice_ZoneStatus == 0)
// {
// LED_stopBlinking(gRedLedHandle);
// LED_setOff(gRedLedHandle);
// }
}

#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif
return (ZStatus_t)(0) ;

}

/*********************************************************************
* @fn zclSampleWarningDevice_SquawkCB
*
* @brief Process in the received Squawk Command.
*
* @param pCmd - pointer to the incoming command
*
*/
ZStatus_t zclSampleWarningDevice_SquawkCB(zclWDSquawk_t* squawk)
{
zclWDSquawk_t squawks = *squawk;
//Squawk is only valid if there is no warning in progress
if(tempWarningInProgress == 0)
{
if((squawks.squawkbits.squawkMode == SS_IAS_SQUAWK_SQUAWK_MODE_SYSTEM_ALARMED_NOTIFICATION_SOUND)
|| (squawks.squawkbits.strobe == SS_IAS_SQUAWK_STROBE_USE_STROBE_BLINK_IN_PARALLEL_TO_SQUAWK))
{
//Only if there is no fire in the local device
if(zclSampleWarningDevice_ZoneStatus == 0)
{
// LED_startBlinking(gRedLedHandle, 500, 1);
gSquawkReq = TRUE;
}
}
}

#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif

return (ZStatus_t)(0) ;
}
#endif // ZCL_WD

#ifdef ZCL_ZONE
/*******************************************************************************
* @fn static void zclSampleWarningDevice_EnrollResponseCB
*
* @brief Process incoming Enroll Response Command
*
* @param Zone Enroll Response command
*
* @return none
*/
static ZStatus_t zclSampleWarningDevice_EnrollResponseCB(zclZoneEnrollRsp_t *rsp)
{
AddrMgrEntry_t entry;
uint8_t InvalidCIEAddr = true;
uint8_t index;

for(index=0; index < Z_EXTADDR_LEN; index++)
{
if(zclSampleWarningDevice_CIE_Address[index] != 0xFF)
{
InvalidCIEAddr = false;
index = Z_EXTADDR_LEN;
}
}

//if we have a valid CIE Address, check that it comes from CIE
if(!InvalidCIEAddr)
{
entry.user = ADDRMGR_USER_DEFAULT;
entry.nwkAddr = INVALID_NODE_ADDR;
//Get the short address of the CIE if exist
OsalPort_memcpy(entry.extAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
AddrMgrEntryLookupExt(&entry); //AddrMgr stack interface

//if the frame does not comes from CIE, then do not process it
if(entry.nwkAddr != rsp->srcAddr)
{
zstack_zdoNwkAddrReq_t zstack_zdoNwkAddrReq;

OsalPort_memcpy(zstack_zdoNwkAddrReq.ieeeAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
zstack_zdoNwkAddrReq.startIndex = 0;
zstack_zdoNwkAddrReq.type = zstack_NwkAddrReqType_SINGLE_DEVICE;

Zstackapi_ZdoNwkAddrReq(appServiceTaskId, &zstack_zdoNwkAddrReq);

//Maybe CIE changed address due to address conflict?, try to update its address will not hurt.
return ZCL_STATUS_NOT_AUTHORIZED;
}
}

switch(rsp->responseCode)
{
case SS_IAS_ZONE_STATUS_ENROLL_RESPONSE_CODE_SUCCESS:
{
//Must set the Zone State attribute to Enrolled if succesful
zclSampleWarningDevice_ZoneState = SS_IAS_ZONE_STATE_ENROLLED;
zclSampleWarningDevice_ZoneId = rsp->zoneID;

//Save the Zone ID and the enrollment status in Nv
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_ID_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneId),&zclSampleWarningDevice_ZoneId);
zclport_writeNV(IAS_ZONE_NV_ID, IAS_ZONE_ZONE_STATE_NV_SUBID, sizeof(zclSampleWarningDevice_ZoneState),&zclSampleWarningDevice_ZoneState);
#if ZG_BUILD_ENDDEVICE_TYPE
// resume stack poll rate since we have finished zone enrollment
zstack_sysConfigWriteReq_t writeReq = { 0 };
writeReq.has_pollRate = true;
writeReq.pollRate = POLL_RATE_MAX;
writeReq.pollRateType = POLL_RATE_TYPE_APP_1;
Zstackapi_sysConfigWriteReq(appServiceTaskId, &writeReq);
#endif
}
break;

//The rest of the cases indicate that the enrollment was not succesful
//dealt by printing error message
default:
break;
}

#ifndef CUI_DISABLE
zclSampleWarningDevice_UpdateStatusLine();
#endif

return (ZStatus_t)(0) ;
}

/*******************************************************************************
* @fn zclSampleWarningDevice_SendEnrollReqToCIE
*
* @brief Send Enroll Request to CIE if the IEEE address of CIE has been set and local device is not enrolled
*
* @param none
*
* @return none
*/
void zclSampleWarningDevice_SendEnrollReqToCIE(void)
{

uint8_t temp[Z_EXTADDR_LEN] = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF };

zstack_zdoBindReq_t Req;
zstack_sysNwkInfoReadRsp_t Rsp;


Zstackapi_sysNwkInfoReadReq(appServiceTaskId, &Rsp);

//fill in bind request to self
Req.nwkAddr = Rsp.nwkAddr;
OsalPort_memcpy(Req.bindInfo.srcAddr, Rsp.ieeeAddr, Z_EXTADDR_LEN);
Req.bindInfo.dstAddr.addrMode = zstack_AFAddrMode_EXT;
OsalPort_memcpy(Req.bindInfo.dstAddr.addr.extAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
Req.bindInfo.dstAddr.endpoint = tempCIEsrcEndpoint;
Req.bindInfo.clusterID = ZCL_CLUSTER_ID_SS_IAS_ZONE;
Req.bindInfo.srcEndpoint = SAMPLEWARNINGDEVICE_ENDPOINT;

//create the bind to that device
Zstackapi_ZdoBindReq(appServiceTaskId, &Req);

//If we have the IEEE address of the CIE device and is not enrolled, then send enrollment request, otherwise we can't do it
if( memcmp(temp, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN) && (zclSampleWarningDevice_ZoneState == SS_IAS_ZONE_STATE_NOT_ENROLLED))
{
AddrMgrEntry_t entry;

entry.user = ADDRMGR_USER_DEFAULT;
OsalPort_memcpy(entry.extAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
AddrMgrEntryLookupExt(&entry);

if(entry.nwkAddr != INVALID_NODE_ADDR)
{
uint16_t manufacturerCode;
uint8_t disableDefaultRsp = TRUE;
zstack_getZCLFrameCounterRsp_t Rsp;

manufacturerCode = BUILD_UINT16(ZDO_Config_Node_Descriptor.ManufacturerCode[0],ZDO_Config_Node_Descriptor.ManufacturerCode[1]);

//get the appropriate sequence number
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);

//Send enroll request
zclSS_IAS_Send_ZoneStatusEnrollRequestCmd(SAMPLEWARNINGDEVICE_ENDPOINT, &zclSampleWarningDevice_DstAddr,
zclSampleWarningDevice_ZoneType, manufacturerCode,
disableDefaultRsp, Rsp.zclFrameCounter);
}
}

}

/*********************************************************************
* @fn zclSampleWarningDevice_AuthenticateCIE
*
* @brief Authenticate write attribute operation to IAS Zone cluster
*
* @param afAddrType_t *srcAddr - Address of the remote device requesting the operation
* @param zclAttrRec_t *pAttr - Attribute record on which the operation will be performed
* @param uint8_t oper - type of operation (write, read)
* @return none
*/
static uint8_t zclSampleWarningDevice_AuthenticateCIE( afAddrType_t *srcAddr, zclAttrRec_t *pAttr, uint8_t oper )
{
//If it is not write, do not interfere with other operations.
if(oper != ZCL_OPER_WRITE)
{
return ZCL_STATUS_SUCCESS;
}

if(pAttr->clusterID == ZCL_CLUSTER_ID_SS_IAS_ZONE)
{
AddrMgrEntry_t entry;
uint8_t InvalidCIEAddr = true;
uint8_t index;

for(index=0; index < Z_EXTADDR_LEN; index++)
{
if(zclSampleWarningDevice_CIE_Address[index] != 0xFF)
{
InvalidCIEAddr = false;
index = Z_EXTADDR_LEN;
}
}

//if we have a valid CIE Address, check that it comes from CIE
if(!InvalidCIEAddr)
{
entry.user = ADDRMGR_USER_DEFAULT;
entry.nwkAddr = INVALID_NODE_ADDR;
//Get the short address of the CIE if exist
OsalPort_memcpy(entry.extAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
AddrMgrEntryLookupExt(&entry); //AddrMgr stack interface

//if the frame does not comes from CIE, then do not process it
if(entry.nwkAddr != srcAddr->addr.shortAddr)
{
zstack_zdoNwkAddrReq_t zstack_zdoNwkAddrReq;

OsalPort_memcpy(zstack_zdoNwkAddrReq.ieeeAddr, zclSampleWarningDevice_CIE_Address, Z_EXTADDR_LEN);
zstack_zdoNwkAddrReq.startIndex = 0;
zstack_zdoNwkAddrReq.type = zstack_NwkAddrReqType_SINGLE_DEVICE;

//Maybe CIE changed address due to address conflict?, try to update its address will not hurt.
Zstackapi_ZdoNwkAddrReq(appServiceTaskId, &zstack_zdoNwkAddrReq);

return ZCL_STATUS_NOT_AUTHORIZED;
}
}
//Perform Auto-Enroll-Request (if enabled via UI)
else if(pAttr->attr.attrId == ATTRID_SS_IAS_CIE_ADDRESS)
{
tempCIEsrcEndpoint = srcAddr->endPoint;

if(zclSampleWarningDevice_enrollmentMode == AUTO_ENROLL_REQUEST)
{
//Start the timer to send auto enroll request
UtilTimer_setTimeout( AutoEnrollReqClkHandle, SAMPLEAPP_AUTO_ENROLL_REQ_DELAY );
UtilTimer_start( &AutoEnrollReqClkStruct );
}

//Set and event which will be process after write operation takes place.
appServiceTaskEvents |= SAMPLEAPP_WRITE_TO_CIE_DONE_EVT;
// Wake up the application thread when it waits for clock event
Semaphore_post(appSemHandle);
}
}

return ZCL_STATUS_SUCCESS;
}

#ifndef CUI_DISABLE
/*******************************************************************************
* @fn zclSampleWarningDevice_SendChangeNotification
*
* @brief
*
* @param
*
* @return none
*/
static void zclSampleWarningDevice_SendChangeNotification(void)
{
uint8_t extendedStatus = 0;
uint16_t delay = 0;

zstack_getZCLFrameCounterRsp_t Rsp;
uint8_t disableDefaultRsp = TRUE;

// Using this as the "Alarm Switch"
//Toggle the zone status attrib with button press
zclSampleWarningDevice_ZoneStatus ^= SS_IAS_ZONE_STATUS_ALARM1_ALARMED;

//get the appropiate sequence number
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);

//generates a Zone Status Change Notification Command
zclSS_IAS_Send_ZoneStatusChangeNotificationCmd(SAMPLEWARNINGDEVICE_ENDPOINT,
&zclSampleWarningDevice_DstAddr,
zclSampleWarningDevice_ZoneStatus, extendedStatus, zclSampleWarningDevice_ZoneId,delay,
disableDefaultRsp, Rsp.zclFrameCounter );


if(zclSampleWarningDevice_ZoneStatus == SS_IAS_ZONE_STATUS_ALARM1_ALARMED)
{
LED_startBlinking(gRedLedHandle, 500, LED_BLINK_FOREVER);
}
else
{
LED_stopBlinking(gRedLedHandle);
LED_setOff(gRedLedHandle);
}
}

void zclSampleWarningDevice_UiActionSendEnroll(const int32_t _itemEntry)
{
zclSampleWarningDevice_SendEnrollReqToCIE();
zclSampleWarningDevice_UpdateStatusLine();
}

void zclSampleWarningDevice_UiActionToggleAlarm(const int32_t _itemEntry)
{
zclSampleWarningDevice_SendChangeNotification();

if(zclSampleWarningDevice_ZoneStatus == SS_IAS_ZONE_STATUS_ALARM1_ALARMED)
{
LED_startBlinking(gRedLedHandle, 500, LED_BLINK_FOREVER);
}
else
{
LED_stopBlinking(gRedLedHandle);
LED_setOff(gRedLedHandle);
}

zclSampleWarningDevice_UpdateStatusLine();
}

/*********************************************************************
* @fn zclSampleWarningDevice_UiActionChangeEnrollmentMode
*
* @brief Process UART input for device enrollment mode
*
* @param _input - uart key or uart notification
* _pLines - pointers to the buffers to be displayed
* _pCurInfo - pointer to the cursor position. The position is given
* by the length of _pLines and the number of lines.
* If -1,-1 is provided, no pointer is displayed
*
* @return none
*/
void zclSampleWarningDevice_UiActionChangeEnrollmentMode(const char _input, char* _pLines[3], CUI_cursorInfo_t* _pCurInfo)
{
// loop through enrollment modes
if (_input == CUI_INPUT_UP)
{
zclSampleWarningDevice_enrollmentMode =(IAS_Zone_EnrollmentModes_t) \
((uint8_t)(zclSampleWarningDevice_enrollmentMode + 1) %
(uint8_t)ENROLLMENT_MODE_ENUM_LENGTH);
}
else if(_input == CUI_INPUT_DOWN)
{
zclSampleWarningDevice_enrollmentMode = (IAS_Zone_EnrollmentModes_t) \
((uint8_t)(zclSampleWarningDevice_enrollmentMode - 1) %
(uint8_t)ENROLLMENT_MODE_ENUM_LENGTH);
}

switch(zclSampleWarningDevice_enrollmentMode)
{
case TRIP_TO_PAIR:
{
strncpy(_pLines[1], "TRIP-TO-PAIR", MAX_MENU_LINE_LEN);
break;
}
case AUTO_ENROLL_REQUEST:
{
strncpy(_pLines[1], "AUTO ENROLL REQ", MAX_MENU_LINE_LEN);
break;
}
case ENROLLMENT_MODE_ENUM_LENGTH:
default:
break;
}

if (_input != CUI_ITEM_PREVIEW) {
strncpy(_pLines[0], "Up/Down to select:", MAX_MENU_LINE_LEN);
strncpy(_pLines[2], " ENROLLMENT MODE ", MAX_MENU_LINE_LEN);
}
}

/*********************************************************************
* @fn zclSampleWarningDevice_UiActionDiscoverCIE
*
* @brief Process UART input for manual CIE Discovery
*
* @param _input - uart key or uart notification
* _pLines - pointers to the buffers to be displayed
* _pCurInfo - pointer to the cursor position. The position is given
* by the length of _pLines and the number of lines.
* If -1,-1 is provided, no pointer is displayed
*
* @return none
*/
void zclSampleWarningDevice_UiActionDiscoverCIE(const char _input, char* _pLines[3], CUI_cursorInfo_t* _pCurInfo)
{
static uint8_t discoveryEnabled = FALSE;

if (_input == CUI_INPUT_UP || _input == CUI_INPUT_DOWN)
{
discoveryEnabled = !discoveryEnabled;
}

zstack_sysNwkInfoReadRsp_t Rsp;
zstack_getZCLFrameCounterRsp_t zclCounterRsp;
afAddrType_t dstAddr;

Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &zclCounterRsp);

//Get our short address
Zstackapi_sysNwkInfoReadReq(appServiceTaskId, &Rsp);

dstAddr.endPoint = SAMPLEWARNINGDEVICE_ENDPOINT;
dstAddr.addrMode = afAddr16Bit;
dstAddr.addr.shortAddr = Rsp.nwkAddr;

switch(discoveryEnabled)
{
case TRUE:
{
// 0xFFFF = identify forever, until disabled
zclGeneral_SendIdentify(SAMPLEWARNINGDEVICE_ENDPOINT, &dstAddr, 0xFFFF, TRUE, zclCounterRsp.zclFrameCounter);

strncpy(_pLines[1], "ENABLED", MAX_MENU_LINE_LEN);
}
break;
case FALSE:
{
// 0 = stop identifying
zclGeneral_SendIdentify(SAMPLEWARNINGDEVICE_ENDPOINT, &dstAddr, 0, TRUE, zclCounterRsp.zclFrameCounter);

strncpy(_pLines[1], "DISABLED", MAX_MENU_LINE_LEN);
}
break;
}

if (_input != CUI_ITEM_PREVIEW) {
strncpy(_pLines[0], "Up/Down to select:", MAX_MENU_LINE_LEN);
strncpy(_pLines[2], " DISCOVER ZONE ", MAX_MENU_LINE_LEN);
}
}

/*********************************************************************
* @fn ArrayToString
*
* @brief format a memory buffer into a string buffer in hex representation.
*
* @param buf - pointer to a bufer to be formatted
* str - pointer to a buffer to store the formatted string
* num_of_digists - number of digits to include in the formatted string
* big_endian - whether the memory content should be represented as big or little endian
*
* @return none
*/
static void ArrayToString (uint8_t * buf, char * str, uint8_t num_of_digists, bool big_endian)
{
int i;
uint8_t stringIndex;
uint8_t value;

for (i = 0; i < num_of_digists; i++)
{
stringIndex = (big_endian ? i : num_of_digists - 1 - i);
if(big_endian)
{
value = (buf[i / 2] >> (4 * (!(i % 2)))) & 0x0F;
}
else
{
value = (buf[i / 2] >> (4 * (i % 2))) & 0x0F;
}
str[stringIndex] = '0' + value;
if (str[stringIndex] > '9')
{
str[stringIndex] += 'A' - '0' - 10;
}
}
}
#endif // CUI_DISABLE

#endif //ZCL_ZONE

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Chintimani、

    尽管我尚未全面复查您的代码、但我可以告诉 您 zclSampleWarningDevice_processAuto_ADC_readCallback 应该设置一个事件标志、 该事件标志可以处理 来自 zclSampleWarningDevice_Process_loop 的 Gas 传感器、而不是直接处理该事件。  所有初始化也应通过 zclSampleWarningDevice_Init 完成、而不是在 Gas 传感器的每次迭代期间完成、因为 AutogasReqClk 会过期。  我还建议 共享一个 ADC 实例、而不是在 Temperature_sensor 和 Gas 传感器的每次运行之间切换实例、尽管它看起来好像从未引用过 Temperature_sensor。   如果您认为 ADC 的实现存在问题、可以查看 ADC TI 驱动程序示例。  目前、您的开发与源材料存在很大差异、因此很难确定问题所在的位置。  您将需要执行自己 的调试 、也许还需要使用 监听器 来监控无线通信、并在器件停止工作时提供有关器件状态和行为的更多信息。  例如、它是否停留在一个断言内、并且它是否仍然可以在 Zigbee 网络上进行通信?

    此致、
    Ryan