This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] RTOS/CC2630:CC2630复位

Guru**** 2924030 points

Other Parts Discussed in Thread: CC2630

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/764238/rtos-cc2630-cc2630-reset

器件型号:CC2630

工具/软件:TI-RTOS

我们    将 CC2630用作 eLock 项目、使用1.8V 电源。 由于其他电路具有电流消耗、因此我们使用示波器观察到电源电压大约为20微分下拉至大约1.6V、从而导致 CC2630重新启动。 我们采用了三批 CC2630、AZ0R、AI8P 批次不会重新启动、但 AF0H 批次将重新启动。

问题:  

1.希望了解 CC2630屏幕打印上每个字母的含义,如 AF0H。  

2.如何解决重启问题?