This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2652P:直线路由器中的最大跳数

Guru**** 2769075 points

Other Parts Discussed in Thread: CC2652P, SYSCONFIG, Z-STACK

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1178093/cc2652p-maximum-number-of-hops-in-a-straight-line-of-routers

器件型号:CC2652P
Thread 中讨论的其他器件: SysConfigZ-stack

 早上好。

我们将测试一些基于 CC2652P ZNP 协调器的拓扑架构、这些架构连接到一条直线型器件、这些器件由定制路由器和定制终端设备组合而成、每个都具有8个"智能插头"型端点、 用于轮询它们的计量/ONOFF 值并由 ONOFF 命令到达。

我们的应用需要至少30个器件的一些线路、这些器件的间距约为20米、从而最大程度地减少了协调器的数量。 低于这些数字的任何数量的器件都不能证明 Zigbee 不适合使用传统的大 Wi-Fi 网络。

固件是 zr_genericapp 和 zed_genericapp 的变体、手动添加工作端点、群集和属性。

1 -我们首先尝试将一系列20台路由器直接连接到一条直线上,标准间约为20/30米

结果并不是很有希望:首次尝试到第10个节点时、设备的现场配对一直在进行、然后面谈在需要6、7次尝试才能成功结束之前逐渐失败。 然后、轮询器件对于第一个节点运行良好、然后在轮询第12 /第13个及以上器件时导致超时。 因此、我们可以减去最大跳数大约为10 (正如 Ryan 几次之前告诉我的那样)。 是否可以以任何方式递增此数字? 我尝试对默认/ti_zstack_config.h 和 Stack/nwk_globals.h 中的一些旋钮进行调优、但没有区别:

/*
 *                           ti_zstack_config.h
 *
 *  DO NOT EDIT - This file was generated by the SysConfig tool.
 *
 *  Macros used to define a TI Z-Stack ZigBee device. New user defined
 *  options may be added to this file, as necessary.
 *
 */

#ifndef TI_ZSTACK_CONFIG_H
#define TI_ZSTACK_CONFIG_H

/* Default (primary) and secondary channel masks. Secondary mask is used when the
 * default channels fail.
 * Channels are defined in the following:
 *        11 - 26 : 2.4 GHz     0x07FFF800
 */
#ifndef DEFAULT_CHANLIST
#define DEFAULT_CHANLIST              0x04000000
#endif

#ifndef SECONDARY_CHANLIST
#define SECONDARY_CHANLIST            0x00000000
#endif

/* Define the default PAN ID.
 *
 * Setting this to a value other than 0xFFFF causes
 * ZDO_COORD to use this value as its PAN ID and
 * Routers and end devices to join PAN with this ID
 */
#ifndef ZDAPP_CONFIG_PAN_ID
#define ZDAPP_CONFIG_PAN_ID           0xFFFE
#endif

/* Specifiy whether to set the EPID to the Extended Address, or to use the
 * custom Extended Pan ID (EPID) defined by ZDAPP_CONFIG_EPID
 */
#ifndef SET_EPID_AS_EXT_ADDR
#define SET_EPID_AS_EXT_ADDR          TRUE
#endif

/* Define the default Extended Pan ID (EPID)
 * ZDAPP_CONFIG_EPID is only used if SET_EPID_AS_EXT_ADDR is FALSE. Otherwise,
 * the EPID is set to the Extended Address.
 */
#ifndef ZDAPP_CONFIG_EPID
#define ZDAPP_CONFIG_EPID             {0x01,0x23,0x45,0x67,0x89,0xAB,0xCD,0xEF}
#endif

/* in seconds; set to 255 to turn off route expiry */
#ifndef ROUTE_EXPIRY_TIME
#define ROUTE_EXPIRY_TIME             30
#endif

/*  Default indirect message holding timeout value:
 *  1-65535 (0 -> 65536) X CNT_RTG_TIMER X RTG_TIMER_INTERVAL
 */
#ifndef NWK_INDIRECT_MSG_TIMEOUT
#define NWK_INDIRECT_MSG_TIMEOUT      7
#endif

/* The number of simultaneous route discoveries in network */
#ifndef MAX_RREQ_ENTRIES
#define MAX_RREQ_ENTRIES              8
#endif

/* The maximum number of MAC frame transmission attempts allowed */
#ifndef ZMAC_MAX_FRAME_RETRIES
#define ZMAC_MAX_FRAME_RETRIES          3
#endif

/* Max number of times attempts looking for the next hop address of a message */
#ifndef NWK_MAX_DATA_RETRIES
#define NWK_MAX_DATA_RETRIES          2
#endif

/* The maximum number of times APS frames are retried after not receiving an APS ACK */
#ifndef APSC_MAX_FRAME_RETRIES
#define APSC_MAX_FRAME_RETRIES        3
#endif

/* This number is used by polled devices, since the spec'd formula
 * doesn't work for sleeping end devices.  For non-polled devices,
 * a formula is used. Value is in 2 milliseconds periods
 */
#ifndef APSC_ACK_WAIT_DURATION_POLLED
#define APSC_ACK_WAIT_DURATION_POLLED 3000
#endif

/* The maximum number of groups in the groups table */
#ifndef APS_MAX_GROUPS
#define APS_MAX_GROUPS                40
#endif

/* Number of entries in the regular routing table plus additional
 * entries for route repair
 */
#ifndef MAX_RTG_ENTRIES
#define MAX_RTG_ENTRIES               40
#endif

/* Maximum number of entries in the Binding table. */
#ifndef NWK_MAX_BINDING_ENTRIES
#define NWK_MAX_BINDING_ENTRIES       40
#endif

/* Default security key. */
#ifndef DEFAULT_KEY
#define DEFAULT_KEY                   {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}
#endif

/* ZigBee Alliance Pre-configured Distributed Link Key (for Distributed networks) */
#ifndef DISTRIBUTED_GLOBAL_LINK_KEY
#define DISTRIBUTED_GLOBAL_LINK_KEY   {0xD0,0xD1,0xD2,0xD3,0xD4,0xD5,0xD6,0xD7,0xD8,0xD9,0xDA,0xDB,0xDC,0xDD,0xDE,0xDF}
#endif

/* ZigBee Alliance Pre-configured TC Link Key - 'ZigBeeAlliance09' (for Centralized networks) */
#ifndef DEFAULT_TC_LINK_KEY
#define DEFAULT_TC_LINK_KEY           {0x5a,0x69,0x67,0x42,0x65,0x65,0x41,0x6c,0x6c,0x69,0x61,0x6e,0x63,0x65,0x30,0x39}
#endif

/* The number of milliseconds to wait between data request polls to the coordinator. */
#ifndef TXPOWER
#define TXPOWER                     20
#endif

/****************************************
 * The following are for End Devices only
 ***************************************/

/* Determine whether the radio on an End Device is always on */
#ifndef RFD_RX_ALWAYS_ON_CAPABLE
#define RFD_RX_ALWAYS_ON_CAPABLE            TRUE
#endif

#ifndef RFD_RX_ALWAYS_ON
#define RFD_RX_ALWAYS_ON                    TRUE
#endif

/* The minimum poll rate. */
#ifndef MINIMUM_APP_POLL_RATE
#define MINIMUM_APP_POLL_RATE                     100
#endif

/* The number of milliseconds to wait between data request polls to the coordinator. */
#ifndef POLL_RATE
#define POLL_RATE                     3000
#endif

/* This is used after receiving a data indication to poll immediately
 * for queued messages...in milliseconds.
 */
#ifndef QUEUED_POLL_RATE
#define QUEUED_POLL_RATE              100
#endif

/* This is used after receiving a data confirmation to poll immediately
 * for response messages...in milliseconds
 */
#ifndef RESPONSE_POLL_RATE
#define RESPONSE_POLL_RATE            100
#endif

/* This is used as an alternate response poll rate only for rejoin request.
 * This rate is determined by the response time of the parent that the device
 * is trying to join.
 */
#ifndef REJOIN_POLL_RATE
#define REJOIN_POLL_RATE              440
#endif

/* Maximum number of devices in the Assoc/Device list. */
#ifndef NWK_MAX_DEVICE_LIST
#define NWK_MAX_DEVICE_LIST           20
#endif

/* Total Number of APS keys that a TC can manage. This is equal to the number of devices a ZC can allow to join the network */
#ifndef ZDSECMGR_TC_DEVICE_MAX
#define ZDSECMGR_TC_DEVICE_MAX        3
#endif

/* Value used by end device when sending End Device Timeout Request */
/* This is an index into table timeoutValue[] defined in nwk_globals.c */
#ifndef END_DEV_TIMEOUT_VALUE
#define END_DEV_TIMEOUT_VALUE        8
#endif





#endif /* TI_ZSTACK_CONFIG_H */

/**************************************************************************************************
  Filename:       nwk_globals.h
  Revised:        $Date: 2015-01-08 16:32:12 -0800 (Thu, 08 Jan 2015) $
  Revision:       $Revision: 41678 $

  Description:    User definable Network Parameters.


  Copyright 2004-2015 Texas Instruments Incorporated.

  All rights reserved not granted herein.
  Limited License.

  Texas Instruments Incorporated grants a world-wide, royalty-free,
  non-exclusive license under copyrights and patents it now or hereafter
  owns or controls to make, have made, use, import, offer to sell and sell
  ("Utilize") this software subject to the terms herein. With respect to the
  foregoing patent license, such license is granted solely to the extent that
  any such patent is necessary to Utilize the software alone. The patent
  license shall not apply to any combinations which include this software,
  other than combinations with devices manufactured by or for TI ("TI
  Devices"). No hardware patent is licensed hereunder.

  Redistributions must preserve existing copyright notices and reproduce
  this license (including the above copyright notice and the disclaimer and
  (if applicable) source code license limitations below) in the documentation
  and/or other materials provided with the distribution.

  Redistribution and use in binary form, without modification, are permitted
  provided that the following conditions are met:

    * No reverse engineering, decompilation, or disassembly of this software
      is permitted with respect to any software provided in binary form.
    * Any redistribution and use are licensed by TI for use only with TI Devices.
    * Nothing shall obligate TI to provide you with source code for the software
      licensed and provided to you in object code.

  If software source code is provided to you, modification and redistribution
  of the source code are permitted provided that the following conditions are
  met:

    * Any redistribution and use of the source code, including any resulting
      derivative works, are licensed by TI for use only with TI Devices.
    * Any redistribution and use of any object code compiled from the source
      code and any resulting derivative works, are licensed by TI for use
      only with TI Devices.

  Neither the name of Texas Instruments Incorporated nor the names of its
  suppliers may be used to endorse or promote products derived from this
  software without specific prior written permission.

  DISCLAIMER.

  THIS SOFTWARE IS PROVIDED BY TI AND TI'S LICENSORS "AS IS" AND ANY EXPRESS
  OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
  OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
  IN NO EVENT SHALL TI AND TI'S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT,
  INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT
  NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY
  OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING
  NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
**************************************************************************************************/

#ifndef NWK_GLOBALS_H
#define NWK_GLOBALS_H

#ifdef __cplusplus
extern "C" {
#endif

/*********************************************************************
 * INCLUDES
 */

#include "zcomdef.h"
#include "nwk_bufs.h"
#include "assoc_list.h"
#include "binding_table.h"
#include "zglobals.h"

/*********************************************************************
 * MACROS
 */

/*********************************************************************
 * CONSTANTS
 */
#if !defined ( CONFIG_ITEM )
  #define CONFIG_ITEM CONST
#endif

#if !defined ( NWK_LINK_STATUS_PERIOD )
  #define NWK_LINK_STATUS_PERIOD 60       // 15 seconds
#endif
#if !defined ( ZIGBEE_FRAGMENTATION )
  #define ZIGBEE_FRAGMENTATION
#endif

#if ( RFD_RX_ALWAYS_ON_CAPABLE == TRUE ) || ( ZG_BUILD_RTR_TYPE )
  // The PANID Conflict feature is mandatory for both 2007 and 2007 PRO.
  // So, it will be ON all the time (except sleeping end devices).
  #if !defined ( ZIGBEE_PANID_CONFLICT )
    #define ZIGBEE_PANID_CONFLICT
  #endif
#endif

#if ( ZG_BUILD_RTR_TYPE )
  // The Frequency Agility feature is mandatory for both 2007 and 2007 PRO.
  // So, it will be ON all the time for routers.
  #if !defined ( ZIGBEE_FREQ_AGILITY )
    #define ZIGBEE_FREQ_AGILITY
  #endif
#endif

#if defined ( ZIGBEE_FREQ_AGILITY ) || defined ( ZBIT )
  // Make Frequency Agility to look for all MAC errors for Certification test
  // by setting the following to TRUE. The default value is FALSE meaning
  // that only ZMacChannelAccessFailure error code will trigger a scan.
  #if !defined ( NWK_FREQ_AGILITY_ALL_MAC_ERRS )
    #define NWK_FREQ_AGILITY_ALL_MAC_ERRS  FALSE
  #endif
#endif

// Controls various stack parameter settings
#define ZIGBEEPRO_PROFILE     2

// Channel mask
#define MAX_CHANNELS_868MHZ     0x00000001
#define MAX_CHANNELS_915MHZ     0x000007FE

#if !defined ( MAX_CHANNELS_24GHZ )
  #define MAX_CHANNELS_24GHZ    0x07FFF800
#endif

#define STACK_PROFILE_ID      ZIGBEEPRO_PROFILE

//Z-Stack does not support other than ZigbeePro_Profile.
//These parameters must not be modified to keep Zigbee Core compliance.
// Refer to Zigbee PRO Stack Profile 2 (07-4855-05) for more information
#if ( STACK_PROFILE_ID == ZIGBEEPRO_PROFILE )
    #define MAX_NODE_DEPTH      30
    #define USE_NWK_SECURITY    1   // true or false
    #define SECURITY_LEVEL      5
#endif

// Zigbee protocol version
#define ZB_PROT_V1_0                 1
#define ZB_PROT_V1_1                 2

#define ZB_PROT_VERS      ZB_PROT_V1_1
#define ZIGBEE_PROT_ID            0x00

// Status and error codes for extra information
#define NWK_STATUS_PING_RCVD            0x0001
#define NWK_STATUS_ASSOC_CNF            0x0002
#define NWK_STATUS_ED_ADDR              0x0003
#define NWK_STATUS_PARENT_ADDR          0x0004
#define NWK_STATUS_COORD_ADDR           0x0005
#define NWK_STATUS_ROUTER_ADDR          0x0006
#define NWK_STATUS_ORPHAN_RSP           0x0007

#define NWK_ERROR_ASSOC_RSP             0x1001
#define NWK_ERROR_ASSOC_RSP_MF          0x1002
#define NWK_ERROR_ASSOC_CNF_DENIED      0x1003
#define NWK_ERROR_ENERGY_SCAN_FAILED    0x1004

// Indicate whether incoming NWK frames must be all checked for freshness
// when the memory for incoming frame counts is exceeded
#if !defined( NWK_ALL_FRESH )
  #define NWK_ALL_FRESH TRUE  // Default to TRUE - Check all frames
#endif

// Indicate whether to use Multicast in NIB value
#if !defined( MULTICAST_ENABLED )
  #define MULTICAST_ENABLED TRUE  // Default to TRUE
#endif

// Maximum number in tables
#if !defined( NWK_MAX_DEVICE_LIST )
#define NWK_MAX_DEVICE_LIST     60  // Maximum number of devices in the
                                    // Assoc/Device list.
#endif

// Don't change this value to set the number of devices.  Change
//  NWK_MAX_DEVICE_LIST above
#define NWK_MAX_DEVICES   ( NWK_MAX_DEVICE_LIST + 1 )    // One extra space for parent

// Number of End Devices that will be stored in the SrcMatch and NotMyChildList lists
// when aged out by the Child Table Management process
#define MAX_NOT_MYCHILD_DEVICES  5

// Number of reserved places for router and end device children, to be used in stochastic addressing.
#if !defined ( NWK_MIN_ROUTER_CHILDREN )
  #define NWK_MIN_ROUTER_CHILDREN          0
#endif
#if !defined ( NWK_MIN_ENDDEVICE_CHILDREN )
  #define NWK_MIN_ENDDEVICE_CHILDREN       0
#endif

#if !defined ( MAX_NEIGHBOR_ENTRIES )
  #if ( ZG_BUILD_RTR_TYPE )
    #define MAX_NEIGHBOR_ENTRIES    16
  #else
    #define MAX_NEIGHBOR_ENTRIES    4
  #endif
#endif

#if !defined ( APS_MAX_GROUPS )
  #define APS_MAX_GROUPS  10
#endif

#define NWK_MAX_REFLECTOR_ENTRIES ( NWK_MAX_BINDING_ENTRIES )

#if !defined( MAX_BCAST )
  #define MAX_BCAST 9
#endif

#if !defined ( NWK_MAX_BROADCAST_JITTER )
  // The maximum broadcast jitter time in 2 msec periods (0x40 msec on 2.4GHz)
  #define NWK_MAX_BROADCAST_JITTER  0x20
#endif

// Maxiumum number of secure partners(Commercial mode only).
#if ZG_BUILD_COORDINATOR_TYPE
// Adding 5 entries to allow up to 5 legacy devices join concurrently when the rest of the
// table is filled with ZigBee 3.0 devices, binding table related addresses, association
// table related addresses, etc. the usage of these 5 entries is just temporary during joining
// of the legacy devices. A few seconds (BDB_DEFAULT_TC_NODE_JOIN_TIMEOUT) after they joined,
// these entries are released and can be used for joining more legacy devices.
  #define NWK_MAX_SECURE_PARTNERS (5 + ZDSECMGR_TC_DEVICE_MAX)
#else
// Add 1 for the Trust Center(Coordinator) if it is not the parent.
  #define NWK_MAX_SECURE_PARTNERS 1
#endif

// Maximum number of addresses managed by the Address Manager
#define NWK_MAX_ADDRESSES (uint16_t)                          \
                          ( ( NWK_MAX_DEVICES           ) +   \
                            ( NWK_MAX_REFLECTOR_ENTRIES ) +   \
                            ( NWK_MAX_SECURE_PARTNERS   )   )

// Network PAN Coordinator Address
#define NWK_PAN_COORD_ADDR 0x0000

// Network Addressing modes
#define NWK_ADDRESSING_DISTRIBUTED    0x00
#define NWK_ADDRESSING_STOCHASTIC     0x02

#if !defined ( NWK_LINK_STATUS_PERIOD )
  #define NWK_LINK_STATUS_PERIOD 60       // 15 seconds
#endif

#if !defined ( LINK_STATUS_JITTER_MASK )
  #define LINK_STATUS_JITTER_MASK 0x007F   // 127 milliseconds
#endif

#if !defined ( NWK_ROUTE_AGE_LIMIT )
  #define NWK_ROUTE_AGE_LIMIT 3       // 3 missed link satus frames
#endif

#if !defined ( MAX_RTG_SRC_ENTRIES )
  #define MAX_RTG_SRC_ENTRIES 60
#endif

#if !defined ( SRC_RTG_EXPIRY_TIME )
  #define SRC_RTG_EXPIRY_TIME 20   // seconds before the source route entry expires
#endif

#if !defined ( MTO_RREQ_LIMIT_TIME )
  // in milliseconds. The time limited to one MTO RReq (Concentrator Announce)
  #define MTO_RREQ_LIMIT_TIME 1000
#endif

#if !defined ( MTO_ROUTE_EXPIRY_TIME )
  // The number of seconds a MTO routing entry will last. Default to not expiring.
  #define MTO_ROUTE_EXPIRY_TIME RTG_NO_EXPIRY_TIME
#endif

#if ( ZG_BUILD_ENDDEVICE_TYPE )
  #define APS_MAX_ENDDEVICE_BROADCAST_ENTRIES   ( 2 * MAX_BCAST )
#endif

#if !defined( NWK_CONFLICTED_ADDR_EXPIRY_TIME )
  #define NWK_CONFLICTED_ADDR_EXPIRY_TIME  4    // number of link status period after the
                                                // last received address conflict
                                                // report (network status command)
#endif

#if !defined ( LINK_DOWN_TRIGGER )
  #define LINK_DOWN_TRIGGER          3   // Link is down if txCounter exceeds this
#endif

#if !defined ( GOOD_LINK_COST )
  #define GOOD_LINK_COST             ( MAX_LINK_COST / 2 )   // 3 is considered good cost
#endif

// This the size of the conflicted address table
// Scale it up if the size of the network is over 100 nodes
#if !defined( CONFLICTED_ADDR_TABLE_SIZE )
  #define CONFLICTED_ADDR_TABLE_SIZE   3
#endif

// Maximum number of relays in source routing
#if !defined ( MAX_SOURCE_ROUTE )
  #define MAX_SOURCE_ROUTE             12
#endif

#if !defined ( MAX_BROADCAST_QUEUED )
  #define MAX_BROADCAST_QUEUED 10
#endif

#if !defined ( DEFAULT_ROUTE_REQUEST_RADIUS )
  #define DEFAULT_ROUTE_REQUEST_RADIUS DEF_NWK_RADIUS
#endif

#if !defined ( DEF_NWK_RADIUS )
  // the default network radius set twice the value of <nwkMaxDepth>
  #define DEF_NWK_RADIUS           ( 2 * BEACON_MAX_DEPTH )
#endif

#if !defined ( MAX_PASSIVE_ACK_CNT )
  #define MAX_PASSIVE_ACK_CNT 8
#endif

//Define the number of network security material entries that this device can have.
//The first MAX_NWK_SEC_MATERIAL_TABLE_ENTRIES-1 networks will be stored, while the last
//will be used for the remaining networks joined
#define MAX_NWK_SEC_MATERIAL_TABLE_ENTRIES   5

#if !defined ( NWK_JOIN_SECURITY_TIMEOUT_PERIOD )
  #define NWK_JOIN_SECURITY_TIMEOUT_PERIOD 5000
#endif

/*********************************************************************
 * TYPEDEFS
 */
#if ( MAX_NEIGHBOR_ENTRIES > 255 ) || defined ( LARGE_NEIGHBOR_TABLE )
  typedef uint16_t neighborTableIndex_t;
#else
  typedef uint8_t neighborTableIndex_t;
#endif

#if ( NWK_MAX_DEVICES > 255 ) || defined ( LARGE_DEVICE_TABLE )
  typedef uint16_t deviceTableIndex_t;
#else
  typedef uint8_t deviceTableIndex_t;
#endif

#if ( MAX_RTG_ENTRIES > 255 ) || defined ( LARGE_ROUTING_TABLE )
  typedef uint16_t rtgTableIndex_t;
#else
  typedef uint8_t rtgTableIndex_t;
#endif

#if ( MAX_RTG_SRC_ENTRIES > 255 ) || defined ( LARGE_SOURCE_ROUTE_TABLE )
  typedef uint16_t srcRtgTableIndex_t;
#else
  typedef uint8_t srcRtgTableIndex_t;
#endif

#if ( MAX_RREQ_ENTRIES > 255 ) || defined ( LARGE_ROUTE_REQUEST_TABLE )
  typedef uint16_t rreqTableIndex_t;
#else
  typedef uint8_t rreqTableIndex_t;
#endif

#if ( NWK_MAX_BINDING_ENTRIES > 255 ) || defined ( LARGE_BINDING_TABLE )
  typedef uint16_t bindTableIndex_t;
#else
  typedef uint8_t bindTableIndex_t;
#endif

#if ( MAX_BCAST > 255 ) || defined ( LARGE_BROADCAST_TABLE )
  typedef uint16_t bcastTableIndex_t;
#else
  typedef uint8_t bcastTableIndex_t;
#endif

#if defined ( FEATURE_MNP )
  #if !defined ( MAX_MNP_QUEUED )
    #define MAX_MNP_QUEUED 2
  #endif
#endif

/*********************************************************************
 * NWK GLOBAL VARIABLES
 */

// Variables for MAX data buffer levels
extern CONST byte gNWK_MAX_DATABUFS_WAITING;
extern CONST byte gNWK_MAX_DATABUFS_SCHEDULED;
extern CONST byte gNWK_MAX_DATABUFS_CONFIRMED;
extern CONST byte gNWK_MAX_DATABUFS_TOTAL;

extern CONST byte gNWK_INDIRECT_CNT_RTG_TMR;
extern CONST byte gNWK_INDIRECT_MSG_MAX_PER;
extern CONST byte gNWK_INDIRECT_MSG_MAX_ALL;

extern CONFIG_ITEM neighborTableIndex_t gMAX_NEIGHBOR_ENTRIES;

extern CONFIG_ITEM rtgTableIndex_t gMAX_RTG_ENTRIES;
extern CONFIG_ITEM srcRtgTableIndex_t gMAX_RTG_SRC_ENTRIES;
extern CONFIG_ITEM rreqTableIndex_t gMAX_RREQ_ENTRIES;

extern CONST uint16_t gMTO_RREQ_LIMIT_TIME;
extern CONST uint8_t gMTO_ROUTE_EXPIRY_TIME;

extern CONST uint8_t gMAX_PASSIVE_ACK_CNT;

// Variables for MAX list size
extern CONST deviceTableIndex_t gNWK_MAX_DEVICE_LIST;

extern CONST uint8_t gNWK_TREE_ALLOCATE_ROUTERADDR_FOR_ENDDEVICE;

extern CONST uint16_t gNWK_MIN_ROUTER_CHILDREN;
extern CONST uint16_t gNWK_MIN_ENDDEVICE_CHILDREN;

extern byte gMIN_TREE_LQI;

extern CONFIG_ITEM byte defaultKey[];

#if (ZG_BUILD_JOINING_TYPE)
extern CONFIG_ITEM byte distributedDefaultKey[];
#endif

extern CONST byte defaultTCLinkKey[];

extern CONST uint8_t gMAX_SOURCE_ROUTE;
extern uint16_t rtgSrcRelayList[];

extern CONFIG_ITEM bcastTableIndex_t gMAX_BCAST;

extern CONST byte gNWK_CONFLICTED_ADDR_EXPIRY_TIME;

#if defined ( ZIGBEE_FREQ_AGILITY ) || defined ( ZBIT )
extern CONST uint8_t gNWK_FREQ_AGILITY_ALL_MAC_ERRS;
#endif
extern CONST uint8_t gMAX_BROADCAST_QUEUED;

extern CONST uint8_t gLINK_DOWN_TRIGGER;

extern CONST uint8_t gGOOD_LINK_COST;

extern CONST uint8_t gDEFAULT_ROUTE_REQUEST_RADIUS;

extern CONST uint8_t gDEF_NWK_RADIUS;

#if ( ZSTACK_ROUTER_BUILD ) || defined ( ZBIT )
extern CONST uint16_t gLINK_STATUS_JITTER_MASK;
#endif

extern CONST uint8_t gMAX_NOT_MYCHILD_DEVICES;

extern CONST uint32_t timeoutValue[];

extern CONST uint32_t gMAX_NWK_FRAMECOUNTER_CHANGES;

#if defined ( FEATURE_MNP )
  extern uint8_t gMAX_MNP_QUEUED;
#endif

extern CONFIG_ITEM uint16_t gNWK_MAX_BROADCAST_JITTER;

extern CONST uint32_t gNWK_JOIN_SECURITY_TIMEOUT_PERIOD;

/*********************************************************************
 * APS GLOBAL VARIABLES
 */

// Variables for Binding Table
extern CONFIG_ITEM bindTableIndex_t gNWK_MAX_BINDING_ENTRIES;
extern CONFIG_ITEM uint8_t gMAX_BINDING_CLUSTER_IDS;
extern CONST uint16_t gBIND_REC_SIZE;

extern CONFIG_ITEM uint8_t gAPS_MAX_GROUPS;

extern uint8_t gAPS_MAX_ENDDEVICE_BROADCAST_ENTRIES;

/*********************************************************************
 * GLOBAL VARIABLES - Statistics
 */

#if defined ( FEATURE_PACKET_FILTER_STATS )
  extern uint32_t apsInvalidPackets;
  extern uint32_t apsSecurityFailures;
  extern uint32_t nwkInvalidPackets;
  extern uint32_t nwkSecurityFailures;
#endif

/*********************************************************************
 * FUNCTIONS
 */

/*
 * Init Global Variables
 */
extern void nwk_globals_init( void );
extern void NIB_init( void );

extern void nwk_Status( uint16_t statusCode, uint16_t statusValue );

extern uint16_t nwk_adjustDelay( uint16_t existingDelay, uint8_t confirmStatus, uint16_t bufOptions );

/*********************************************************************
*********************************************************************/
#ifdef __cplusplus
}
#endif

#endif /* NWK_GLOBALS_H */


我还会为路由器发布 SysConfig

/**
 * These arguments were used when this file was generated. They will be automatically applied on subsequent loads
 * via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
 * @cliArgs --board "/ti/boards/CC1352P_2_LAUNCHXL" --rtos "tirtos" --product "simplelink_cc13xx_cc26xx_sdk@6.20.00.29"
 * @versions {"tool":"1.13.0+2553"}
 */

/**
 * Import the modules used in this configuration.
 */
const CCFG     = scripting.addModule("/ti/devices/CCFG");
const rfdesign = scripting.addModule("/ti/devices/radioconfig/rfdesign");
const AESCBC   = scripting.addModule("/ti/drivers/AESCBC");
const AESCBC1  = AESCBC.addInstance();
const AESCCM   = scripting.addModule("/ti/drivers/AESCCM");
const AESCCM1  = AESCCM.addInstance();
const AESECB   = scripting.addModule("/ti/drivers/AESECB");
const AESECB1  = AESECB.addInstance();
const DMA      = scripting.addModule("/ti/drivers/DMA");
const ECDH     = scripting.addModule("/ti/drivers/ECDH");
const ECDH1    = ECDH.addInstance();
const ECDSA    = scripting.addModule("/ti/drivers/ECDSA");
const ECDSA1   = ECDSA.addInstance();
const GPIO     = scripting.addModule("/ti/drivers/GPIO", {}, false);
const GPIO1    = GPIO.addInstance();
const GPIO2    = GPIO.addInstance();
const GPIO3    = GPIO.addInstance();
const NVS      = scripting.addModule("/ti/drivers/NVS");
const NVS1     = NVS.addInstance();
const NVS2     = NVS.addInstance();
const Power    = scripting.addModule("/ti/drivers/Power");
const RF       = scripting.addModule("/ti/drivers/RF");
const SHA2     = scripting.addModule("/ti/drivers/SHA2");
const SHA21    = SHA2.addInstance();
const SPI      = scripting.addModule("/ti/drivers/SPI", {}, false);
const SPI1     = SPI.addInstance();
const TRNG     = scripting.addModule("/ti/drivers/TRNG");
const TRNG1    = TRNG.addInstance();
const Timer    = scripting.addModule("/ti/drivers/Timer", {}, false);
const Timer1   = Timer.addInstance();
const UART     = scripting.addModule("/ti/drivers/UART", {}, false);
const UART1    = UART.addInstance();
const Button   = scripting.addModule("/ti/drivers/apps/Button");
const Button1  = Button.addInstance();
const Button2  = Button.addInstance();
const LED      = scripting.addModule("/ti/drivers/apps/LED");
const LED1     = LED.addInstance();
const LED2     = LED.addInstance();
const zstack   = scripting.addModule("/ti/zstack/zstack");

/**
 * Write custom configuration values to the imported modules.
 */
CCFG.xoscCapArray             = true;
CCFG.xoscCapArrayDelta        = 0xC1;
CCFG.enableBootloader         = true;
CCFG.enableBootloaderBackdoor = true;
CCFG.dioBootloaderBackdoor    = 15;
CCFG.levelBootloaderBackdoor  = "Active low";
CCFG.forceVddr                = true;
CCFG.ccfgTemplate.$name       = "ti_devices_CCFG_CCFGCC26XXTemplate0";

rfdesign.rfDesign = "LAUNCHXL-CC1352P-2";

AESCBC1.$name = "CONFIG_AESCBC_0";

AESCCM1.$name             = "CONFIG_AESCCM_0";
AESCCM1.interruptPriority = "2";

AESECB1.$name             = "CONFIG_AESECB_0";
AESECB1.interruptPriority = "1";

ECDH1.$name = "CONFIG_ECDH_0";

ECDSA1.$name = "CONFIG_ECDSA_0";

GPIO1.$name = "CONFIG_GPIO_TEST_OUT";
GPIO1.mode  = "Output";

GPIO2.$name = "CONFIG_GPIO_RFID_SS";
GPIO2.mode  = "Output";

GPIO3.$name = "CONFIG_GPIO_RFID_RST";
GPIO3.mode  = "Output";

NVS1.$name                    = "CONFIG_NVSINTERNAL";
NVS1.internalFlash.$name      = "ti_drivers_nvs_NVSCC26XX0";
NVS1.internalFlash.regionSize = 0x4000;
NVS1.internalFlash.regionBase = 0x52000;

NVS2.$name                          = "CONFIG_NVSEXTERNAL";
NVS2.nvsType                        = "External";
NVS2.$hardware                      = system.deviceData.board.components.MX25R8035F;
NVS2.externalFlash.$name            = "ti_drivers_nvs_NVSSPI25X0";
NVS2.externalFlash.regionSize       = 0x256000;
NVS2.externalFlash.verifyBufferSize = 64;

RF.$hardware = system.deviceData.board.components["SKY13317-373LF"];

SHA21.$name = "CONFIG_SHA2_0";

TRNG1.$name = "CONFIG_TRNG_0";

Timer1.$name               = "CONFIG_TIMER_0";
Timer1.timerType           = "32 Bits";
Timer1.timerInstance.$name = "CONFIG_GPTIMER_0";

UART1.$name               = "CONFIG_UART";
UART1.txPinInstance.$name = "CONFIG_GPIO_1";
UART1.rxPinInstance.$name = "CONFIG_GPIO_2";

Button1.$name          = "CONFIG_BTN_LEFT";
Button1.autoHwConfig   = false;
Button1.button.$assign = "boosterpack.8";
Button1.gpioPin.$name  = "CONFIG_GPIO_BTN1";
Button1.gpioPin.pull   = "Pull Up";

Button2.$name                        = "CONFIG_BTN_RIGHT";
Button2.autoHwConfig                 = false;
Button2.button.$assignAllowConflicts = "boosterpack.4";
Button2.gpioPin.$name                = "CONFIG_GPIO_BTN2";
Button2.gpioPin.pull                 = "Pull Up";
scripting.suppress("Connected to hardware,@@@.+?@@@ is connected to XDS110 UART on the CC1352P-2 LaunchPad\. Consider selecting it in 'use hardware' above\. @@@.+?@@@", Button2, "button");

LED1.$name         = "CONFIG_LED_RED";
LED1.$hardware     = system.deviceData.board.components.LED_RED;
LED1.gpioPin.$name = "CONFIG_GPIO_RLED";

LED2.$name         = "CONFIG_LED_GREEN";
LED2.$hardware     = system.deviceData.board.components.LED_GREEN;
LED2.gpioPin.$name = "CONFIG_GPIO_GLED";

const NVSSPI25XDevice                         = scripting.addModule("/ti/drivers/nvs/NVSSPI25XDevice", {}, false);
const NVSSPI25XDevice1                        = NVSSPI25XDevice.addInstance({}, false);
NVSSPI25XDevice1.$name                        = "CONFIG_NVS_SPI_0";
NVS2.externalFlash.spiFlashDevice             = NVSSPI25XDevice1;
NVSSPI25XDevice1.slaveSelectPinInstance.$name = "CONFIG_GPIO_0";

NVSSPI25XDevice1.sharedSpiInstance = SPI1;
SPI1.$name                         = "CONFIG_SPI_RFID";

zstack.deviceType                            = "zr";
zstack.deviceTypeReadOnly                    = true;
zstack.touchlink.$name                       = "ti_zstack_touchlink_zstack_touchlink0";
zstack.pm.$name                              = "ti_zstack_pm_zstack_pm0";
zstack.rf.$name                              = "ti_zstack_rf_zstack_rf0";
zstack.rf.txPower                            = "20";
zstack.rf.primaryChannels                    = [26];
zstack.rf.radioConfig.$name                  = "ti_devices_radioconfig_settings_ieee_15_40";
zstack.rf.radioConfig.codeExportConfig.$name = "ti_devices_radioconfig_code_export_param0";
zstack.rf.coexSettings.$name                 = "ti_zstack_rf_zstack_coex_mod0";
zstack.network.$name                         = "ti_zstack_network_zstack_network0";
zstack.network.panID                         = "0xFFFE";
zstack.advanced.$name                        = "ti_zstack_advanced_zstack_advanced0";
zstack.advanced.routing.$name                = "ti_zstack_advanced_zstack_routing0";
zstack.advanced.packetSending.$name          = "ti_zstack_advanced_zstack_packet_sending0";
zstack.advanced.tableSize.$name              = "ti_zstack_advanced_zstack_table_size0";
zstack.advanced.tableSize.bindingTableSize   = 40;
zstack.advanced.tableSize.groupTableSize     = 40;

/**
 * Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
 * version of the tool will not impact the pinmux you originally saw.  These lines can be completely deleted in order to
 * re-solve from scratch.
 */
GPIO1.gpioPin.$suggestSolution                = "boosterpack.10";
GPIO2.gpioPin.$suggestSolution                = "boosterpack.36";
GPIO3.gpioPin.$suggestSolution                = "boosterpack.19";
RF.rfAntennaPin0.$suggestSolution             = "ball.41";
RF.rfAntennaPin1.$suggestSolution             = "ball.42";
RF.rfAntennaPin2.$suggestSolution             = "ball.43";
Timer1.timerInstance.timer.$suggestSolution   = "GPTM0";
UART1.uart.$suggestSolution                   = "UART0";
UART1.uart.txPin.$suggestSolution             = "boosterpack.31";
UART1.uart.rxPin.$suggestSolution             = "boosterpack.32";
LED1.ledPin.$suggestSolution                  = "boosterpack.39";
LED2.ledPin.$suggestSolution                  = "boosterpack.40";
NVSSPI25XDevice1.slaveSelect.$suggestSolution = "boosterpack.38";
SPI1.spi.$suggestSolution                     = "SSI0";
SPI1.spi.sclkPin.$suggestSolution             = "boosterpack.7";
SPI1.spi.misoPin.$suggestSolution             = "boosterpack.14";
SPI1.spi.mosiPin.$suggestSolution             = "boosterpack.15";
SPI1.spi.dmaRxChannel.$suggestSolution        = "DMA_CH3";
SPI1.spi.dmaTxChannel.$suggestSolution        = "DMA_CH4";

2 -我们将路由器数量限制为8台,从而获得以下拓扑:

然后、我创建了一个脚本来轮询器件的端点(使用 Zigbee2Mqtt API)并测量经过的时间、首先仅轮询每个器件的单个端点(2个集群、计量和 ONOFF)、然后针对8个器件中的每个器件的所有8个端点(智能插头)。 未发生超时。 以下是日志:

Field test, polling 1 endpoint per device, Routers only

Device: 0x00124b002590e188 [Router],            Time elapsed: 153.884ms, Average per attribute : 76.942ms    
Device: 0x00124b0025907b5c [Router],            Time elapsed: 208.8629ms, Average per attribute : 104.43145ms
Device: 0x00124b0025908a25 [Router],            Time elapsed: 219.8165ms, Average per attribute : 109.90825ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 238.5847ms, Average per attribute : 119.29235ms
Device: 0x00124b00259087a1 [Router],            Time elapsed: 118.6589ms, Average per attribute : 59.32945ms 
Device: 0x00124b002590dd78 [Router],            Time elapsed: 185.6975ms, Average per attribute : 92.84875ms 
Device: 0x00124b002590e021 [Router],            Time elapsed: 146.0539ms, Average per attribute : 73.02695ms 
Device: 0x00124b002590dd33 [Router],            Time elapsed: 184.1201ms, Average per attribute : 92.06005ms 

Full poll time: 1.4556785s

Field test, polling 8 endpoint per device, Routers only

Device: 0x00124b0025907b5c [Router],            Time elapsed: 1.7198454s, Average per attribute : 107.490331ms
Device: 0x00124b0025908a25 [Router],            Time elapsed: 1.5746697s, Average per attribute : 98.416852ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 1.7933287s, Average per attribute : 112.083037ms
Device: 0x00124b00259087a1 [Router],            Time elapsed: 914.7183ms, Average per attribute : 57.169888ms
Device: 0x00124b002590dd78 [Router],            Time elapsed: 1.4159681s, Average per attribute : 88.498001ms
Device: 0x00124b002590e021 [Router],            Time elapsed: 1.1336071s, Average per attribute : 70.850438ms
Device: 0x00124b002590dd33 [Router],            Time elapsed: 1.4949566s, Average per attribute : 93.434781ms
Device: 0x00124b002590e188 [Router],            Time elapsed: 1.23612s, Average per attribute : 77.257493ms

Full poll time: 11.2832139s

3 -我们沿线路绑定了8个终端设备、通过16个设备获得以下拓扑:

现在我再次运行了脚本、没有发生超时、但终端设备出现了巨大的延迟、以下是日志:

Field test, polling 1 endpoint per device, 8 Routers + 8 EndDevices

Device: 0x00124b0025908a25 [Router],            Time elapsed: 176.9852ms, Average per attribute : 88.4926ms
Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 222.6546ms, Average per attribute : 111.3273ms
Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 1.0652301s, Average per attribute : 532.61505ms
Device: 0x00124b0025907b5c [Router],            Time elapsed: 198.8744ms, Average per attribute : 99.4372ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 197.2419ms, Average per attribute : 98.62095ms
Device: 0x00124b002590dd78 [Router],            Time elapsed: 167.8257ms, Average per attribute : 83.91285ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 1.431613s, Average per attribute : 715.8065ms
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 5.8469776s, Average per attribute : 2.9234888s
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 2.9179497s, Average per attribute : 1.45897485s
Device: 0x00124b00259087a1 [Router],            Time elapsed: 103.736ms, Average per attribute : 51.868ms
Device: 0x00124b002590dd33 [Router],            Time elapsed: 177.8675ms, Average per attribute : 88.93375ms
Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 4.1672753s, Average per attribute : 2.08363765s
Device: 0x00124b0025906ff3 [EndDevice],         Time elapsed: 5.6209016s, Average per attribute : 2.8104508s
Device: 0x00124b002590e188 [Router],            Time elapsed: 120.3848ms, Average per attribute : 60.1924ms
Device: 0x00124b002590e021 [Router],            Time elapsed: 126.3897ms, Average per attribute : 63.19485ms
Device: 0x00124b0025907cb1 [EndDevice],         Time elapsed: 4.1024619s, Average per attribute : 2.05123095s

Full poll time: 26.644369s

Field test, polling 8 endpoint per device, 8 Routers + 8 End devices

Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 4.1211526s, Average per attribute : 257.572031ms
Device: 0x00124b0025907b5c [Router],            Time elapsed: 1.3779558s, Average per attribute : 86.122231ms
Device: 0x00124b0025908a25 [Router],            Time elapsed: 1.0705681s, Average per attribute : 66.910501ms
Device: 0x00124b002590dd78 [Router],            Time elapsed: 1.0820209s, Average per attribute : 67.626301ms
Device: 0x00124b002590e021 [Router],            Time elapsed: 806.58ms, Average per attribute : 50.411245ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 2.0414714s, Average per attribute : 127.591957ms
Device: 0x00124b002590e188 [Router],            Time elapsed: 982.7829ms, Average per attribute : 61.423924ms
Device: 0x00124b00259087a1 [Router],            Time elapsed: 726.5046ms, Average per attribute : 45.40653ms
Device: 0x00124b002590dd33 [Router],            Time elapsed: 1.2341957s, Average per attribute : 77.137225ms
Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 43.8911905s, Average per attribute : 2.7431994s
Device: 0x00124b0025906ff3 [EndDevice],         Time elapsed: 47.6144099s, Average per attribute : 2.975900614s
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 47.1970158s, Average per attribute : 2.949813481s
Device: 0x00124b0025907cb1 [EndDevice],         Time elapsed: 29.1029119s, Average per attribute : 1.818931989s
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 3.3832635s, Average per attribute : 211.453963ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 1.4299035s, Average per attribute : 89.368962ms
Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 4.2789814s, Average per attribute : 267.436331ms

Full poll time: 3m10.3409085s

因此、向中央路由器线路添加终端设备似乎可以减少跳数并使网络更大、但我们的应用无法接受这些数量级的延迟。

4 -我们还在实验室中将先前测试中的16个器件(8个路由器+ 8个终端设备)带到了内部、保留了绑定和配对、并重复了测量测试

Lab test, polling 1 endpoint per device, 8 Routers + 8 End-Devices

Device: 0x00124b0025906ff3 [EndDevice],         Time elapsed: 1.4267376s, Average per attribute : 713.3688ms
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 2.4122712s, Average per attribute : 1.2061356s
Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 2.1348938s, Average per attribute : 1.0674469s
Device: 0x00124b002590dd33 [Router],            Time elapsed: 91.4669ms, Average per attribute : 45.73345ms
Device: 0x00124b002590e021 [Router],            Time elapsed: 92.4419ms, Average per attribute : 46.22095ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 83.5755ms, Average per attribute : 41.78775ms
Device: 0x00124b002590dd78 [Router],            Time elapsed: 93.2088ms, Average per attribute : 46.6044ms
Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 2.0595667s, Average per attribute : 1.02978335s
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 1.4978588s, Average per attribute : 748.9294ms
Device: 0x00124b002590e188 [Router],            Time elapsed: 89.6877ms, Average per attribute : 44.84385ms
Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 917.0266ms, Average per attribute : 458.5133ms
Device: 0x00124b0025907b5c [Router],            Time elapsed: 97.2496ms, Average per attribute : 48.6248ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 1.5685691s, Average per attribute : 784.28455ms
Device: 0x00124b0025907cb1 [EndDevice],         Time elapsed: 2.7326952s, Average per attribute : 1.3663476s
Device: 0x00124b0025908a25 [Router],            Time elapsed: 88.3405ms, Average per attribute : 44.17025ms
Device: 0x00124b00259087a1 [Router],            Time elapsed: 96.2979ms, Average per attribute : 48.14895ms

Full poll time: 15.4818878s

Lab test, polling 8 endpoint per device, 8 Routers + 8 End-Devices

Device: 0x00124b002590e021 [Router],            Time elapsed: 864.2836ms, Average per attribute : 54.017718ms
Device: 0x00124b00259087a1 [Router],            Time elapsed: 1.1681567s, Average per attribute : 73.00979ms
Device: 0x00124b0025907b63 [Router],            Time elapsed: 744.4813ms, Average per attribute : 46.530076ms
Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 4.7857835s, Average per attribute : 299.111463ms
Device: 0x00124b0025908a25 [Router],            Time elapsed: 727.6489ms, Average per attribute : 45.47805ms
Device: 0x00124b0025910009 [EndDevice],         Time elapsed: 4.1694748s, Average per attribute : 260.592169ms
Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 2.5862343s, Average per attribute : 161.639637ms
Device: 0x00124b0025907b5c [Router],            Time elapsed: 1.1745931s, Average per attribute : 73.412063ms
Device: 0x00124b002590dd33 [Router],            Time elapsed: 1.1568752s, Average per attribute : 72.304694ms
Device: 0x00124b0025906ff3 [EndDevice],         Time elapsed: 4.7752102s, Average per attribute : 298.450632ms
Device: 0x00124b0025907cb1 [EndDevice],         Time elapsed: 4.2859462s, Average per attribute : 267.871634ms
Device: 0x00124b002590e188 [Router],            Time elapsed: 648.5117ms, Average per attribute : 40.531974ms
Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 3.9794359s, Average per attribute : 248.714738ms
Device: 0x00124b002590dd78 [Router],            Time elapsed: 964.7451ms, Average per attribute : 60.296564ms
Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 3.5703009s, Average per attribute : 223.1438ms
Device: 0x00124b002591071d [EndDevice],         Time elapsed: 3.2085772s, Average per attribute : 200.536071ms

Full poll time: 38.8102586s

如何继续? 如何增加消息可以重复完成的跳数、或者如何减少终端设备轮询延迟?
提前感谢您提供任何提示。

此致

Rn

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您的测试终端设备的轮询率是多少? 我假设您可以提高轮询速率以减少 终端设备轮询延迟

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,我很抱歉,但我不会对你的意思表示失望。 您是否认为我应该比路由器更频繁地询问属性?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    ZigBee à 终端器件使用轮询从其父节点获取数据、而轮询速率是睡眠终端器件检查其父节点以接收数据的频率。 如果睡眠终端设备的轮询率太大,则睡眠终端设备的响应速度会很慢,因此我建议您缩短睡眠终端设备轮询周期。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、RN、

    对于  此应用、您不需要大幅增加 APS_MAX_Groups 或 NWK_MAX_BBINARTing_entries、并且如果您打算向网络添加更多的 ZDSECMGR_TC_DEVICE_MAX 器件、则在某些情况 下还需要增加 NV 存储器空间。  这可能有助于增加 MAX_RTG_entries 和 MAX_NODE_DEPTH。  您还可以考虑 MTO 路由。  请参阅 《Z-Stack 用户指南》的 SWRA650和网络配置部分。

    加入可能会带来困难、因为节点请求 ZC TC 提供 TCLK 更新、必须将响应隧道传输回器件。  您可以通过在 ZD_sec_mgr.c 文件中将 requestNewTrustCenterLinkKey 设置为 false 来减少网络上的压力。

    您可以尝试增大 SysConfig -> Z-Stack -> Advanced -> Packet Sending 值(生成 *重试选项 ti_Zstack_config.h)、以允许更多重试或更大延迟。  另外请记住、ZED 必须使用 SysConfig 中的 POLL_RATE 轮询其父设备的消息、并且父设备的消息将在 Nwk_INDIRECT _MSG_TIMEOUT 秒后过期、而不会观察到数据请求。  这就是为什么您注意到在网络应用中涉及到 ZED 时会出现更大的延迟的原因。

    单向属性报告对于您的应用程序来说是否是不可行的选择?  这将产生较少的流量、并会延迟双向轮询数据。  从物理角度来看、如果只有一个路由选项、则很难轮询超过8跳的节点、并期望在两者之间返回响应而不会出现任何问题。

    此致、
    Ryan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 Ryan 和 YiKai、通过以下拓扑将 ZED 始终开启、大幅减少了这些延迟:

    Field test, 8 endpoint per device, R + EP
    ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
    Device: 0x00124b0025908a6a [EndDevice],         Time elapsed: 5.9300137s, Average per attribute : 370.625849ms
    Device: 0x00124b002590dd78 [Router],            Time elapsed: 785.5134ms, Average per attribute : 49.094582ms
    Device: 0x00124b002590dd33 [Router],            Time elapsed: 2.3118213s, Average per attribute : 144.488825ms
    Device: 0x00124b0025907b63 [Router],            Time elapsed: 7.0933361s, Average per attribute : 443.333502ms
    Device: 0x00124b002590e021 [Router],            Time elapsed: 1.474791s, Average per attribute : 92.174429ms
    Device: 0x00124b0025907b5c [EndDevice],         Time elapsed: 6.6505646s, Average per attribute : 415.660281ms
    Device: 0x00124b0025909133 [EndDevice],         Time elapsed: 1.9263135s, Average per attribute : 120.394586ms
    Device: 0x00124b002591071d [EndDevice],         Time elapsed: 1.0205053s, Average per attribute : 63.781575ms
    Device: 0x00124b002590fbf6 [EndDevice],         Time elapsed: 1.3835267s, Average per attribute : 86.470412ms
    Device: 0x00124b002590e188 [Router],            Time elapsed: 1.195753s, Average per attribute : 74.734558ms
    Device: 0x00124b0025908a25 [Router],            Time elapsed: 1.05071s, Average per attribute : 65.669369ms
    Device: 0x00124b00259087a1 [Router],            Time elapsed: 2.3342729s, Average per attribute : 145.892051ms
    Device: 0x00124b002590e1d0 [EndDevice],         Time elapsed: 2.0695823s, Average per attribute : 129.348889ms
    Device: 0x00124b002590f613 [EndDevice],         Time elapsed: 1.7096683s, Average per attribute : 106.854263ms
    Full poll time: 36.9363721s

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、也可以通过使用常开器件来改进它、但常开器件的功耗比 SED 高得多。