This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:为什么15.4堆栈通道26的最大功耗为15dbm

Guru**** 2813605 points

Other Parts Discussed in Thread: CC1352P

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1182625/cc1352p-why-15-4-stack-channel-26-max-power-is-15dbm

器件型号:CC1352P

大家好、TI 团队

 该 SDK 是 simplelink_cc13x2_26x2_sdk_5_20_00_52 示例 RTOS\cC1352P_2_LAUNCHXL\ti154stack\collector_2_4g

  我发现通道26的最大功率比其他通道低5dBm。

  为什么故意降低通道26的最大功率?

  

/******************************************************************************
 * GLOBAL VARIABLES
 */
int8_t PLTableIeee[RF_CONFIG_IEEE_PL_NO_CHANNELS] =
{
     20,    //20dBm max for Channel = 11
     20,    //20dBm max for Channel = 12
     20,    //20dBm max for Channel = 13
     20,    //20dBm max for Channel = 14
     20,    //20dBm max for Channel = 15
     20,    //20dBm max for Channel = 16
     20,    //20dBm max for Channel = 17
     20,    //20dBm max for Channel = 18
     20,    //20dBm max for Channel = 19
     20,    //20dBm max for Channel = 20
     20,    //20dBm max for Channel = 21
     20,    //20dBm max for Channel = 22
     20,    //20dBm max for Channel = 23
     20,    //20dBm max for Channel = 24
     19,    //19dBm max for Channel = 25
     15,    //15dBm max for Channel = 26
};

macRfCfg_maxPower_t maxPowerIeee =
{
    RF_CONFIG_IEEE_PL_FIRST_CHANNEL,
    RF_CONFIG_IEEE_PL_NO_CHANNELS,
    PLTableIeee
};

此致、
LiuMengyang