Other Parts Discussed in Thread: CC2652RB, UNIFLASH, SYSCONFIG
主题中讨论的其他器件:CC2652RB、 UNIFLASH、 SysConfig
已获取我的 ZigBee 温度传感器应用并添加了 OTA 功能、 如此处所示。 但是、该教程似乎已过时、不会使用其中所述的 post-build 步骤进行构建。 我们必须调整 post-building 步骤、使之适应 ZED_SW_OTA_CLIENT_OFFCHIP_CC2652rb_tirtos7_ticlang 。
当前 post-build 步骤:
${CG_TOOL_ROOT}/bin/tiarmobjcopy ${BuildArtifactFileName} --output-target ihex ${BuildArtifactFileBaseName}.hex
${CG_TOOL_ROOT}/bin/tiarmobjcopy ${BuildArtifactFileName} --output-target binary ${BuildArtifactFileBaseName}_oad.bin
${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tools/common/oad/oad_image_tool --verbose ccs ${PROJECT_LOC} 7 -hex1 ${ConfigName}/${ProjName}.hex -k ${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tools/common/oad/private.pem -o ${ConfigName}/${ProjName}_oad
${COM_TI_SIMPLELINK_CC13XX_CC26XX_SDK_INSTALL_DIR}/tools/zstack/zigbee_ota_image_converter/zOTAfileGen ${PROJECT_LOC}/${ConfigName}/${ProjName}_oad.bin ${PROJECT_LOC}/${ConfigName}/ BEBE 2652 00000001
不知道这是否相关,但我想提到它。 程序构建和运行没有错误、但收到以下警告:
warning #10247-D: creating output section ".ccfg" without a SECTIONS specification
我已经添加了 OTA 库和 OTA_客户端_集成 来自的代码 ZED_SW_OTA_CLIENT_OFFCHIP_CC2652rb_tirtos7_ticlang 。
我可以对板进行编程而不会出现问题、但程序会卡在内部 macRadioPowerUpWait 根据调用堆栈:

我认为这与 从示例工程中添加的代码无关、因为在 BIOS 可以启动 SampleApp 任务并调用 OTA 函数之前会失败。 如果我擦除闪存并使用其他工程对其进行编程(不进行任何 OTA 修改)、该板会按预期工作、因此我认为可能不会有任何硬件问题。
这可能是由于编译后处理步骤、app.cfg 文件或链接器配置文件遇到一些未发现的问题引起的吗?
链接器文件:
/* Retain interrupt vector table variable */
--retain=g_pfnVectors
/* Override default entry point. */
--entry_point ResetISR
/* Allow main() to take args */
--args 0x8
/* Suppress warnings and errors: */
/* - 10063: Warning about entry point not being _c_int00 */
/* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */
/* files compiled using Keil (ARM compiler) */
--diag_suppress=10063,16011,16012
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */
/* The starting address of the application. Normally the interrupt vectors */
/* must be located at the beginning of the application. */
#ifndef NVOCMP_NVPAGES
#define NVOCMP_NVPAGES 2
#endif
#define FLASH_BASE 0x00000000
#define FLASH_NV_BASE (0x56000 - (NVOCMP_NVPAGES * 0x2000))
#define FLASH_NV_SIZE (NVOCMP_NVPAGES * 0x2000)
#define FLASH_LAST_BASE 0x56000
#define FLASH_LAST_SIZE 0x2000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x14000
#define GPRAM_BASE 0x11000000
#define GPRAM_SIZE 0x2000
#define OAD_HDR_START FLASH_BASE
#define OAD_HDR_SIZE 0xA8
#define OAD_HDR_END (OAD_HDR_START + OAD_HDR_SIZE - 1)
#define ENTRY_START (OAD_HDR_END + 1)
#define ENTRY_SIZE 0x40
#define ENTRY_END (ENTRY_START + ENTRY_SIZE - 1)
#define FLASH_START (ENTRY_END + 1)
#define FLASH_END (FLASH_NV_BASE - FLASH_START)
#define FLASH_SIZE (FLASH_END - FLASH_START)
#define PAGE_SIZE 0x2000
/* System memory map */
MEMORY
{
ENTRY (RX) : origin = ENTRY_START, length = ENTRY_SIZE
FLASH_IMG_HDR (RX) : origin = OAD_HDR_START, length = OAD_HDR_SIZE
/* Application stored in and executes from internal flash */
FLASH (RX) : origin = FLASH_START, length = FLASH_SIZE
/* FLASH NV */
FLASH_NV (RWX) : origin = FLASH_NV_BASE, length = FLASH_NV_SIZE
/* Last flash page */
FLASH_LAST (RX) : origin = FLASH_LAST_BASE, length = FLASH_LAST_SIZE
/* Application uses internal RAM for data */
SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
/* Application can use GPRAM region as RAM if cache is disabled in the CCFG
(DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
/* Explicitly placed off target for the storage of logging data.
* The data placed here is NOT loaded onto the target device.
* This is part of 1 GB of external memory from 0x60000000 - 0x9FFFFFFF.
* ARM memory map can be found here:
* developer.arm.com/.../about-the-memory-map
*/
LOG_DATA (R) : origin = 0x90000000, length = 0x40000 /* 256 KB */
}
/* Section allocation in memory */
SECTIONS
{
GROUP > FLASH_IMG_HDR
{
.image_header //align PAGE_SIZE
}
GROUP > ENTRY
{
.resetVecs LOAD_START(prgEntryAddr)
.intvecs
EntrySection
}
.text : > FLASH
config_const { mac_user_config.o(.rodata) } > FLASH
.const : > FLASH
.constdata : > FLASH
.rodata : > FLASH
.cinit : > FLASH LOAD_END(flashEndAddr)
.pinit : > FLASH
.init_array : > FLASH
.emb_text : > FLASH
.vtable : > SRAM
.vtable_ram : > SRAM
vtable_ram : > SRAM
.data : >> SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
.nonretenvar : > SRAM
.gpram : > GPRAM
.log_data : > LOG_DATA, type = COPY
}
/* Create global constant that points to top of stack */
/* CCS: Change stack size under Project Properties */
__STACK_TOP = __stack + __STACK_SIZE;