This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2652R7:OTBR + RCP 设置

Guru**** 2932960 points

Other Parts Discussed in Thread: CC2652R7

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread/f/zigbee-thread-forum/1264821/cc2652r7-otbr-rcp-set-up

器件型号:CC2652R7

您好、

以下是我的 OTBR + RCP 设置的详细信息:

OTBR:RPI 4B、带  Ubuntu  Server  22.04.2  LTS  (64位)

RCP:CC2652R7 + simplelink_cc13xx_cc26xx_sdk_7_10_01_24\examples\rtos\LP_CC2652r7\thready\rcp

我按照指南: https://openthread.io/guides/border-router/build、尝试设置我的 Matter 边界路由器。

当我尝试执行步骤5: 验证服务时、我遇到一些错误:

我使用命令

sudo systemctl status


它会显示 降级  状态:
● ubuntu
    State: degraded
     Jobs: 0 queued
   Failed: 1 units
    Since: Mon 2023-03-20 14:32:39 UTC; 5 months 10 days ago
   CGroup: /
           ├─user.slice
           │ └─user-1000.slice
           │   ├─user@1000.service …
           │   │ ├─app.slice
           │   │ │ ├─fluidsynth.service
           │   │ │ │ └─1386 /usr/bin/fluidsynth -is /usr/share/sounds/sf3/default-GM.sf3
           │   │ │ └─dbus.service
           │   │ │   └─1403 /usr/bin/dbus-daemon --session --address=systemd: --nofork --nopidfile --systemd-activation --syslog-only
           │   │ └─init.scope
           │   │   ├─1379 /lib/systemd/systemd --user
           │   │   └─1380 (sd-pam)
           │   └─session-1.scope
           │     ├─1348 sshd: ubuntu [priv]
           │     ├─1500 sshd: ubuntu@pts/0
           │     ├─1501 -bash
           │     ├─1510 sudo systemctl status
           │     ├─1511 sudo systemctl status
           │     ├─1512 systemctl status
           │     └─1513 less
           ├─init.scope
           │ └─1 /sbin/init fixrtc splash
           └─system.slice
             ├─irqbalance.service
             │ └─760 /usr/sbin/irqbalance --foreground
             ├─systemd-networkd.service
             │ └─742 /lib/systemd/systemd-networkd
             ├─systemd-udevd.service
             │ └─446 /lib/systemd/systemd-udevd
             ├─cron.service
             │ └─1132 /usr/sbin/cron -f -P
             ├─system-serial\x2dgetty.slice
             │ └─serial-getty@ttyS0.service
             │   └─1170 /sbin/agetty -o -p -- \u --keep-baud 115200,57600,38400,9600 ttyS0 vt220
             ├─otbr-web.service
             │ └─1169 /usr/sbin/otbr-web
             ├─polkit.service
             │ └─770 /usr/libexec/polkitd --no-debug
             ├─networkd-dispatcher.service
             │ └─762 /usr/bin/python3 /usr/bin/networkd-dispatcher --run-startup-triggers
             ├─bluetooth.service
             │ └─985 /usr/lib/bluetooth/bluetoothd
             ├─multipathd.service
             │ └─435 /sbin/multipathd -d -s
             ├─wpa_supplicant.service
             │ └─787 /sbin/wpa_supplicant -u -s -i wlan0 -c /etc/wpa_supplicant/wpa_supplicant.conf
             ├─ModemManager.service
             │ └─953 /usr/sbin/ModemManager
             ├─systemd-journald.service
             │ └─399 /lib/systemd/systemd-journald
             ├─unattended-upgrades.service
             │ └─963 /usr/bin/python3 /usr/share/unattended-upgrades/unattended-upgrade-shutdown --wait-for-signal
             ├─ssh.service
             │ └─1173 sshd: /usr/sbin/sshd -D [listener] 0 of 10-100 startups
             ├─NetworkManager.service
             │ └─756 /usr/sbin/NetworkManager --no-daemon
             ├─snapd.service
             │ └─781 /usr/lib/snapd/snapd
             ├─hciuart.service
             │ └─935 /usr/bin/hciattach /dev/serial1 bcm43xx 3000000 flow -
             ├─rsyslog.service
             │ └─773 /usr/sbin/rsyslogd -n -iNONE
             ├─update-notifier-download.service
             │ └─1520 /usr/bin/python3 /usr/lib/update-notifier/package-data-downloader
             ├─systemd-resolved.service
             │ └─744 /lib/systemd/systemd-resolved
             ├─otbr-agent.service
             │ └─1282 /usr/sbin/otbr-agent -I wpan0 -B wlan0 spinel+hdlc+uart:///dev/ttyACM0 trel://wlan0
             ├─dbus.service
             │ └─755 @dbus-daemon --system --address=systemd: --nofork --nopidfile --systemd-activation --syslog-only
             ├─systemd-timesyncd.service
             │ └─688 /lib/systemd/systemd-timesyncd
             ├─system-getty.slice
             │ └─getty@tty1.service
             │   └─1172 /sbin/agetty -o -p -- \u --noclear tty1 linux
             ├─mdns.service
             │ └─1159 /usr/sbin/mdnsd
             ├─avahi-daemon.service
             │ ├─754 avahi-daemon: running [ubuntu-15.local]
             │ └─789 avahi-daemon: chroot helper
             └─systemd-logind.service
               └─783 /lib/systemd/systemd-logind


然后我检查一下服务:
sudo systemctl --failed
  UNIT           LOAD   ACTIVE SUB    DESCRIPTION
● iipsrv.service loaded failed failed IIPImage server

LOAD   = Reflects whether the unit definition was properly loaded.
ACTIVE = The high-level unit activation state, i.e. generalization of SUB.
SUB    = The low-level unit activation state, values depend on unit type.
1 loaded units listed.


sudo service mdns status
● mdns.service - LSB: Apple Multicast DNS / DNS Service Discovery daemon
     Loaded: loaded (/etc/init.d/mdns; generated)
     Active: active (running) since Tue 2023-08-29 09:31:41 UTC; 15h ago
       Docs: man:systemd-sysv-generator(8)
    Process: 1122 ExecStart=/etc/init.d/mdns start (code=exited, status=0/SUCCESS)
      Tasks: 1 (limit: 4416)
     Memory: 1.2M
        CPU: 478ms
     CGroup: /system.slice/mdns.service
             └─1159 /usr/sbin/mdnsd


sudo service otbr-agent status
● otbr-agent.service - OpenThread Border Router Agent
     Loaded: loaded (/lib/systemd/system/otbr-agent.service; enabled; vendor preset: enabled)
     Active: active (running) since Wed 2023-08-30 00:41:06 UTC; 12min ago
    Process: 1276 ExecStartPre=/usr/sbin/service mdns start (code=exited, status=0/SUCCESS)
   Main PID: 1282 (otbr-agent)
      Tasks: 1 (limit: 4416)
     Memory: 1012.0K
        CPU: 1.518s
     CGroup: /system.slice/otbr-agent.service
             └─1282 /usr/sbin/otbr-agent -I wpan0 -B wlan0 spinel+hdlc+uart:///dev/ttyACM0 trel://wlan0


sudo service otbr-web status
● otbr-web.service - Border Router Web
     Loaded: loaded (/lib/systemd/system/otbr-web.service; enabled; vendor preset: enabled)
     Active: active (running) since Tue 2023-08-29 09:31:41 UTC; 15h ago
   Main PID: 1169 (otbr-web)
      Tasks: 1 (limit: 4416)
     Memory: 1.9M
        CPU: 15ms
     CGroup: /system.slice/otbr-web.service
             └─1169 /usr/sbin/otbr-web

Aug 29 09:31:41 ubuntu systemd[1]: Started Border Router Web.
Aug 29 09:31:41 ubuntu otbr-web[1169]: otbr-web[1169]: [INFO]-WEB-----: Running 0.3.0-thread-reference-20230119-276-g8299da302a
Aug 29 09:31:41 ubuntu otbr-web[1169]: otbr-web[1169]: [INFO]-WEB-----: Border router web started on wpan0
Aug 29 09:31:41 ubuntu otbr-web[1169]: otbr-web[1169]: [ERR ]-WEB-----: OpenThread daemon is not running.
Aug 29 09:31:41 ubuntu otbr-web[1169]: [INFO]-WEB-----: Running 0.3.0-thread-reference-20230119-276-g8299da302a
Aug 29 09:31:41 ubuntu otbr-web[1169]: [INFO]-WEB-----: Border router web started on wpan0
Aug 29 09:31:41 ubuntu otbr-web[1169]: [ERR ]-WEB-----: OpenThread daemon is not running.

如何解决此问题?
此致、
Seamus
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Seamus:

    由于该问题可能与 CC2652R7不直接相关、因此您的问题可能更适合作为 ot-br-POSIX Github 问题。  在 OTBR 编译过程中是否观察到任何错误?  重置 RPi4后、尝试打开 ot-ctl 会话时会出现什么情况?  确保 CC2652R7正确连接、并填充反向通道 XDS110 UART 接头等。

    此致、
    瑞安

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ryan、

    感谢您的回复!   或许我能 找到有关 ot-br-POSIX Github 问题的答案。  

    关于 RCP 器件、我需要向您确认的另一件事是、我能否在基于 Windows 的 CCS 上构建和刷写 RCP 器件、还是我是否需要使用 Linux 版本?

    此致、

    Seamus

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    要构建 RCP 和 Matter 示例、我认为您必须使用 GitHub 源代码在 Linux 基础上构建。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 YiPai:

    感谢您的答复。 我最初认为只有 Matter 终端设备或 Matter 控制器需要通过 Linux 基础版编译。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果您希望进一步了解该解决方案的指导、则已经发布了 Matter Smifilink Academy Labs。

    此致、
    瑞安

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ryan、

    因此、如果我需要在 Linux 中编译和刷写 RCP 器件、我可以遵循  Matter Device Creation 的#Task 2 吗?  我需要更改什么?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我看到 SDK examples\rtos\LP_CC2652R7\thread\rcp 文件夹下存在 CCS Thread RCP 项目。 您可以尝试使用 CCS 12进行编译以使用 OTBR 进行测试。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    感谢您的答复。 现在、我有一点困惑、是否可以从 Windows CCS 构建和刷写该 RCP 示例、或者我仍然需要一些 GitHub 源代码并从 Linux 构建?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您可以从 Windows CCS 构建和刷写该 RCP 示例。 我们已经对其进行了测试、可以看到其正常工作。