您好,我想问一下,对于28335中写svpwm程序,从svpwm程序中得出CMPRx的幅值很小,就是脉冲周期,而所配置的EPWM模块中prd值很大,如何比较啊,有些不理解。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我想问一下,对于28335中写svpwm程序,从svpwm程序中得出CMPRx的幅值很小,就是脉冲周期,而所配置的EPWM模块中prd值很大,如何比较啊,有些不理解。谢谢
是的是的,我感觉计数值比较大,而CMPRx非常小。这是怎么理解?
我设置的pwm脉冲周期为100微秒,计数值是从0开始到PRD,PRD是7500,是吧?
而出来的TaTbTc幅值就是0.0001,比较小。所以不知道怎么理解
haixin wang 说:我设置的pwm脉冲周期为100微秒,计数值是从0开始到PRD,PRD是7500,是吧?
如果主频150MHz,增减计数方式的话,是对的
haixin wang 说:而出来的TaTbTc幅值就是0.0001,比较小。所以不知道怎么理解
0.0001是相对值吧?相对值乘以TxPR(==绝对值)如果仍小于1,那说明就是有一半桥臂一直开通,另一半桥臂一直关断
现在出来的幅值是0.0001,已经乘完了周期T,但是没有乘PRD,0.0001乘7500=0.75,还是比计数值小很多啊。。。求解,谢谢
haixin wang 说:现在出来的幅值是0.0001,已经乘完了周期T,但是没有乘PRD,0.0001乘7500=0.75,还是比计数值小很多啊。。。求解,谢谢
已被你的提问问糊涂了,感觉不能理解你到底要表达什么意思了