This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: 如何使用MCAN做CANFD通信?

Part Number: TMS320F28388D


您好!
我正在使用TMS320F28388D的CANFD通信代码,我在使用官方提供的代码时发现问题如下:
我使用的例程是MCAN_ex3_loopback_syscfg;在下载程序后进行仿真发现代码卡在while循环里面:
具体位置如下:


在这个例程中我只修改了我的晶振时钟和引脚,由25MHz变为了20Mhz,引脚由原本的GPIO30,31改为了GPIO36,37,使用了软件配置,具体如下:


请问我该如何解决这个问题,来实现CANFD的通信收发代码?

感谢答复!!