This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp28335 外部RAM仿真



.test 程序空间太大,无法放在内部RAM中运行,希望把程序放在外部RAM中运行。看了以前的问题回答还是没有实验成功。我修改如下:

1、配置芯片GPIO84~87引脚, 引导模式为Jump to XINTF x16。

2、修改CMD文件如下:

MEMORY
{
PAGE 0 :

BEGIN : origin = 0x100000, length = 0x000002
BOOT_RSVD : origin = 0x000002, length = 0x00004E
RAMM0 : origin = 0x000050, length = 0x0003B0

RAML0 : origin = 0x008000, length = 0x001000
RAML1 : origin = 0x009000, length = 0x001000
RAML2 : origin = 0x00A000, length = 0x001000
RAML3 : origin = 0x00B000, length = 0x001000
ZONE6A : origin = 0x100000, length = 0x00FC00 /* XINTF zone 6 - program space */
CSM_RSVD : origin = 0x33FF80, length = 0x000076 
CSM_PWL : origin = 0x33FFF8, length = 0x000008
ADC_CAL : origin = 0x380080, length = 0x000009
RESET : origin = 0x3FFFC0, length = 0x000002
IQTABLES : origin = 0x3FE000, length = 0x000b50
IQTABLES2 : origin = 0x3FEB50, length = 0x00008c
FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0
BOOTROM : origin = 0x3FF27C, length = 0x000D44


PAGE 1 :
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML4 : origin = 0x00C000, length = 0x001000
RAML5 : origin = 0x00D000, length = 0x001000
RAML6 : origin = 0x00E000, length = 0x001000
RAML7 : origin = 0x00F000, length = 0x001000
ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAML0, PAGE = 0
.text : > ZONE6A , PAGE = 0
.cinit : > RAML0, PAGE = 0
.pinit : > RAML0, PAGE = 0
.switch : > RAML0, PAGE = 0

.stack : > RAMM1, PAGE = 1
.ebss : > RAML4, PAGE = 1
.econst : > RAML5, PAGE = 1
.esysmem : > RAMM1, PAGE = 1

IQmath : > RAML1, PAGE = 0
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

DMARAML4 : > RAML4, PAGE = 1
DMARAML5 : > RAML5, PAGE = 1
DMARAML6 : > RAML6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1

ZONE7DATA : > ZONE7B, PAGE = 1

.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used */
csm_rsvd : > CSM_RSVD PAGE = 0, TYPE = DSECT /* not used for SARAM examples */
csmpasswds : > CSM_PWL PAGE = 0, TYPE = DSECT /* not used for SARAM examples */

/* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
.adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD

3、程序中使用:init_zone6();

还是没有成功,我还需要修改哪里或者在哪里加程序。

CMD文件修改的对吗?