As shown in the figure, the typical value of the erasure time for a single 8k sector of the TMS320F28035 is 2 seconds, and the maximum value is 12 seconds.
Now,There are two questions.
1. What is the approximate proportion of samples with a maximum erasure time of 12 seconds among the randomly produced samples?
2. What is the maximum erasure time for a single 8k sector after exceeding the erasure cycle by 100?
Thanks.