This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过测试仿真器的接口EMU0和1,发现EMU0为低电平,EMU1为高电平。似乎是进入了WIR模式。
将仿真器连接上,通过SCI引导重启后,连接仿真器看到寄存器MWIR为2,与端口上的电平逻辑一致。
通过手动更改MWIR的值,在通过C2Prog可以实现目标板自动波特率的锁定,但是后面就又不行了。
再看MWIR寄存器还是为2,又变回去了。
每次重启后都是这样,MWIR的值无法更改。
通过更改MWIR之后,之前描述的串口TX信号线也立即由低变为高。
大家能告诉怎么样更改这个值么? 为什么这个值为会为2而不是其他的值。
导致我正好进入了WIR中无法自拔。
你好
需要那么复杂吗?你是给M3还是C28下载。如果是M3只需要让GPIO34,35,47,43 为0,0,1,0. PA0-RX PA1-TX 就可以了。