This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035 SCI下载的bootloader出厂固化了吗



就是出厂时的BootLoader中包含通过SCI串口下载程序吗

  • 是的,具体的传输格式为:可以在TI网站搜索SPRUGO0A文档得到详细信息。

    AA 08 ; 0x08AA 8-bit key value

    00 00 00 00 ; 8 reserved words

    00 00 00 00

    00 00 00 00

    00 00 00 00

    3F 00 00 80 ; 0x003F8000 EntryAddr, starting point after boot load completes

    05 00 ; 0x0005 - First block consists of 5 16-bit words

    3F 00 10 90 ; 0x003F9010 - First block will be loaded starting at 0x3F9010

    01 00 ; Data loaded = 0x0001 0x0002 0x0003 0x0004 0x0005

    02 00

    03 00

    04 00

    05 00

    02 00 ; 0x0002 - 2nd block consists of 2 16-bit words

    3F 00 00 80 ; 0x003F8000 - 2nd block will be loaded starting at 0x3F8000

    00 77 ; Data loaded = 0x7700 0x7625

    25 76

    00 00 ; 0x0000 - Size of 0 indicates end of data stream

    After load has completed the following memory values will have been initialized as follows:

    Location Value

    0x3F9010 0x0001

    0x3F9011 0x0002

    0x3F9012 0x0003

    0x3F9013 0x0004

    0x3F9014 0x0005

    0x3F8000 0x7700

    0x3F8001 0x7625

    PC Begins execution at 0x3F8000

  • 嗯 固化了,请楼主下载Boot Rom User Guide,上面写的很清楚。