Part Number: TMS320F28P650DK
从Table 17-4. Analog Internal Connections可以看出GPIO224到GPIO242这些引脚类型为AIO,从14.3和17.3章节内容来看AIO的引脚默认工作在AD模式,是不需要配置的,那Table 17-26. AGPIOCTRLH Register Field Descriptions里面为什么又会有对这些IO的AGPIOCTRLx.GPIOy的配置,个人认为手册有误
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28P650DK
从Table 17-4. Analog Internal Connections可以看出GPIO224到GPIO242这些引脚类型为AIO,从14.3和17.3章节内容来看AIO的引脚默认工作在AD模式,是不需要配置的,那Table 17-26. AGPIOCTRLH Register Field Descriptions里面为什么又会有对这些IO的AGPIOCTRLx.GPIOy的配置,个人认为手册有误
您好
我认为AGPIO和AIO之间存在一些混淆。根据第14.3和14.4节,AIO引脚是一个GPIO,它“与模拟引脚多路复用,仅具有数字输入功能”,而AGPIO引脚“与模拟针脚多路复用,具有数字输入和输出功能”,强调数字输入和输入功能。
在表17-4中,AGPIO引脚(表中称为“GPIO”)不包括224-242的范围,但确实包括该范围内的AIO引脚。此外,寄存器AGPIOCTRLH(表17-26)配置AGPIO引脚(在这种情况下为224-242)是否可以与模拟输入复用。
将AGPIOCTRLx视为模拟输入启用,将GPxAMSEL视为多路复用器选择(见表14-2,注意当AGPIOCTRL为0且GPxAMSIL选择模拟输入时,“无信号连接”是一个选项)。