Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: LAUNCHXL-F28P65X
我尝试将F28P65的spi_ex3_external_loopback示例工程修改为DMA传输,但是始终无法成功,无法进入DMA中断,同时使用逻辑分析仪无法捕捉到正常的SPI信号,但如果不使用DMA SPI通信正常,想咨询一下我的代码处理在哪里还有问题。完整工程见附件,我的测试平台是 LAUNCHXL-F28P65X 开发版,使用SPIA作为从,SPID作为主形成外部回环。
//#############################################################################
//
// FILE: spi_ex3_external_loopback.c
//
// TITLE: SPI Digital Loopback without using FIFOs and Interrupts
//
//! \addtogroup driver_example_list
//! <h1>SPI Digital External Loopback without FIFO Interrupts</h1>
//!
//! This program uses the external loopback between two SPI modules. Both
//! the SPI FIFOs and interrupts are not used in this example. SPIA is
//! configured as a peripheral and SPI B is configured as controller. This example
//! demonstrates full duplex communication where both controller and peripheral transmits
//! and receives data simultaneously.
//!
//
//#############################################################################
// $Copyright:
// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "CPU1_RAM/syscfg/board.h"
#include "driverlib.h"
#include "device.h"
#include "board.h"
#include <string.h>
//
// SPI_peripheral
//
#define SPI_peripheral_BASE SPIA_BASE
// slave SPIA --> SPIA
// GPIO201 MOSI --> GPIO16
// GPIO202 MISO --> GPIO17
// GPIO203 CLK --> GPIO18
// GPIO204 CS --> GPIO57
//
// PICO - MOSI
#define SPI_peripheral_SPIPICO_GPIO 16
#define SPI_peripheral_SPIPICO_PIN_CONFIG GPIO_16_SPIA_PICO
// POCI - MISO
#define SPI_peripheral_SPIPOCI_GPIO 17
#define SPI_peripheral_SPIPOCI_PIN_CONFIG GPIO_17_SPIA_POCI
// CLK - CLK
#define SPI_peripheral_SPICLK_GPIO 18
#define SPI_peripheral_SPICLK_PIN_CONFIG GPIO_18_SPIA_CLK
// PTE - CS
#define SPI_peripheral_SPIPTE_GPIO 57
#define SPI_peripheral_SPIPTE_PIN_CONFIG GPIO_57_SPIA_PTE
//
// SPI_controller Pinmux
//
#define SPI_controller_BASE SPID_BASE
// master SPIB --> SPID
// GPIO58 MOSI --> GPIO91
// GPIO59 MISO --> GPIO92
// GPIO60 CLK --> GPIO93
// GPIO61 CS --> GPIO94
//
// PICO - MOSI
#define SPI_controller_SPIPICO_GPIO 91
#define SPI_controller_SPIPICO_PIN_CONFIG GPIO_91_SPID_PICO
// POCI - MISO
#define SPI_controller_SPIPOCI_GPIO 92
#define SPI_controller_SPIPOCI_PIN_CONFIG GPIO_92_SPID_POCI
// CLK - CLK
#define SPI_controller_SPICLK_GPIO 93
#define SPI_controller_SPICLK_PIN_CONFIG GPIO_93_SPID_CLK
// PTE - CS
#define SPI_controller_SPIPTE_GPIO 94
#define SPI_controller_SPIPTE_PIN_CONFIG GPIO_94_SPID_PTE
void UserPinMux_init()
{
//
// PinMux for modules assigned to CPU1
//
// SPI_peripheral Pinmux
GPIO_setPinConfig(SPI_peripheral_SPIPICO_PIN_CONFIG);
GPIO_setPadConfig(SPI_peripheral_SPIPICO_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_peripheral_SPIPICO_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_peripheral_SPIPOCI_PIN_CONFIG);
GPIO_setPadConfig(SPI_peripheral_SPIPOCI_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_peripheral_SPIPOCI_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_peripheral_SPICLK_PIN_CONFIG);
GPIO_setPadConfig(SPI_peripheral_SPICLK_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_peripheral_SPICLK_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_peripheral_SPIPTE_PIN_CONFIG);
GPIO_setPadConfig(SPI_peripheral_SPIPTE_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_peripheral_SPIPTE_GPIO, GPIO_QUAL_ASYNC);
// SPI_controller Pinmux
GPIO_setPinConfig(SPI_controller_SPIPICO_PIN_CONFIG);
GPIO_setPadConfig(SPI_controller_SPIPICO_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_controller_SPIPICO_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_controller_SPIPOCI_PIN_CONFIG);
GPIO_setPadConfig(SPI_controller_SPIPOCI_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_controller_SPIPOCI_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_controller_SPICLK_PIN_CONFIG);
GPIO_setPadConfig(SPI_controller_SPICLK_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_controller_SPICLK_GPIO, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(SPI_controller_SPIPTE_PIN_CONFIG);
GPIO_setPadConfig(SPI_controller_SPIPTE_GPIO, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(SPI_controller_SPIPTE_GPIO, GPIO_QUAL_ASYNC);
}
void UserSPI_peripheral_init(){
SPI_disableModule(SPI_peripheral_BASE);
SPI_setConfig(SPI_peripheral_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
SPI_MODE_PERIPHERAL, 500000, 16);
SPI_setPTESignalPolarity(SPI_peripheral_BASE, SPI_PTE_ACTIVE_LOW);
SPI_disableFIFO(SPI_peripheral_BASE);
SPI_disableLoopback(SPI_peripheral_BASE);
SPI_setEmulationMode(SPI_peripheral_BASE, SPI_EMULATION_FREE_RUN);
SPI_enableModule(SPI_peripheral_BASE);
}
void UserSPI_controller_init(){
SPI_disableModule(SPI_controller_BASE);
SPI_setConfig(SPI_controller_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
SPI_MODE_CONTROLLER, 500000, 16);
SPI_setPTESignalPolarity(SPI_controller_BASE, SPI_PTE_ACTIVE_LOW);
SPI_disableFIFO(SPI_controller_BASE);
SPI_disableLoopback(SPI_controller_BASE);
SPI_setEmulationMode(SPI_controller_BASE, SPI_EMULATION_FREE_RUN);
SPI_enableModule(SPI_controller_BASE);
}
void UserSPI_init(){
UserSPI_peripheral_init();
UserSPI_controller_init();
}
typedef struct
{
uint16_t pinId; //gpio的pin脚
uint16_t cpuId; //使用cpu1还是cpu2
uint32_t gpioMux; //gpio引脚的复用
uint16_t gpioDir; //gpio引脚的方向:输入/输出
uint16_t gpioPull; //gpio是否需要上拉
uint32_t analogMode; //是否是模拟引脚
}GpioCfg_Stu;
static void gpioX_Init(const GpioCfg_Stu *gpioInit)
{
GPIO_setControllerCore(gpioInit->pinId, (GPIO_CoreSelect)gpioInit->cpuId);
GPIO_setPinConfig(gpioInit->gpioMux);
GPIO_setDirectionMode(gpioInit->pinId, (GPIO_Direction)gpioInit->gpioDir);
GPIO_setPadConfig(gpioInit->pinId, gpioInit->gpioPull);
if((gpioInit->gpioMux & 0xf) != 0)
GPIO_setQualificationMode(gpioInit->pinId, GPIO_QUAL_ASYNC);
if (((gpioInit->pinId >= 198U) && (gpioInit->pinId <= 242U)) || (gpioInit->pinId == 42U) || (gpioInit->pinId == 43U))
{
if(gpioInit->analogMode == GPIO_ANALOG_ENABLED)
GPIO_setAnalogMode(gpioInit->pinId, GPIO_ANALOG_ENABLED);
else
GPIO_setAnalogMode(gpioInit->pinId, GPIO_ANALOG_DISABLED);
}
}
typedef struct SpiPal{
uint16_t spiId;
uint32_t base;
uint32_t msgNum;
SPI_Mode mode;
SPI_TransferProtocol protocol;
SPI_PTEPolarity csPolarity;
uint32_t bitRate;
uint16_t dataBitWidth;
uint8_t busy;
void* buff;
uint32_t buffSize;
struct {
GpioCfg_Stu cs, clk, miso, mosi;
}gpio;
struct {
uint32_t dmaChBase;
}tx;
struct {
uint32_t dmaChBase;
void (*callback)(void* cbData);
void* cbData;
uint16_t* pReadBuf;
}rx;
}SpiPal_Stu;
#pragma DATA_SECTION(dmaBuff, "ramgs0");
#define MAX_SPI_TXRX_BUFF_LEN 256
uint16_t dmaBuff[6][MAX_SPI_TXRX_BUFF_LEN] = {0};
SpiPal_Stu spi[4] = {0};
static SpiPal_Stu* SpiPal_DmaChToSpiHandle(uint32_t dmaChBase)
{
uint16_t i = 0;
for (i = 0; i < sizeof(spi)/sizeof(spi[0]); i++) {
if ((spi[i].tx.dmaChBase == dmaChBase) || (spi[i].rx.dmaChBase == dmaChBase))
{
return &spi[i];
}
}
return NULL;
}
static void SpiPal_SlaveDmaHandler(SpiPal_Stu* handle, uint32_t chBase)
{
DMA_clearErrorFlag(chBase);
if (DMA_getOverflowFlag(chBase))
return;
if (handle->rx.dmaChBase == chBase)
{
// rx dma channal
memcpy(handle->rx.pReadBuf, handle->buff, handle->msgNum);
DMA_stopChannel(handle->rx.dmaChBase);
DMA_triggerSoftReset(handle->rx.dmaChBase);
SPI_disableModule(handle->base);
SPI_enableModule(handle->base);
handle->busy = 0;
if (handle->rx.callback)
{
handle->rx.callback(handle->rx.cbData);
}
} else if (handle->tx.dmaChBase == chBase)
{
// tx dma channal, do nothing
DMA_stopChannel(handle->tx.dmaChBase);
DMA_triggerSoftReset(handle->tx.dmaChBase);
}else
{
}
}
#define SPIPAL_DMA_LIST(_do)\
_do(1)\
_do(2)\
_do(3)\
_do(4)\
_do(5)\
_do(6)
#define SPIPAL_IRQ_HANDLER(_ch) \
__interrupt void SpiPal_SlaveDmaCh##_ch##Handler(void) \
{ \
SpiPal_Stu* spiHandle = SpiPal_DmaChToSpiHandle(DMA_CH##_ch##_BASE); \
SpiPal_SlaveDmaHandler(spiHandle, DMA_CH##_ch##_BASE); \
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7); \
}
SPIPAL_DMA_LIST(SPIPAL_IRQ_HANDLER)
static void* SpiPal_DmaToChIsrHandler(uint32_t chBase)
{
switch(chBase)
{
case DMA_CH1_BASE:
return SpiPal_SlaveDmaCh1Handler;
case DMA_CH2_BASE:
return SpiPal_SlaveDmaCh2Handler;
case DMA_CH3_BASE:
return SpiPal_SlaveDmaCh3Handler;
case DMA_CH4_BASE:
return SpiPal_SlaveDmaCh4Handler;
case DMA_CH5_BASE:
return SpiPal_SlaveDmaCh5Handler;
case DMA_CH6_BASE:
return SpiPal_SlaveDmaCh6Handler;
default:
return NULL;
}
}
static uint32_t SpiPal_DmaToChIsr(uint32_t chBase)
{
switch(chBase)
{
case DMA_CH1_BASE:
return INT_DMA_CH1;
case DMA_CH2_BASE:
return INT_DMA_CH2;
case DMA_CH3_BASE:
return INT_DMA_CH3;
case DMA_CH4_BASE:
return INT_DMA_CH4;
case DMA_CH5_BASE:
return INT_DMA_CH5;
case DMA_CH6_BASE:
return INT_DMA_CH6;
default:
return 0;
}
}
static int32_t SpiPal_RxDmaInit(SpiPal_Stu* spiHandle)
{
uint32_t config = 0;
if (spiHandle->dataBitWidth == 16)
config = DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT;
else if (spiHandle->dataBitWidth == 32)
config = DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_32BIT;
else
return -1;
DMA_setEmulationMode(DMA_EMULATION_STOP);
DMA_Trigger dmaRxTriggerMap[] = {DMA_TRIGGER_SPIARX, DMA_TRIGGER_SPIBRX, DMA_TRIGGER_SPICRX, DMA_TRIGGER_SPIDRX};
DMA_configAddresses(spiHandle->rx.dmaChBase, spiHandle->buff, (uint16_t *)spiHandle->base + SPI_O_RXBUF);
DMA_configBurst(spiHandle->rx.dmaChBase, 1U, 0, 1);
DMA_configTransfer(spiHandle->rx.dmaChBase, 16U, 0, 1);
DMA_configWrap(spiHandle->rx.dmaChBase, 65535U, 0, 65535U, 0);
DMA_configMode(spiHandle->rx.dmaChBase, dmaRxTriggerMap[spiHandle->spiId], config);
DMA_disableOverrunInterrupt(spiHandle->rx.dmaChBase);
DMA_setInterruptMode(spiHandle->rx.dmaChBase, DMA_INT_AT_END);
DMA_enableInterrupt(spiHandle->rx.dmaChBase);
DMA_enableTrigger(spiHandle->rx.dmaChBase);
DMA_stopChannel(spiHandle->rx.dmaChBase);
Interrupt_register(SpiPal_DmaToChIsr(spiHandle->rx.dmaChBase), (void (*)(void))SpiPal_DmaToChIsrHandler(spiHandle->rx.dmaChBase));
Interrupt_enable(SpiPal_DmaToChIsr(spiHandle->rx.dmaChBase));
return 0;
}
static int32_t SpiPal_TxDmaInit(SpiPal_Stu* spiHandle)
{
uint32_t config = 0;
if (spiHandle->dataBitWidth == 16)
config = DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_16BIT;
else if (spiHandle->dataBitWidth == 32)
config = DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_DISABLE | DMA_CFG_SIZE_32BIT;
else
return -1;
DMA_setEmulationMode(DMA_EMULATION_STOP);
DMA_Trigger dmaTxTriggerMap[] = {DMA_TRIGGER_SPIATX, DMA_TRIGGER_SPIATX, DMA_TRIGGER_SPIATX, DMA_TRIGGER_SPIATX};
DMA_configAddresses(spiHandle->tx.dmaChBase, (uint16_t *)spiHandle->base + SPI_O_TXBUF, spiHandle->buff);
DMA_configBurst(spiHandle->tx.dmaChBase, 1U, 1, 0);
DMA_configTransfer(spiHandle->tx.dmaChBase, 16U, 1, 0);
DMA_configWrap(spiHandle->tx.dmaChBase, 65535U, 0, 65535U, 0);
DMA_configMode(spiHandle->tx.dmaChBase, dmaTxTriggerMap[spiHandle->spiId], config);
DMA_disableOverrunInterrupt(spiHandle->tx.dmaChBase);
DMA_setInterruptMode(spiHandle->tx.dmaChBase, DMA_INT_AT_END);
DMA_enableInterrupt(spiHandle->tx.dmaChBase);
DMA_enableTrigger(spiHandle->tx.dmaChBase);
DMA_stopChannel(spiHandle->tx.dmaChBase);
Interrupt_register(SpiPal_DmaToChIsr(spiHandle->tx.dmaChBase), (void (*)(void))SpiPal_DmaToChIsrHandler(spiHandle->tx.dmaChBase));
Interrupt_enable(SpiPal_DmaToChIsr(spiHandle->tx.dmaChBase));
return 0;
}
static int32_t SpiPal_DmaInit(SpiPal_Stu* spiHandle)
{
SpiPal_RxDmaInit(spiHandle);
SpiPal_TxDmaInit(spiHandle);
return 0;
}
static int32_t SpiPal_PinMux_init(SpiPal_Stu* spiHandle)
{
gpioX_Init(&spiHandle->gpio.cs);
gpioX_Init(&spiHandle->gpio.clk);
gpioX_Init(&spiHandle->gpio.miso);
gpioX_Init(&spiHandle->gpio.mosi);
return 0;
}
static int32_t SPI_Hw_init(SpiPal_Stu* spiHandle)
{
SPI_disableModule(spiHandle->base);
SPI_setConfig(spiHandle->base, DEVICE_LSPCLK_FREQ, spiHandle->protocol,
spiHandle->mode, spiHandle->bitRate, spiHandle->dataBitWidth);
SPI_setPTESignalPolarity(spiHandle->base, spiHandle->csPolarity);
SPI_disableFIFO(spiHandle->base);
SPI_disableLoopback(spiHandle->base);
SPI_setEmulationMode(spiHandle->base, SPI_EMULATION_FREE_RUN);
SPI_enableModule(spiHandle->base);
return 0;
}
static SpiPal_Stu* SpiPal_idToHandle(uint16_t spiId)
{
uint16_t i = 0;
for (i = 0; i < sizeof(spi)/sizeof(spi[0]); i++)
{
if(spiId == spi[i].spiId)
return &spi[i];
}
return NULL;
}
static int32_t SpiPal_Request(uint16_t spiId, uint16_t *pWriteBuf, uint16_t *pReadBuf, uint16_t msgNum)
{
SpiPal_Stu* handle = SpiPal_idToHandle(spiId);
if (handle->busy)
return -1;
//===DMA spi receive
handle->msgNum = msgNum;
handle->rx.pReadBuf = pReadBuf;
DMA_configBurst(handle->rx.dmaChBase, 1U, 0, 1);
DMA_configTransfer(handle->rx.dmaChBase, msgNum, 0, 1);
//===DMA spi send
memcpy(handle->buff, pWriteBuf, msgNum);
DMA_configBurst(handle->tx.dmaChBase, 1U, 1, 0);
DMA_configTransfer(handle->tx.dmaChBase, msgNum, 1, 0);
DMA_triggerSoftReset(handle->rx.dmaChBase);
DMA_triggerSoftReset(handle->tx.dmaChBase);
handle->busy = 1;
DMA_startChannel(handle->rx.dmaChBase);
DMA_startChannel(handle->tx.dmaChBase);
return 0;
}
static int32_t SpiPal_Transfer(uint16_t spiId, uint16_t *pWriteBuf, uint16_t *pReadBuf, uint16_t msgNum)
{
SpiPal_Stu* handle = SpiPal_idToHandle(spiId);
SpiPal_Request(spiId, pWriteBuf, pReadBuf, msgNum);
while (handle->busy == 1);
return 0;
}
static int32_t SpiPal_Init(SpiPal_Stu* spiHandle)
{
int32_t ret = 0;
ret = SpiPal_PinMux_init(spiHandle);
if (ret != 0)
return ret;
ret = SPI_Hw_init(spiHandle);
if (ret != 0)
return ret;
ret = SpiPal_DmaInit(spiHandle);
if (ret != 0)
return ret;
return ret;
}
#define SPI_SLAVE_IDX 0
#define SPI_MASTER_IDX 1
#define SPI_SLAVE spi[SPI_SLAVE_IDX]
#define SPI_MASTER spi[SPI_MASTER_IDX]
void UserBoard_init()
{
EALLOW;
SPI_SLAVE.spiId = 0;
SPI_SLAVE.base = SPI_peripheral_BASE;
SPI_SLAVE.protocol = SPI_PROT_POL0PHA0;
SPI_SLAVE.mode = SPI_MODE_PERIPHERAL;
SPI_SLAVE.bitRate = 500000;
SPI_SLAVE.dataBitWidth = 16;
SPI_SLAVE.csPolarity = SPI_PTE_ACTIVE_LOW;
SPI_SLAVE.gpio.cs.pinId = SPI_peripheral_SPIPTE_GPIO;
SPI_SLAVE.gpio.cs.cpuId = GPIO_CORE_CPU1;
SPI_SLAVE.gpio.cs.gpioMux = SPI_peripheral_SPIPTE_PIN_CONFIG;
SPI_SLAVE.gpio.cs.gpioDir = GPIO_DIR_MODE_IN;
SPI_SLAVE.gpio.cs.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_SLAVE.gpio.cs.analogMode = GPIO_ANALOG_DISABLED;
SPI_SLAVE.gpio.clk.pinId = SPI_peripheral_SPICLK_GPIO;
SPI_SLAVE.gpio.clk.cpuId = GPIO_CORE_CPU1;
SPI_SLAVE.gpio.clk.gpioMux = SPI_peripheral_SPICLK_PIN_CONFIG;
SPI_SLAVE.gpio.clk.gpioDir = GPIO_DIR_MODE_IN;
SPI_SLAVE.gpio.clk.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_SLAVE.gpio.clk.analogMode = GPIO_ANALOG_DISABLED;
SPI_SLAVE.gpio.miso.pinId = SPI_peripheral_SPIPOCI_GPIO;
SPI_SLAVE.gpio.miso.cpuId = GPIO_CORE_CPU1;
SPI_SLAVE.gpio.miso.gpioMux = SPI_peripheral_SPIPOCI_PIN_CONFIG;
SPI_SLAVE.gpio.miso.gpioDir = GPIO_DIR_MODE_OUT;
SPI_SLAVE.gpio.miso.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_SLAVE.gpio.miso.analogMode = GPIO_ANALOG_DISABLED;
SPI_SLAVE.gpio.mosi.pinId = SPI_peripheral_SPIPICO_GPIO;
SPI_SLAVE.gpio.mosi.cpuId = GPIO_CORE_CPU1;
SPI_SLAVE.gpio.mosi.gpioMux = SPI_peripheral_SPIPICO_PIN_CONFIG;
SPI_SLAVE.gpio.mosi.gpioDir = GPIO_DIR_MODE_IN;
SPI_SLAVE.gpio.mosi.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_SLAVE.gpio.mosi.analogMode = GPIO_ANALOG_DISABLED;
SPI_SLAVE.rx.dmaChBase = DMA_CH1_BASE;
SPI_SLAVE.tx.dmaChBase = DMA_CH2_BASE;
SPI_SLAVE.buff = dmaBuff[0];
SPI_MASTER.spiId = 1;
SPI_MASTER.base = SPI_controller_BASE;
SPI_MASTER.protocol = SPI_PROT_POL0PHA0;
SPI_MASTER.mode = SPI_MODE_CONTROLLER;
SPI_MASTER.bitRate = 500000;
SPI_MASTER.dataBitWidth = 16;
SPI_MASTER.csPolarity = SPI_PTE_ACTIVE_LOW;
SPI_MASTER.gpio.cs.pinId = SPI_controller_SPIPTE_GPIO;
SPI_MASTER.gpio.cs.cpuId = GPIO_CORE_CPU1;
SPI_MASTER.gpio.cs.gpioMux = SPI_controller_SPIPTE_PIN_CONFIG;
SPI_MASTER.gpio.cs.gpioDir = GPIO_DIR_MODE_OUT;
SPI_MASTER.gpio.cs.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_MASTER.gpio.cs.analogMode = GPIO_ANALOG_DISABLED;
SPI_MASTER.gpio.clk.pinId = SPI_controller_SPICLK_GPIO;
SPI_MASTER.gpio.clk.cpuId = GPIO_CORE_CPU1;
SPI_MASTER.gpio.clk.gpioMux = SPI_controller_SPICLK_PIN_CONFIG;
SPI_MASTER.gpio.clk.gpioDir = GPIO_DIR_MODE_OUT;
SPI_MASTER.gpio.clk.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_MASTER.gpio.clk.analogMode = GPIO_ANALOG_DISABLED;
SPI_MASTER.gpio.miso.pinId = SPI_controller_SPIPOCI_GPIO;
SPI_MASTER.gpio.miso.cpuId = GPIO_CORE_CPU1;
SPI_MASTER.gpio.miso.gpioMux = SPI_controller_SPIPOCI_PIN_CONFIG;
SPI_MASTER.gpio.miso.gpioDir = GPIO_DIR_MODE_IN;
SPI_MASTER.gpio.miso.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_MASTER.gpio.miso.analogMode = GPIO_ANALOG_DISABLED;
SPI_MASTER.gpio.mosi.pinId = SPI_controller_SPIPICO_GPIO;
SPI_MASTER.gpio.mosi.cpuId = GPIO_CORE_CPU1;
SPI_MASTER.gpio.mosi.gpioMux = SPI_controller_SPIPICO_PIN_CONFIG;
SPI_MASTER.gpio.mosi.gpioDir = GPIO_DIR_MODE_OUT;
SPI_MASTER.gpio.mosi.gpioPull = GPIO_PIN_TYPE_PULLUP;
SPI_MASTER.gpio.mosi.analogMode = GPIO_ANALOG_DISABLED;
SPI_MASTER.rx.dmaChBase = DMA_CH3_BASE;
SPI_MASTER.tx.dmaChBase = DMA_CH4_BASE;
SPI_MASTER.buff = dmaBuff[1];
//UserPinMux_init();
SpiPal_PinMux_init(&SPI_SLAVE);
SpiPal_PinMux_init(&SPI_MASTER);
DMA_initController();
SpiPal_DmaInit(&SPI_SLAVE);
SpiPal_DmaInit(&SPI_MASTER);
//UserSPI_init();
SPI_Hw_init(&SPI_SLAVE);
SPI_Hw_init(&SPI_MASTER);
EDIS;
}
uint16_t TxData_Peripheral[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F};
uint16_t RxData_Peripheral[] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint16_t TxData_Controller[] = {0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F};
uint16_t RxData_Controller[] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
int16_t resault = 0;
//
// Main
//
void main(void)
{
uint16_t i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Board initialization
//
UserBoard_init();
SpiPal_Request(SPI_SLAVE_IDX, TxData_Peripheral, RxData_Peripheral, sizeof(TxData_Peripheral));
SpiPal_Transfer(SPI_MASTER_IDX, TxData_Controller, RxData_Controller, sizeof(TxData_Controller)+1);
if(0 != memcmp(TxData_Controller, RxData_Peripheral, sizeof(TxData_Peripheral)))
{
resault = -1;
ESTOP0;
}
if(0 != memcmp(TxData_Peripheral, RxData_Controller, sizeof(TxData_Peripheral)))
{
resault = -1;
ESTOP0;
}
// //
// // Loop forever. Suspend or place breakpoints to observe the buffers.
// //
// for(i = 0; i < 16; i++)
// {
// //
// // Set the TX buffer of peripheral SPI.
// //
// SPI_writeDataNonBlocking(SPI_peripheral_BASE, TxData_Peripheral[i]);
// //
// // Set the the controller TX buffer. This triggers the data transmission
// //
// SPI_writeDataNonBlocking(SPI_controller_BASE, TxData_Controller[i]);
// //
// // Read the received data
// //
// RxData_Peripheral[i] = SPI_readDataBlockingNonFIFO(SPI_peripheral_BASE);
// RxData_Controller[i] = SPI_readDataBlockingNonFIFO(SPI_controller_BASE);
// //
// // Check the received data
// //
// if(RxData_Peripheral[i] != TxData_Controller[i])
// {
// resault = -1;
// ESTOP0;
// }
// if(RxData_Controller[i] != TxData_Peripheral[i])
// {
// resault = -1;
// ESTOP0;
// }
// }
ESTOP0;
resault = 1;
//
// Loop forever
//
while(1);
}