This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000系列(28335)DSP的Flash_API的限制



API可以:
1、可以运行在静态内部SARAM中
2、配置真确的CPU频率
3、根据Flash_API列表去集成API到应用中
4、初始化PLL控制寄存器,在使用API函数前等待PLL锁住
5、初始化API回调函数指针(Flash_CallbackPtr),如果不 不用回调函数请指向NULL。如果初始化失败将会导致程序跳转到未定义位置
6、仔细阅读API关于回调函数、中断、看门狗等的限制
API不可以:
1、不能执行在flash或者OTP中,如果APIs存储在flash或者OTP中,使用前请复制到SARAM中。
2、在擦写、编程或者其他API函数操作flash和OTP存储块时,不要执行任何的中断服务程序。直到API函数完成或者退出flash和OTP,才可以执行或者操作数据空间
3、不能执行API回调函数在flash或者OTP中
4、不要停止擦除、编程当他们执行时
5、在执行擦除、编程时,不要执行代码或者从flash或者OTP数据空间里取数据。