This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049:SPI作为从机通讯和ADC同步采样产生冲突的问题

Part Number: TMS320F280049


我想请教一下各位大佬,遇到了下面这个问题,恳请提供建议和帮助,谢谢!描述和问题如下:

1.使用了SPIA,作为从机,比特为15M,FIFO的接收和发送的深度都为8,同步收发16位的200个缓存元素的缓存。

2.SPI启用了DMA的CH4(RX)、CH5(TX),都为循环模式,burst_size=8,transfer_size=25,都开启了循环模式。

3.ADC使用了EPWM的SOC触发采样,使用了三个ADC,ADC1、、ADC2、ADC3,分别采样128个数据。

4.ADC分别使用了CH1、CH2、CH3

5.问题现象:现在的工况是工作是开启ADC采样DMA发送触发完成,后函数执行FFT以及触发CLA任务完成后再次开启采样,直到工作接收停止这个循环过程;SPI配置好和主机同步后就一直通过DMA循环接收,中间不停止不重启,现在是只要不启动工作,SPI的通讯收发是正常的,但是只需开启工作,AD一直开始采样,SPI的接收FIFO就会溢出,清除标志位也一样很快还是溢出,调试看DMA的发送完成触发的时间变慢了,一溢出通讯就异常了,是因为DMA接收被ADC一直大量占用了吗,优先级比其他的低导致SPI的中断和DMA的中断响应不及时导致的,尝试了降低比特率和FIFO的阈值都起效果达不到,恳请给出好的建议!!!

下面是程序的一些配置:

void ADC_init(){
//AD_PI初始化

// ADC 初始化:写入 ADC 配置并启动 ADC
// 配置 ADC 模块的失调调整
ADC_setOffsetTrimAll(ADC_REFERENCE_EXTERNAL,ADC_REFERENCE_3_3V);
// 配置模数转换器模块预分频器。
ADC_setPrescaler(AD_PI_BASE, ADC_CLK_DIV_2_0);
// 设置转换结束脉冲的时序
ADC_setInterruptPulseMode(AD_PI_BASE, ADC_PULSE_END_OF_CONV);
// 启动模数转换器核心。
ADC_enableConverter(AD_PI_BASE);
// 延迟 1ms 以允许 ADC 有时间启动
DEVICE_DELAY_US(500);

// SOC 配置:设置 ADC EPWM 通道和触发器设置
// 禁用 SOC 突发模式。ADC_disableBurstMode
(AD_PI_BASE);
// 设置 SOC 的优先级模式。ADC_setSOCPriority
(AD_PI_BASE, ADC_PRI_ALL_ROUND_ROBIN);
// 转换开始 0 配置
// 配置 ADC 中的转换开始 (SOC) 及其中断 SOC 触发器。
// SOC 编号:0
// 触发器:ADC_TRIGGER_EPWM3_SOCA
// 通道:ADC_CH_ADCIN0
// 采样窗口:16 个 SYSCLK 周期
// 中断触发器:ADC_INT_SOC_TRIGGER_NONE
ADC_setupSOC(AD_PI_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM3_SOCA, ADC_CH_ADCIN0, 16U);
ADC_setInterruptSOCTrigger(AD_PI_BASE, ADC_SOC_NUMBER0, ADC_INT_SOC_TRIGGER_NONE);
// ADC 中断 1 配置
// SOC/EOC 编号:0
// 中断源:启用
// 连续模式:启用
ADC_setInterruptSource(AD_PI_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER0);
ADC_enableInterrupt(AD_PI_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(AD_PI_BASE, ADC_INT_NUMBER1);
ADC_enableContinuousMode(AD_PI_BASE, ADC_INT_NUMBER1);

//AD_SI初始化

// ADC Initialization: Write ADC configurations and power up the ADC
// Configures the ADC module's offset trim
ADC_setOffsetTrimAll(ADC_REFERENCE_EXTERNAL,ADC_REFERENCE_3_3V);
// Configures the analog-to-digital converter module prescaler.
ADC_setPrescaler(AD_SI_BASE, ADC_CLK_DIV_2_0);
// Sets the timing of the end-of-conversion pulse
ADC_setInterruptPulseMode(AD_SI_BASE, ADC_PULSE_END_OF_CONV);
// Powers up the analog-to-digital converter core.
ADC_enableConverter(AD_SI_BASE);
// Delay for 1ms to allow ADC time to power up
DEVICE_DELAY_US(500);

// SOC Configuration: Setup ADC EPWM channel and trigger settings
// Disables SOC burst mode.
ADC_disableBurstMode(AD_SI_BASE);
// Sets the priority mode of the SOCs.
ADC_setSOCPriority(AD_SI_BASE, ADC_PRI_ALL_ROUND_ROBIN);
// Start of Conversion 0 Configuration
// Configures a start-of-conversion (SOC) in the ADC and its interrupt SOC trigger.
// SOC number : 0
// Trigger : ADC_TRIGGER_EPWM3_SOCA
// Channel : ADC_CH_ADCIN4
// Sample Window : 16 SYSCLK cycles
// Interrupt Trigger: ADC_INT_SOC_TRIGGER_NONE
ADC_setupSOC(AD_SI_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM3_SOCA, ADC_CH_ADCIN4, 16U);
ADC_setInterruptSOCTrigger(AD_SI_BASE, ADC_SOC_NUMBER0, ADC_INT_SOC_TRIGGER_NONE);
// ADC Interrupt 1 Configuration
// SOC/EOC number : 0
// Interrupt Source: enabled
// Continuous Mode : enabled
ADC_setInterruptSource(AD_SI_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER0);
ADC_enableInterrupt(AD_SI_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(AD_SI_BASE, ADC_INT_NUMBER1);
ADC_enableContinuousMode(AD_SI_BASE, ADC_INT_NUMBER1);

//AD_SU initialization

// ADC Initialization: Write ADC configurations and power up the ADC
// Configures the ADC module's offset trim
ADC_setOffsetTrimAll(ADC_REFERENCE_EXTERNAL,ADC_REFERENCE_3_3V);
// Configures the analog-to-digital converter module prescaler.
ADC_setPrescaler(AD_SU_BASE, ADC_CLK_DIV_2_0);
// Sets the timing of the end-of-conversion pulse
ADC_setInterruptPulseMode(AD_SU_BASE, ADC_PULSE_END_OF_CONV);
// Powers up the analog-to-digital converter core.
ADC_enableConverter(AD_SU_BASE);
// Delay for 1ms to allow ADC time to power up
DEVICE_DELAY_US(500);

// SOC Configuration: Setup ADC EPWM channel and trigger settings
// Disables SOC burst mode.
ADC_disableBurstMode(AD_SU_BASE);
// Sets the priority mode of the SOCs.
ADC_setSOCPriority(AD_SU_BASE, ADC_PRI_ALL_ROUND_ROBIN);
// Start of Conversion 0 Configuration
// Configures a start-of-conversion (SOC) in the ADC and its interrupt SOC trigger.
// SOC number : 0
// Trigger : ADC_TRIGGER_EPWM3_SOCA
// Channel : ADC_CH_ADCIN0
// Sample Window : 16 SYSCLK cycles
// Interrupt Trigger: ADC_INT_SOC_TRIGGER_NONE
ADC_setupSOC(AD_SU_BASE, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM3_SOCA, ADC_CH_ADCIN0, 16U);
ADC_setInterruptSOCTrigger(AD_SU_BASE, ADC_SOC_NUMBER0, ADC_INT_SOC_TRIGGER_NONE);
// ADC Interrupt 1 Configuration
// SOC/EOC number : 0
// Interrupt Source: enabled
// Continuous Mode : enabled
ADC_setInterruptSource(AD_SU_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER0);
ADC_enableInterrupt(AD_SU_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(AD_SU_BASE, ADC_INT_NUMBER1);
ADC_enableContinuousMode(AD_SU_BASE, ADC_INT_NUMBER1);

}

void FB_start(void)
{
EPWM_clearADCTriggerFlag(EPWM_AD_BASE, EPWM_SOC_A);

ADC_clearInterruptStatus(AD_PI_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(AD_SI_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(AD_SU_BASE, ADC_INT_NUMBER1);

DMA_clearTriggerFlag(DMA_CH1_BASE);
DMA_clearTriggerFlag(DMA_CH2_BASE);
DMA_clearTriggerFlag(DMA_CH3_BASE);


// Clearing all pending interrupt flags & Start DMA
//DMA_clearTriggerFlag(DMA_CH1_BASE);
DMA_startChannel(DMA_CH1_BASE);
//DMA_clearTriggerFlag(DMA_CH2_BASE);
DMA_startChannel(DMA_CH2_BASE);
//DMA_clearTriggerFlag(DMA_CH3_BASE);
DMA_startChannel(DMA_CH3_BASE);

EPWM_enableADCTrigger(EPWM_AD_BASE, EPWM_SOC_A);
}

SPI配置:

SPi_To_N32_Init();
// //
// // 初始化 DMA
// //
// DMA_initController();
DMA_triggerSoftReset(DMA_CH4_BASE);
DMA_triggerSoftReset(DMA_CH5_BASE);
//------------------------------------------------------------------------------------------------------------------------------------------------
// 为 SPI_RX 设置 DMA 通道 4
DMA_configAddresses(DMA_CH4_BASE, (uint16_t *)DSP_RxArray, (uint16_t *)(SCR_SPI_BASE + SPI_O_RXBUF));
// 执行足够的 16 字突发以填充结果缓冲区。数据将以
每次 32 位 // 的速度传输,因此地址步骤如下。DMA_configBurst
(DMA_CH4_BASE, burst_size, 0, 1);
DMA_configTransfer(DMA_CH4_BASE, transfer_size, 0, 1);
DMA_configMode(DMA_CH4_BASE,DMA_TRIGGER_SPIARX,(DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_ENABLE | DMA_CFG_SIZE_16BIT));

//
// 配置 DMA Ch4 中断
//
DMA_setInterruptMode(DMA_CH4_BASE, DMA_INT_AT_END);
DMA_enableInterrupt(DMA_CH4_BASE);
DMA_enableTrigger(DMA_CH4_BASE);

// 为 SPI_TX 设置 DMA 通道 5
DMA_configAddresses(DMA_CH5_BASE, (uint16_t *)(SCR_SPI_BASE + SPI_O_TXBUF), (uint16_t *)DSP_TxArray);
// 执行足够的 16 字突发以填充结果缓冲区。数据将以
每次 32 位的速度传输,因此地址步骤如下。DMA_configBurst
(DMA_CH5_BASE, burst_size, 1, 0);
DMA_configTransfer(DMA_CH5_BASE, transfer_size, 1, 0);
DMA_configMode(DMA_CH5_BASE, DMA_TRIGGER_SPIATX, (DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_ENABLE | DMA_CFG_SIZE_16BIT));

//
// 配置 DMA Ch5 中断
//
DMA_setInterruptMode(DMA_CH5_BASE, DMA_INT_AT_END);
DMA_enableInterrupt(DMA_CH5_BASE);
DMA_enableTrigger(DMA_CH5_BASE);

//SCR_SPI 初始化
SPI_disableModule(SCR_SPI_BASE);
SPI_clearInterruptStatus(SCR_SPI_BASE, SPI_INT_RXFF | SPI_INT_TXFF);
SPI_setFIFOInterruptLevel(SCR_SPI_BASE, SPI_FIFO_TX8, SPI_FIFO_RX8);
SPI_setConfig(SCR_SPI_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA1,
SPI_MODE_SLAVE, 15000000, 16);
SPI_disableLoopback(SCR_SPI_BASE);
SPI_enableFIFO(SCR_SPI_BASE);
SPI_setEmulationMode(SCR_SPI_BASE, SPI_EMULATION_STOP_MIDWAY);
SPI_enableInterrupt(SCR_SPI_BASE, SPI_INT_RXFF | SPI_INT_TXFF);
SPI启用模块(SCR_SPI_基座);

//SPI_FIFO
DMA_启动通道(DMA_CH4_BASE);
DMA_启动通道(DMA_CH5_BASE);

}

  • 感谢您对TI产品的关注!
    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 好的,感谢!

  • 好的,感谢!

  • 您好,

         DMA模块一次只能为一个通道执行传输。

        因此,是的,您提到的问题确实存在,当使用通道1-3时,通道4-5之间的每次传输会有一些延迟,因为其他通道也需要服务。

       几个问题:配置的是哪种通道优先级模式 - 通道1优先级模式还是轮询模式?

       我认为这两者都有问题,但特别是通道1优先级模式可能会导致其他通道被阻塞。

       每个ADC DMA通道传输多少数据?是否可以减少,以使这些通道的操作不需要花费太长时间?

       是否可以让发送的SPI设备在发送每8个元素之间插入延迟,以便DMA有时间服务其他通道?

       我还建议的另一个选项是使用CLA任务来进行SPI操作,而不是使用DMA。

       这样,CLA可以用于SPI操作,并且DMA可以同时处理ADC数据。

  • 十分感谢您的回复!!!
    通道1优先模式及轮询把SPI的接收发送放到通道1,2都尝试过了:
    1.通道1优先模式会导致通道和DMA长时间阻塞,特殊情况还会引起错误中断。
    2.SPI的接收发送放到通道1,2和放在4,5在轮询方式下并没有太大差异。
    3.每个ADC都是128个数据,要用做FIFO运算,所以点数不能再减少了。
    4.中间插入延时这个可以尝试下,因为会涉及到协议和同步问题。
    5.最后一个建议我重点尝试下,可以使用CLA来处理SPI,但是我还有个问题,就是现在的CLA还用来做HPWM的控制调节和两个增量式的PID闭环,用CLA任务来处理SPI会不会导致和DMA一样占用阻塞时间过长导致其他任务响应不及时,因为CLA任务也是通过触发源还有优先级去执行的。
    期待您的回复,谢谢!!!

  • 您好,

          如果在通道1优先级模式下对CH1进行SPI操作没有解决问题,那么您能做的也不多。

          我明白了,是的,如果CLA上有其他高频任务在运行,您可能会遇到类似的问题。这些任务的频率和ADC SOC一样吗?

         需要注意的是,这个设备的CLA还有一个可选的后台任务(任务8),可能会被更高优先级的任务打断。有关详细信息,请参见TRM部分。

         如果CLA上的某个任务被触发得非常频繁,并且阻塞了SPI任务,您可以将其设为后台任务,并允许SPI任务在收到SPI任务触发时打断它。对于CLA的另一个选项是,由于其在逻辑上有些灵活,您还可以将SPI操作与其他频繁任务中的操作配对。例如,在HRPWM控制调整任务结束时,您可以检查SPI标志是否被设置,如果需要则接收SPI数据。或者,是否不可以在主CPU上使用SPI ISR?通过这种方式,您可以使用中断嵌套来确保SPI操作始终优先完成。