Part Number: TMS320F28375S
Other Parts Discussed in Thread: C2000WARE
尊敬的工程师您好:
我再使用fpu32的时候遇到了一个问题,我发现在系统启动之前,也就是在main函数中的BIOS_start函数启动之前,不能进行正常的除法运算,除法运算不执行,得到的结果是0。但是bios启动之后,又可以正常工作。是什么原因呢,配置如下,谢谢
应用的库是cla1_math_library_fpu32.libs 因为CLA需要函数


Int main()
{
// Step 0. Copy Key Code from Flash into RAM
memcpy((uint16_t *)&RamfuncsRunStart, (uint16_t *) &RamfuncsLoadStart, (unsigned long) &RamfuncsLoadSize);
// Copy over code from FLASH to RAM
memcpy(&Cla1funcsRunStart, &Cla1funcsLoadStart, (Uint32)&Cla1funcsLoadSize);
memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
//例如有些事中就没有使用,那么就应该把他禁止
//这个函数里面还增添了将SPI SCI McBSP的时钟输入提高到200MHz
PeripheralsClocksInit();
CLA_configClaMemory();
CLA_initCpu1Cla1();
GpioInit();
DELAY_US(100000);
AllPeripheralsInit(); //把所有的外设初始化
DELAY_US(100000);
DYNRegisterInit(); //把寄存器都读取出来这里面有浮点数除法,计算不正确
BIOS_start(); /* does not return */
return(0);
}
Void SystemInitTaskFxn(UArg a0, UArg a1)
{
DYNRegisterInitCalc(); //这里也有浮点除法,但是可以计算正确
PlayMusic(0,2); //播放开机声音
}