Part Number: TMS320F28377D
尊敬的TI技术支持您好,我使用的CCS12.8.1
工程编译后提示:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
IcePick_C_0: Trouble Reading Memory Block at 0x0 on Page 0 of Length 0xc8
不知道怎么解决,希望得到您的帮助!
还有就是我最近在开发设备中,CCS处于debug模式,但如果此时周围器件突然接入电压,会导致CCS断开,这个问题又该如何解决呢?