This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
在选择SCI BOOT时,SCIA有两种选择,
SCI-Boot0 : GPIO84和85 ,注释是: SCIA Boot IO option 1 (default SCI option when chosen through Boot Mode GPIOs)
SCI-Boot1 :GPIO29和28, 注释是:SCIA Boot option 2 – with alternate IOs.
这两个注释要怎么理解?
OPTION0和OPTION1有什么区别?
当对空片进行SCI BOOT操作时,是不是只能用GPIO84和85作为数据传输吗?
谢谢。
不好意思没有描述清楚,我是想知道
对于没有烧写过的空片子,用硬件配置成SCI BOOT后, SCA的RXD和TXD是用GPIO84\85还是GPIO27\28呢?
谢谢。