This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28332 同 28335 的FLASH 块



datasheet (SPRS439)中提到了28332/28335的FLASH空间,但是没有具体的给出每个FLASH区块的地址空间(虽然cmd文件可以看出),想请问一下:

1、28332中,FLASH有4个块,每个是16K x 16;

2、28335中,FLASH有8个块,每个是32K x 16;

为什么28335中FLASH 块的大小是28332中的一倍大小,而不采用相同大小的FLASH块呢?

谢谢!