Part Number: TMS320F28384S
我的代码需要56kB的RAM空间。芯片是F28384S。
① 我看到手册表5-1中28384S有128kB的全局共享RAM空间。但是在表8-1中,GSx_RAM(全局共享RAM)是从0x0000 D000开始到0x0001 CFFF共16个4kB的小块组成,这不是才64kB吗?剩余64kB可以用吗?地址范围是多少?虽然64kB>我需要的56kB空间,但现在我已经将0x00D000到0x014FFF分配给了别的用途,所以即便表8-1中列出了16个4kB的小块,也不够用。
② 我在模板文件2838x_flash_lnk_cpu1.cmd中也没有发现128kB的全局共享RAM地址范围以及使用方法。是否它不可以分配给代码变量的RAM(.ebss段)?