问题1:根据28377的使用说明书,芯片的BOOT0和BOOT1脚可用寄存器设置为任意管脚,像SCI烧写的管脚好像只有两对选择,GPIO84&GPIO85这一对和GPIO28&GPIO29这一对,在最初使用时需要仿真器先连接,在程序中设置BOOTCTRL寄存器中的EMU_BMODE位为0x81,表示使用SCI BOOT1这个管脚选择,此寄存器为ROM所以只设置一次就OK后期再写程序不用每次重新设置一遍,重新复位上电后,芯片就可以根据BOOT脚电平确认启动状态了,BOOT0&1=0时从FLASH启动,BOOT0=1&BOOT1=0时可以使用GPIO28&GPIO29管脚的SCI下载程序,请问这种理解正确么?
问题2:根据28377的使用说明书,在使用EPWM搭配X-bar时,要用到SYNCIN和SYNCOUT,SYNCIN可以配置成任意管脚,SYNCOUT要配置到一X-baroutput上,请问这种理解正确么?
请各位高手解答,谢谢~~~