This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28054F-Q1: 使用互感器做电流采样时,过调制算法的执行

Prodigy 110 points
Part Number: TMS320F28054F-Q1

  TI的专家,你们好:

  我在使用28054F这款主控进行项目开发时,遇到了运行母线电流受限的问题,目前怀疑是过调制算法没有正常执行;

我的项目使用的是3个电流互感器进行三相电流采样,在这种情况下如果我想让控制器输出更高的电压(即通过过调制算法提高母线电压利用率),

除了修改调制比系数(在motorware18中是0~0.6666)外,还需要做其他处理吗?当前程序的开发基于lab05a例程

因为我在查看例程lab10a时,发现在mainISR中进行了电流重构和电压补偿及采样窗口修改等处理(据我了解这些处理针对的是电阻采样电流)

  希望能够尽快得到回复,该问题影响项目上市进度!