This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: 关于tms320f28377s编译生成hex相关的问题

Part Number: TMS320F28377S

关于tms320f28377s编译生成hex相关的问题,我打开tms320f28377s的c2000里面的demo,flash_programming_cpu01工程,想生成一个hex文件。

然后我配置1、右击工程选择Properties---->C2000 Hex Utility--->勾选使能。2、Output Format Options------>Output format配置为hex文件格式,

然后我点击编译虽然生成了一个hex文件但是编译器警告Description Resource Path Location Type
Data is being written to auto-generated file flash_programming_cpu01.i01 flash_programming_cpu01 C/C++ Problem。我猜测可能需要改cmd文件,但是不知道怎么改?

网上搜索了一个相关文章参考但是没修改成功链接如下:

blog.csdn.net/.../146123971

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    如果您看到警告消息“数据正在写入自动生成的文件flash_programming_cpu01.i01”,则很可能是项目的十六进制实用程序在编译过程中没有设置指定的内存宽度或指定的ROM宽度:

    在“属性”->“工具”->“十六进制实用程序”->“常规选项”中更改此设置对您有效吗?

  •  您好,这样配置对吗?

     Specify memory width (--memwidth, -memwidth)           16

    Specify data ordering (--order, -order)                         LS

    Specify rom width (--romwidth)                                                              16

  • 您好

    I am not able to replicate the issue by generating the hex. For your project, does the hex file have a page 0 and page 1? Are you able to share your linker command file here?

  • /*
    //###########################################################################
    // FILE:    flash_programming_cpu1_FLASH.cmd
    // TITLE:   Linker Command File For all F28X7x devices
    //###########################################################################
    //
    // 
    // $Copyright:
    // Copyright (C) 2014-2024 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    // The header linker files are found in <base>\headers\cmd
    // For BIOS applications add:      F28X7x_Headers_BIOS.cmd
    // For nonBIOS applications add:   F28X7x_Headers_nonBIOS.cmd
    ========================================================= */
    
    /* Define the memory block start/length for the F28X7x
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
       Notes:
             Memory blocks on F28M3Xx are uniform (ie same
             physical memory) in both PAGE 0 and PAGE 1.
             That is the same memory region should not be
             defined for both PAGE 0 and PAGE 1.
             Doing so will result in corruption of program
             and/or data.
    
             Contiguous SARAM memory blocks or flash sectors can be
             be combined if required to create a larger memory block.
    */
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
              /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
              /* BEGIN is used for the "boot to Flash" bootloader mode   */
    
       BEGIN           	: origin = 0x080000, length = 0x000002
       RAMM0           	: origin = 0x000122, length = 0x0002DE
       RAMD0           	: origin = 0x00B000, length = 0x000800
       RAMLS03          : origin = 0x008000, length = 0x002000
    /*	RAMLS1           : origin = 0x008800, length = 0x000800
        RAMLS2           : origin = 0x009000, length = 0x000800
        RAMLS3           : origin = 0x009800, length = 0x000800 */
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RESET           	: origin = 0x3FFFC0, length = 0x000002
      
    	/* Flash sectors */
       /* FLASHA          : origin = 0x080002, length = 0x03FFFE	/* on-chip Flash */
        FLASHA          : origin = 0x080100, length = 0x03FF00
        FLASHG          : origin = 0x0C0000, length = 0x010000
        FLASHH   		: origin = 0x0D0000, length = 0x010000
    
    	/*FLASHAB  		: origin = 0x0FE000, length = 0x002000  /* Sector 27 (8KB)       */
    
    
    
    //   FLASHN_RSVD     : origin = 0x0BFFF0, length = 0x000010    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    PAGE 1 :   /* Data Memory */
             /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
    
       BOOT_RSVD       : origin = 0x000002, length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
        RAMD1           : origin = 0x00B800, length = 0x000800
    
        RAMLS5      : origin = 0x00A800, length = 0x000800
    
    	RAMGS0          : origin = 0x00C000, length = 0x001000
    	RAMGS1          : origin = 0x00D000, length = 0x001000
    	RAMGS2          : origin = 0x00E000, length = 0x001000
    	RAMGS3          : origin = 0x00F000, length = 0x001000
    	RAMGS4          : origin = 0x010000, length = 0x001000
    	RAMGS5          : origin = 0x011000, length = 0x001000
    	RAMGS6          : origin = 0x012000, length = 0x001000
    	RAMGS7          : origin = 0x013000, length = 0x001000
    
    
    	RAMGS8          : origin = 0x014000, length = 0x001000  /* 4KB */
    	RAMGS9          : origin = 0x015000, length = 0x001000  /* 4KB */
    	RAMGS10         : origin = 0x016000, length = 0x004000  /* 4KB */
    
    	RAMGS14         : origin = 0x01A000, length = 0x002000  /* 4KB */
    
    }
    
    
    SECTIONS
    {
    
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : >> FLASHA      PAGE = 0
       codestart           : > BEGIN	PAGE = 0
    
    #ifdef __TI_COMPILER_VERSION__
        #if __TI_COMPILER_VERSION__ >= 15009000
            GROUP
            {
                .TI.ramfunc
                { -l F021_API_F2837xS_FPU32.lib}
             
            } LOAD = FLASHH,
              RUN  = RAMLS03|RAMLS4,
              LOAD_START(_RamfuncsLoadStart),
              LOAD_SIZE(_RamfuncsLoadSize),
              LOAD_END(_RamfuncsLoadEnd),
              RUN_START(_RamfuncsRunStart),
              RUN_SIZE(_RamfuncsRunSize),
              RUN_END(_RamfuncsRunEnd),
              PAGE = 0    
        #else
            GROUP
            {
                ramfuncs
                { -l F021_API_F2837xS_FPU32.lib}
             
            } LOAD = FLASHH,
              RUN  = RAMLS03|RAMLS4,
              LOAD_START(_RamfuncsLoadStart),
              LOAD_SIZE(_RamfuncsLoadSize),
              LOAD_END(_RamfuncsLoadEnd),
              RUN_START(_RamfuncsRunStart),
              RUN_SIZE(_RamfuncsRunSize),
              RUN_END(_RamfuncsRunEnd),
              PAGE = 0    
        #endif
    #endif
    
    
    
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1       PAGE = 1
       .esysmem            : > RAMLS5       PAGE = 1
    
       /* Initalized sections go in Flash */
       .econst             : >> FLASHA       PAGE = 0
       .switch             : > FLASHA      PAGE = 0
    
       .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       Filter_RegsFile     : > RAMGS0,	   PAGE = 1
    
       SHARERAMGS0		: > RAMGS0,		PAGE = 1
       SHARERAMGS1		: > RAMGS1,		PAGE = 1
    
       /* Flash Programming Buffer */
      /* BufferDataSection : > RAMD1, PAGE = 1, ALIGN(8)*/
      .mydata             : > RAMGS10       PAGE = 1	/*修改成连续16K,用于保存打印缓冲*/
      .uartbuff		   : > RAMGS14       PAGE = 1 /*串口缓冲区*/
      .ziku               : > FLASHG      PAGE = 0 /*自定义段,用于存放自定义字库点阵*/
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    
    
    
    

  • 您好

    该错误似乎与链接器命令文件中映射到PAGE 1的单元化部分(可能是.mydata、.uartbuff)有关。

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/761417/compiler-tms320f28377s-warning-data-is-being-written-to-auto-generated-file

    请您参考这个帖子。