This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP工作温度和工作功率会很大吗?



在调试过程中发现,F28069工作的温度为70℃,不知这个工作温度对于DSP来说是否正常?
另外我们使用36V数字电源为控制板供电(板子上有降压电路),当DSP(F28069)中没有程序时,电源输出电流为0.1A(36V),当DSP运行程序时,电源输出电流变成了0.2A(36V),DSP功耗会有那么大吗?