This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 生成的HEX文件怎么烧写到外部FLASH中?



我使用CCS5.4开发F28335遇到如下疑惑:

如果需要从外部FLASH中启动F28335,应该有哪些操作?

我编写了外部FLASH烧写的基本函数,可以读写擦等操作,也知道怎么从CCS读取HEX文件写入到FLASH。

主要是一个问题:HEX文件写入FLASH是逐位WORD对齐依次写入的吗?我的FLASH是SST39VF800A,是16位的,转换为HEX是采用CCS自己生成的HEX方式。

非常感谢!