This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335XINTF程序一段,运行不起来,麻烦TI技术员和各位朋友帮忙看看吧



要用28335xintf输出16位数据。按照我这样配置,D0口会产生方波的。但是程序写进去之后,接上示波器观察,没反应。程序是运行的,因为led在闪烁。

void main(void)

{

  short temp=0;

  InitSysCtrl();

  DINT;

  IER=0x0000;

  IFR=0x0000;

  InitPieCtrl();

  InitPieVectTable();

initled();

 init_zone7();

 LED1off;

LED2off;

while(1)

{

 temp++;

 if(temp==1)

 {

   uint16* p=(uint*)0x20000;

  *p=0x00000000;

       LED1on; LED2off;

 }

 if(temp==2)

   {

   uint16* p=(uint*)0x20000;

  *p=0x00000001;

      temp=0;

       LED1off;

  LED2on;

   }

   delay(10000); 

}

}

 

void init_zone7(void)

{

 EALLOW;

     SysCtrlRegs.PCLKCR3.bit.XINTFENCLK = 1;

InitXintf16Gpio();

    XintfRegs.XINTCNF2.bit.XTIMCLK = 0;

    XintfRegs.XINTCNF2.bit.WRBUFF = 3;

    XintfRegs.XINTCNF2.bit.CLKOFF = 0;

    XintfRegs.XINTCNF2.bit.CLKMODE = 0;

    XintfRegs.XTIMING7.bit.XWRLEAD = 1;//写建立等待状态周期=1XTIMCLK

    XintfRegs.XTIMING7.bit.XWRACTIVE = 2;//写激活等待周期=2XTIMCLK

    XintfRegs.XTIMING7.bit.XWRTRAIL = 1;//写追踪等待周期=1XTIMCLK

    XintfRegs.XTIMING7.bit.XRDLEAD = 1;//读建立等待状态周期=1XTIMCLK

    XintfRegs.XTIMING7.bit.XRDACTIVE = 3;//读激活等待周期=3XTIMCLK

    XintfRegs.XTIMING7.bit.XRDTRAIL = 0;//读追踪等待周期=0XTIMCLK

    XintfRegs.XTIMING7.bit.X2TIMING = 0;

    XintfRegs.XTIMING7.bit.USEREADY = 0;

    XintfRegs.XTIMING7.bit.READYMODE = 0;

 

    // 1,1 = x16 数据线(采用)

    // 0,1 = x32 数据线

    XintfRegs.XTIMING7.bit.XSIZE = 3;

EDIS;

   asm(" RPT #7 || NOP");

}