请问XDS100V1仿真器的驱动一直识别不出来,在Target Configuration File 中是有xds100v1这个选项的,但是在test connection的时候就会报错,类似于未接仿真器时的提示。而设备管理器里是可以看到有USB口接入,但是驱动设备那有感叹号提示符,重新在C:\ti\ccsv6\ccs_base\emulation\windows\xds100_drivers\ftdi下载驱动也不行,卸载CCS重新下载多次也不行,目前是CCSv6仍不可用,大家有什么好办法吗
错误提示:
The explanation is:
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may one or more of: invalid emulator serial number,
blank emulator EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the emulator can be located.