This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XINTF以及片内AD初始化问题

Other Parts Discussed in Thread: DAC7744

如下代码,建立工程后,直接将例程中adc_soc的.c文件内容复制进我建的工程的main中,然后编译通过,应该就能通过A3、A2两个通道采集AD 观察Voltage1[10]、Voltage2[10]吧?

我现在用的这块板子上有28335和一片FPGA,以及一块有DAC7744的板子。在老师的工程(他的工程里xintf.c没有修改)里用到XINTF,控制FPGA进而控制DAC7744,一切正常可以DA。

但是我自己建立了工程后,将官方例程的adc_soc.c的内容复制到我新建工程的main,再将InitXintf();函数添加到初始化AD函数的后面,为啥不能正常工作了呢?是否还缺少初始化的语句,请各位大神点拨点拨,感谢!

// TI File $Revision: /main/10 $
// Checkin $Date: August 13, 2007 11:17:22 $
//###########################################################################
//
// FILE: Example_2833xAdc.c
//
// TITLE: DSP2833x ADC Example Program.
//
// ASSUMPTIONS:
//
// This program requires the DSP2833x header files.
//
// Make sure the CPU clock speed is properly defined in
// DSP2833x_Examples.h before compiling this example.
//
// Connect signals to be converted to A2 and A3.
//
// As supplied, this project is configured for "boot to SARAM"
// operation. The 2833x Boot Mode table is shown below.
// For information on configuring the boot mode of an eZdsp,
// please refer to the documentation included with the eZdsp,
//
// $Boot_Table:
//
// GPIO87 GPIO86 GPIO85 GPIO84
// XA15 XA14 XA13 XA12
// PU PU PU PU
// ==========================================
// 1 1 1 1 Jump to Flash
// 1 1 1 0 SCI-A boot
// 1 1 0 1 SPI-A boot
// 1 1 0 0 I2C-A boot
// 1 0 1 1 eCAN-A boot
// 1 0 1 0 McBSP-A boot
// 1 0 0 1 Jump to XINTF x16
// 1 0 0 0 Jump to XINTF x32
// 0 1 1 1 Jump to OTP
// 0 1 1 0 Parallel GPIO I/O boot
// 0 1 0 1 Parallel XINTF boot
// 0 1 0 0 Jump to SARAM <- "boot to SARAM"
// 0 0 1 1 Branch to check boot mode
// 0 0 1 0 Boot to flash, bypass ADC cal
// 0 0 0 1 Boot to SARAM, bypass ADC cal
// 0 0 0 0 Boot to SCI-A, bypass ADC cal
// Boot_Table_End$
//
// DESCRIPTION:
//
// This example sets up the PLL in x10/2 mode.
//
// For 150 MHz devices (default)
// divides SYSCLKOUT by six to reach a 25.0Mhz HSPCLK
// (assuming a 30Mhz XCLKIN).
//
// For 100 MHz devices:
// divides SYSCLKOUT by four to reach a 25.0Mhz HSPCLK
// (assuming a 20Mhz XCLKIN).
//
// Interrupts are enabled and the ePWM1 is setup to generate a periodic
// ADC SOC on SEQ1. Two channels are converted, ADCINA3 and ADCINA2.
//
// Watch Variables:
//
// Voltage1[10] Last 10 ADCRESULT0 values
// Voltage2[10] Last 10 ADCRESULT1 values
// ConversionCount Current result number 0-9
// LoopCount Idle loop counter
//
//
//###########################################################################
//
// Original Author: D.F.
//
// $TI Release: DSP2833x Header Files V1.01 $
// $Release Date: September 26, 2007 $
//###########################################################################

#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File

// Prototype statements for functions found within this file.
interrupt void adc_isr(void);

// Global variables used in this example:
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Voltage1[10];
Uint16 Voltage2[10];


main()
{

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();


EALLOW;
#if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT
#define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz
#endif
#if (CPU_FRQ_100MHZ)
#define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz
#endif
EDIS;

// Step 2. Initialize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
InitAdc(); // For this example, init the ADC

InitXintf();

// Step 5. User specific code, enable interrupts:

// Enable ADCINT in PIE
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM

LoopCount = 0;
ConversionCount = 0;

// Configure ADC
AdcRegs.ADCMAXCONV.all = 0x0001; // Setup 2 conv's on SEQ1
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x3; // Setup ADCINA3 as 1st SEQ1 conv.
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x2; // Setup ADCINA2 as 2nd SEQ1 conv.
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;// Enable SOCA from ePWM to start SEQ1
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS)

// Assumes ePWM1 clock is already enabled in InitSysCtrl();
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm1Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start

// Wait for ADC interrupt
for(;;)
{
LoopCount++;
}

}


interrupt void adc_isr(void)
{

Voltage1[ConversionCount] = AdcRegs.ADCRESULT0 >>4;
Voltage2[ConversionCount] = AdcRegs.ADCRESULT1 >>4;

// If 40 conversions have been logged, start over
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else ConversionCount++;

// Reinitialize for next ADC sequence
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE

return;
}

  • 然后还有个问题就是,我从adc_soc.c里复制到我建立工程的main里,几个函数都不是紫色,就是普通的黑色,编译过也还是黑色,这是为啥呢?

  • 再一个,这个adc_soc的描述里面说此例程ad由pwm启动,但是我在DSP2833x_DefaultIsr.h中找到一段定义如下:

    // Group 1 PIE Interrupt Service Routines:
    interrupt void SEQ1INT_ISR(void); // ADC Sequencer 1 ISR
    interrupt void SEQ2INT_ISR(void); // ADC Sequencer 2 ISR
    interrupt void XINT1_ISR(void); // External interrupt 1
    interrupt void XINT2_ISR(void); // External interrupt 2
    interrupt void ADCINT_ISR(void); // ADC
    interrupt void TINT0_ISR(void); // Timer 0
    interrupt void WAKEINT_ISR(void); // WD

    SEQ1INT_ISR()这个函数是TI默认的ADC Sequencer 1 ISR中断服务函数,以及interrupt void ADCINT_ISR(void); // ADC还有这个,但是为什么给的例程里要重新定义PieVectTable.ADCINT = &adc_isr;这个作为中断的入口呢?

  • 你好

    PieVectTable.ADCINT = &adc_isr; 是给ADC的中断向量表赋值 adc_isr是中断处理函数的名字。你可以给中断处理函数写任何名字。只要通过这一句就可以把ADC中断向量指向它。

x 出现错误。请重试或与管理员联系。