Other Parts Discussed in Thread: C2000WARE
Hello TI team,
I am currently working on motor control applications with the F28004x series (e.g., F280049C).
I noticed that the Motor Control SDK Universal Project and Lab provides out-of-box examples mainly for F28002x, F28003x, and F280013x devices, but not for F28004x.
Since F28004x devices are widely used in motor control applications and are also listed as supported devices in C2000Ware MotorControl SDK, it would be very helpful if the Universal Project and Lab could directly support F28004x as well.
This would:
- Reduce the effort of porting existing labs and examples,
- Improve consistency across C2000 families,
- Make it easier for developers to evaluate and deploy solutions on F28004x hardware.
Could you please let us know if there are any plans to add **F28004x support** to the Universal Project and Lab in future SDK releases?
Also, if there is a recommended migration guide or example for porting the current Universal Lab to F28004x, that would be very helpful.
Thank you very much for your support!