This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2407 XINT1中断进不去。



做2407 XINT1中断,中断程序总是无法进去。不知道问题究竟出现在哪里。下面是我的中断程序,麻烦帮我看看,谢谢各位老师了!

;建立中断向量表

.sect ".vectors"
RSVECT: B _c_int0
INT1: B _c_int1
INT2: B _c_int2;PHANTOM
INT3: B PHANTOM;_c_int3
INT4: B PHANTOM;GISR4
INT5: B PHANTOM;GISR5
INT6: B PHANTOM;GISR6    这是一部分中断向量表

void SystemInit()
{

asm(" SETC INTM "); /* 关闭总中断 */
asm(" CLRC SXM "); /* 禁止符号位扩展 */
asm(" CLRC CNF "); /* B0块映射为 on-chip DARAM*/
asm(" CLRC OVM "); /* 累加器结果正常溢出*/
SCSR1=0x83FE; 
/* 打开ADC,EVA,EVB,CAN和SCI的时钟*/
WDCR=0x006F; /*0110 1111 禁止看门狗,看门狗时钟64分频 */
KickDog(); /* 初始化看门狗 */
IFR=0xFFFF; /* 清除中断标志 */
IMR=0x0003; /* 0000 0110打开中断1,2,3*/

}

main()
{
unsigned int Usys=2;
SystemInit(); //系统初始化

XINT1CR=0x0005;   //使能XINT1中断,上升沿 高优先级
MCRA=0x0004;     //XINT1配置为功能引脚
asm(" CLRC INTM ");//开总中断

while(1)
    {  

        if(count!=0)
         {
             Usys=3;
            if(count==10000)
                 {
                  count=0;
                 }
        }

   }

}

void c_int1()
{
if(PIVR!=0x01)
{ asm(" CLRC INTM ");
return;
}
count++;
IFR=0xFFFF;
asm(" CLRC INTM ");
return;

}