This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位老师,问题如题,能吗?在此谢过了。
HRPWM每个PWM模块只有一路,你可以尝试将两个PWM模块同步后进行输出。
F28022不能,每个模块都只有PWMA可以出高精度,但是你可以设置PWMB与PWMA完全取反,这样PWMB就也是高精度模式,只是不能输出带有死区的波形,你可以在输出口加模拟芯片产生死区。
或者使用F2837X或者F2807X都可以输出成对带死区的高精度PWM
感谢囧的热心回复。另外还有几个问题想请教:
1.一般电机控制采用UP-DOWN的对称型PWM控制,考虑降低谐波。那除了电机控制,还有什么应用需要使用UP-DOWN模式的PWM,我做数字电源DC-DC,需要使用UP-DOWN吗?
2.若我采用28022作为DCDC控制用,采用UP或DOWN的PWM,主频50MHz,当我PWM周期设为1000时,我的输出PWM频率可达50kHz,这个计算对吗?