This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: 使用CCS12.8.1,C2000Ware 6.0.0写的新程序无法烧录到核心FLASH内

Part Number: TMS320F2800137
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG

使用的SysConfig空工程进行的测试,程序能正常烧录,但是烧录过程会跳过FLASH擦写过程,使用UniFlash烧录对应的.out文件也会跳过相关步骤。

芯片管脚情况如下

使用的是全jTAG连接,只有芯片的nRST没有与烧录器连接,nRST是一个4.7kOhm上拉+100nF电容组合,振荡器输入是一个有源晶振,使用仪器检查其正常工作,工作频率20MHz

  • 你能详细说明一下你面临的问题吗?我假设在闪存设置中选中了复选框“擦除和编程”,但您没有看到闪存在编程之前被擦除。是这样吗?
    在编程之前,你如何检查闪存是否被擦除?

    此外,E2E线程的标题指出,“新编写的程序……不能刻录到核心FLASH中”,但在您的描述中,您提到该程序确实可以正常编程到FLASH中。
    看到闪存被编程为正确的内容有什么问题吗?

  • 我这边查了下其他器件的情况,改了下板子,把GPIO24与GPIO32调整为上拉,板子掉电后再启动的电流是正常的