This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问control suite中HVPSFB-VMC中关于 DPLIB Variables 的问题 谢谢

volatile long VfbSetSlewed = 2093568; // Slewed set point for the FB voltage loop - start from 4V
volatile long VfbSlewRate = 25600; // FB Slew rate adjustment

volatile long phase = 0; // FB phase command
int16 dbAtoP_leg = 20, dbPtoA_leg = 20; // Dead band adjust for the two legs

请问上述 给定的参考电压 VfbSetSlewed = 2093568 怎么会是从4V开始呢  还有死区时间int16 dbAtoP_leg = 20中,20指的是多少时间  初学者  请指教 谢谢哈