请教大神,这段时间用28035控制DSP28035做一个BOOST单环升压,输入12V 想让输出为24V,但是输出始终达不到,当给定为16V时就可以达到,做了PI的闭环调节,做了限幅,上限占空比为90%,下限占空比为10%,但是当我给定输出16V的时候占空比打的是70%,这样的逻辑是不对的,按说我能达到16V的话占空比应该最后稳到10%才对啊,我这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教大神,这段时间用28035控制DSP28035做一个BOOST单环升压,输入12V 想让输出为24V,但是输出始终达不到,当给定为16V时就可以达到,做了PI的闭环调节,做了限幅,上限占空比为90%,下限占空比为10%,但是当我给定输出16V的时候占空比打的是70%,这样的逻辑是不对的,按说我能达到16V的话占空比应该最后稳到10%才对啊,我这是什么原因?
PWM的频率是10K啊 配置没问题的 断续模式下可以正常工作