This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: TMS320F280049C – CMPSS5 and CMPSS6 not responding while CMPSS3 works normally

Part Number: TMS320F280049C


Hello TI Team,

I am using the TMS320F280049C in my project and encountered an issue where CMPSS5 and CMPSS6 do not respond to input signals, while CMPSS3 works normally under the same conditions. I am reporting the issue here for further support.


1. Test Environment

  • Device: TMS320F280049C

  • Test code: TI official example project for CMPSS

  • Test method: Added CMPSS3, CMPSS5, CMPSS6 for comparison under identical configuration

  • Input: External analog voltage signal

  • Reference: Internal DAC threshold


2. Configuration

All three CMPSS modules were configured with the same settings, including:

  • High comparator enabled

  • DAC reference enabled

  • Same DAC threshold value

  • Outputs routed to GPIO for observation

  • Comparator hysteresis and filters disabled (same for all)

I also tested by setting DAC = 0, input 1.25 V, but CMPSS5/6 still show no output change.


3. Observation

  • CMPSS3: Responds correctly to input voltage crossing the threshold.

  • CMPSS5 & CMPSS6:

    • No output toggling

    • No change even when the threshold is set to 0

    • No observable response at output pin or when reading internal status registers


4. Additional Checks

  • Verified the input voltage with oscilloscope

  • Confirmed ADC channels connected to the same pins read correct voltages

  • Swapped test boards:

    • Some boards work fine

    • A few boards consistently show CMPSS5/6 failure

  • No conflicts with pin mux or other peripherals


5. Questions

  1. Are there known issues with CMPSS5 or CMPSS6 on certain lots of the F280049C?

  2. Could this be related to pin mux, analog routing, or silicon errata?

  3. Are there diagnostic registers I can check to further confirm CMPSS hardware failure?

  4. Do you recommend performing additional factory test patterns or self-test routines to validate the CMPSS hardware?


6. Attachment

I can provide:

  • Test code snippet

  • Register dump

  • Video / screenshots of oscilloscope and output signals

  • Affected device lot numbers


Thanks in advance. I appreciate your support.

Regards,

Tang