I would like to see a comparison of resource consumption and performance metrics between the TMS320F28P650DK and F28388D in EtherCAT Applications. This will help me evaluate and select between the two chip types for my design.
I would like to see a comparison of resource consumption and performance metrics between the TMS320F28P650DK and F28388D in EtherCAT Applications. This will help me evaluate and select between the two chip types for my design.
Hi , When comparing these two for EtherCAT applications, the EtherCAT IP implementation is fundamentally the same on both device.Consider your specific application requirements , usecase and select the device based on your requirements considering size of ram , flash .. to determine the most appropriate device for your design.
I understand it. but I'm unclear about the EtherCAT performance and CPU utilization differences between the C28x and the F28388D's M4. Specifically:
1. Can the F28388D's M4 core handle EtherCAT independently while the C28x core runs my application?
2. When the F28P650 uses a single C28x core for EtherCAT, will there be remaining resources for other tasks?
3. Could you share benchmark data comparing their multi-core resource allocation and real-time performance when implementing EtherCAT?