This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: 双核烧写load symbol后无法进入cla中断的问题

Part Number: TMS320F28377D


这是我现在cpu1用的cmd文件代码,现在出现的问题是但我直接点击debug时,能够正常进入cla中断中如图image.pngimage.png

而如果按双核烧写的流程先connect cpu1,cla1,cpu2,然后分别load cpu1,cpu2的.out文件,对cpu1cla load symbol,再依次run cpu1,cla,cpu2,发现无法进到cla中断里(通过观察cla中的变量osgx_a)并且cpu1似乎也没有在进程中因为观察变量没有实时刷新,run cpu1会显示跳转:Break at address "0x3fe44e" with no debug information available, or outside of program code.
run cla会显示跳转:Break at address "0x0" with no debug information available, or outside of program code.
报错: Can't Run Target CPU: (Error -2060 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 12.6.0.00029) 如图image.png


2837xD_FLASH_CLA_lnk_cpu1.cmd:

// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C

MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 :

BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */

RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800


RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080

}


SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB |FLASHC|FLASHE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
//ramfuncs : LOAD = FLASHD,
//RUN = RAMLS4,
// LOAD_START(_RamfuncsLoadStart),
// LOAD_SIZE(_RamfuncsLoadSize),
// LOAD_END(_RamfuncsLoadEnd),
// RUN_START(_RamfuncsRunStart),
// RUN_SIZE(_RamfuncsRunSize),
// RUN_END(_RamfuncsRunEnd),
// PAGE = 0, ALIGN(4)

/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMLS2 PAGE = 1
.esysmem : > RAMLS2 PAGE = 1

/* Initalized sections go in Flash */
.econst : > FLASHB PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)

.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

Filter_RegsFile : > RAMGS0, PAGE = 1

/* CLA specific sections */
Cla1Prog : LOAD = FLASHD,
RUN = RAMLS5,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0, ALIGN(4)

CLADataLS0 : > RAMLS0, PAGE=1
CLADataLS1 : > RAMLS1, PAGE=1

Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1

.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS4,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)

/* The following section definition are for SDFM examples */
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : > RAMGS5, PAGE = 1, fill=0x3333

MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM PAGE = 1
MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM PAGE = 1
IPC_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
#ifdef CLA_C
/* CLA C compiler sections */
//
// Must be allocated to memory the CLA has write access to
//
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > RAMLS1, PAGE = 1

.scratchpad : > RAMLS1, PAGE = 1
.bss_cla : > RAMLS1, PAGE = 1
.const_cla : LOAD = FLASHB,
RUN = RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 1
#endif //CLA_C
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/


想知道是烧写方式有问题还是cmd的内存分配有问题或是其他问题

  • 感谢您对TI产品的关注!
    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好,   

    报错: Can't Run Target CPU: (Error -2060 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 12.6.0.00029)

      如果你尝试“运行”CLA,而CLA当前没有执行任务,就会出现此错误消息。如果CLA处于空闲状态,只能由C28x软件或外设中断启动。CCS无法启动CLA。

    CPU1+CLA子系统与CPU2+CLA子系统是独立的。我能想到的唯一可能是触发CLA的外设可能已被重新分配到另一颗CPU?

    我建议尝试使用C28x软件触发每个CLA,看看是否有效。如果有效,那么问题很可能出在外设的设置上。