用哪个有前途?单片机51比较熟悉,2407和2812有接触和简单使用。想搞电机控制、运动控制,该深入2812和 28335还是转STM32?谢谢指点!
现在不论其他哪个电子网站bbs里面stm32论坛都是最火的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi leo one
me too! 同感!CCS(我现在已用最新版V6.1)的编译速度也较慢。但好在TI给提供的各种资源较全,遇到的问题通过FAE、deyisupport基本都能解决。
但更重要的是TI的产品稳定性、可靠性很好,用着放心。相比较起来ST的是大路货,拼价格,走低端路线,做民品可以考虑。工业品还是首选TI。
自从用了M3、M0、M4后,51就基本放弃了,它的性能、功能还是简单。像AVR、PIC、430等都比他好用很多,但单片机的问题是各自有各自的编译器和开发平台,不通用,这时他最他的问题,而M3、M0、M4解决了这个问题,这也是我为什么用M3、M0、M4的原因。
电机控制最好选C2000,最新的2807x取代了经典型号28335。28069等都不错,如果做多轴电机控制,可用F28M35/6,双核(M3+ C28),最多可做3轴,我就用它做了一款产品,但不是电机控制。
如果高安全领域,建议用570系列,R4F双核,SIL3认证。有ePWM,可做电机控制,我用它来做双BLDC高压电机,效果不错,产品已研发成功。
C2000、570、28M35等技术难度相当大,需花大量时间学习!
加油!
FYI!