This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335能连接但无法烧写



自制控制板,一直工作正常,最近突然出现目标连接不太正常,有时连接很慢,连接上也无法烧写,CCS提示擦除错误,芯片被锁或者未连接,重新焊了一片仍然如此。请问会是哪里的问题

  • 检查电源,3,3V和1.8V是否正常,3.3V是否输出能力足够

    检查是否所有3.3V和1.8V引脚都已经供电?

    用的是哪颗芯片?

    如果是Piccolo系列,请检查跟1.8V相关的引脚是否有1.2uf以上的电容?必须每个都加,至少1.2uf,推荐2.2uf

    检查晶振 和时钟

    检查 Jtag电路,是否该上下拉的已经正确了。

    对照TI的Control Card进行原理图检查。