This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TI公司生产的DSP处理器烧写过程中报错的问题

大家好,我在用TI公式生产的2407芯片烧写程序过程中,CCS与仿真器连接后进行烧写,在烧写过程中报错,其具体提示如下:

**** Begin Sector Clear Operation ****
OK: Flash Algorithm loaded into DSP memory
OK: Write sector value 0x000f to symbol PRG_options
OK: Set Breakpoint at PRG_stop
OK: Running flash algorithm
OK: DSP Halted
OK: Read status value 0x0000 from symbol PRG_status
OK: PC set to PRG_erase
OK: Running flash algorithm
OK: DSP Halted
Error: Read status value 0x0001 from symbol PRG_status
Flash algorithm failed during clear operation

具体情况如附件所示。

现在确定Flash电压为5V,仿真器是好的。大家有遇到这种情况的吗?麻烦各位给与一定的建议,谢谢啦!