我的是关于电机控制的程序,在程序进行多次电机启停测试后进入了ILLEGAL_ISR,在进入ILLEGAL_ISR前,发现一些变量会变成不确定的值,这是我配置的。cmd文件
{
BEGIN : origin = 0x0A0000, length = 0x000002 // Update the codestart location as needed
BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001B1, length = 0x00024F
RAMM1 : origin = 0x000400, length = 0x000400
RAMD0 : origin = 0x00C000, length = 0x002000
RAMD1 : origin = 0x00E000, length = 0x002000
RAMD2 : origin = 0x01A000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0x8000. User should comment/uncomment based on core selection
RAMD3 : origin = 0x01C000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xA000. User should comment/uncomment based on core selection
RAMD4 : origin = 0x01E000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xC000. User should comment/uncomment based on core selection
RAMD5 : origin = 0x020000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xE000. User should comment/uncomment based on core selection
。。。。
codestart : > BEGIN
.text : > FLASH_APPA, ALIGN(8)
.cinit : > FLASH_APPA, ALIGN(8)
.switch : > FLASH_APPA, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.blt_mb : > RAMM0, type = NOINIT, ALIGN(4)
.stack : > RAMM1
停止时候的寄存器值: