F280I第一次上电时,目标板连接正常,但在执行烧写程序是一直处于卡死状态,程序没有烧写成功,但JTAG各口电压及DSP各电源正常,这时断开连接再次上电,烧写程序界面一直处于UNCLOK状态,此后一直处于此状态,求解
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
F280I第一次上电时,目标板连接正常,但在执行烧写程序是一直处于卡死状态,程序没有烧写成功,但JTAG各口电压及DSP各电源正常,这时断开连接再次上电,烧写程序界面一直处于UNCLOK状态,此后一直处于此状态,求解
是unlock 还是lock?
芯片烧写时不能强行断开,否则有几率导致芯片锁死。
楼主烧写不正常,建议楼主对于检查芯片的时钟和电源。
下面几点请楼主注意:
1、C2000芯片本身,C2000芯片没有正确的提供电源和时钟,导致C2000芯片不工作,所以连接不上仿真器
2、仿真器本身,几率比较低,一些仿真器本身有BUG
3、仿真器驱动,由于部分仿真器驱动不支持64位的电脑所以出问题,另外CCSV3不支持WIN7和64位机。
4、JTAG,JATG有短路,JTAG过长,比如超过15CM,JTAG布线如果超过15CM应该加buffer作为中继,建议JTAG的PCB引线越短越好。
5、电脑,碰到过有人用番茄花园版的XP连接不上开发板,经常死机的案例
6、USB线,USB线不能超过2M,否则USB仿真器会不正常
7、TRST引脚,该引脚要连接
8、配置出错,比如TDS510的仿真器选择XDS510,28335的芯片选择28346
是LOCK 烧写时电源供电一切都是正常的,没有突然断电,而且连接也是正常的 我用的XP系统的电脑,设备应该都是正常的,换了其余的板子烧写都是正常的,这块板子芯片各引脚电压也都是正常的