TMS320F280025C: LAUNCHXL-F280025C开发板烧录芯片MSP432E401YT

Part Number: TMS320F280025C
Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-F280025C

我的开发板LAUNCHXL-F280025C在使用Uniflash时,提示Warning: A firmware update is required for the XDS110 probe. The current firmware is version 3.0.0.32. The probe must be upgraded to firmware version 3.0.0.38 to be compatible with this software. Click the "Update" button to update the firmware. DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE. (Emulation package 20.3.0.3656) 

我点击了更新,但是更新失败了,现在无法连接到开发板了。请问这个该如何重新烧录MSP432E401YT芯片程序?