This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812的spi问题

猜测是2812的spi存在频率不稳定抖动情况,导致我的采样出现频率错误。我使用的是ti的dsp2812的spi连接AD7988-5,一切都工作的很好,但是波形总是出现一点相位失真,例如测试3000Hz正弦波会出现几个Hz的频率错误,AD7988-5的输入端是测试的信号,已经确认过输入没有频率错误,但是到dsp端的采样序列就出现了频率错误,会是dsp的spi时钟抖动或者其他问题吗?有碰到过同样问题的同志吗?有没有什么解决方案。采样频率8k,2812spi驱动。并且以前使用的2812的spi控制音频接编码器,通信总是出现错误并且大部分时候配置解编码器的寄存器出现问题,通信过程中也会出现通信错误,是就我自己遇到该问题了吗?有遇到该问题的分享下怎么解决的?