This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用28377D做数字电源开发相关问题

Other Parts Discussed in Thread: CONTROLSUITE

您好!

    现使用贵公司的28377做数字电源的研发,28377数字控制板需要完成的任务大概有这些:输出多路PWM、根据ADC采样结果进行计算调节PWM相关参数、CAN和485接口与其他数字板通信、硬实时的保护功能。在参考了controlSUITE中相关例程后,现有如下问题:

    1.在查看例程时发现双核的例程中都有后缀为cpu01和cpu02两个工程,是否在使用双核时,都需要建立两个工程?两个工程的内存段如何分配?双核的程序如何烧写到FLASH中断电运行?

    2.一个CPU使用BIOS工程,运行通信相关任务;另一个CPU使用裸机工程,监控硬件,实现保护功能;CLA则操作ADC和PWM等外设,实现计算任务。请问这样的设计方案是否可行?

  • 双核的每一个内核都有自己的FLASH,和自己的RAM,也有共享的RAM,必须建立两个工程,双核就可以理解为两个独立的内核。两个CPU可以运行不同的程序,并且CLA也可以独立运行程序。